Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

76-100 из 526

Упорядочить:
On the ENA I am receiving the message "Continuous switching may damage source attenuator". What corrective actions should I pursue?

FAQ 2012-03-16

Is the display intensity adjustable on the ENA?

FAQ 2012-03-16

What is the recommended transit case for my Keysight ENA Series Network Analyzer?
Custom fit ENA Series transit cases are not available. However customer can refer to other commercial company’s product like Pelican or ECS case.

FAQ 2012-02-28

Can I hide the softkey menu when I perform "Dump Screen Image" on the ENA / ENA-L?
Yes.

FAQ 2012-02-02

What are the implications of swapping test heads between different Keysight 4287A Impedance Analyzers?
The Keysight 4287A Impedance Analyzer must be used with the furnished test head as a set because it is an indivisible portion of the calibrated 4287A.

FAQ 2012-01-16

How is trace math implemented within the Keysight Technologies Vector Network Analyzers?

FAQ 2012-01-11

Does the ENA support 87050E / 87075C series multiport test sets?
Unlike the E5061A and E5062A, the E5061B, E5071C and E5072A (ENA) does NOT support full functions of 87050E / 87075C. But it is possible to change switch state of 87050E-Hxx / 87075C-Hxx via GPIB.

FAQ 2012-01-11

What is an alternative solution to the 87075C / 87050E replacement?
Build your home-made switch box using the L4491A RF/MW switches. Refer to the application note for details.

FAQ 2012-01-11

While programming the ENA I am receiving the error, "-128, Numeric data not allowed". Why?
For many analyzers the data transfer format is adjustable when outputting data...

FAQ 2011-10-07

Are the commands compatible between the ENA and the ENA-L?
Yes. Commands for the ENA / ENA-L are fully compatible as far as the common functions are concerned.

FAQ 2011-10-07

Does the ENA-L support a built-in web page similar to the 871x family?

FAQ 2011-10-07

Are the adapters in the 85033E 30kHz to 9GHz calibration kit phase matched?
Yes.

FAQ 2011-10-07

What are the benefits of the built-in VBA?

FAQ 2011-10-07

On the ENA / ENA-L, what is the meaning of "1.#QNB" or "1.#QNAN"?

FAQ 2011-10-07

On the ENA and ENA-L, is there a SCPI command to query the active channel?
Yes.

FAQ 2011-10-07

How do I configure my Keysight IO Libraries Suite 14 to communicate with my ENA via LAN?

FAQ 2011-10-07

What is the difference between Smoothing and Averaging on a Keysight network analyzer?

FAQ 2011-10-07

How can I find accessories for a Keysight product?
For instrument-specific accessories (such as probes for an oscilloscope), first go to the product page and then see the related accessories. For general-purpose accessories (such as rf & microwave test accessories, carts, and racks), go to the ...

FAQ 2011-10-07

How can I calculate the equivalent phase delay, as a function of frequency, for a given electrical delay as set on Vector Network Analyzer?
Equivalent phase delay, based upon electrical delay is computed as: θ˚ = Ftest * Delay * 360

FAQ 2011-10-07

Is it possible to change the font size of softkey menu on ENA?
Yes. The font size of softkey menu can be changed with following procedure...

FAQ 2011-10-07

Are there equation examples for ENA Equation Editor?
Yes.

FAQ 2011-10-07

When I save a Touchstone file with the ENA / ENA-L, which calculation will be reflected in the Touchstone file?
All calculations are reflected in the Touchstone file except for the mixed-mode conversion.

FAQ 2011-10-07

What is the difference between "sweep speed", "cycle time" and "time per data point" as related to a vector network analyzer?

FAQ 2011-10-07

Where can I find upgrade information of ENA?
Please refer to the ENA series service and support home page.

FAQ 2011-10-07

The ENA / ENA-L was infected with the virus. What should I do?
Remove the LAN cable and perform system recovery.

FAQ 2011-10-07

Назад 1 2 3 4 5 6 7 8 9 10 ... Следующие