Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

251-275 из 526

Упорядочить:
Are the GPIB commands of the 4287A compatible with the 4286A?

FAQ 2009-03-11

Can the Rdc measurement function of the 4287A be used instead of a digital multimeter to measure the DC resistance of an inductor?
No, it is not recommended to measure DC resistance of inductors with the Rdc measurement function. This function is provided for contact check.

FAQ 2009-03-11

What should I perform when the 4287A displays an “OVLD” message?
First, check if the DUT has properly contacted the test fixture’s electrodes. If no contact error is found, check for a possible failure of the 4287A.

FAQ 2009-03-11

How can I order the upgrade kit of the 4287A?

FAQ 2009-03-11

How should I make Rdc measurements with the 4287A to improve measurement stability for low DC resistance below 1 ohm?
It is recommended to set the averaging factor of the 4287A to 4 or above in order to make as stable Rdc measurements as the 4286A does.

FAQ 2009-03-11

Can open/short/load correction data be entered in the 4285A from an external PC over GPIB?

FAQ 2009-01-14

What is the output impedance of the 4285A?

FAQ 2009-01-14

What are the key points of the techniques for integrating the 4285A in a scanner system?
To select an appropriate scanner, you need to determine the connection method (three-terminal, four-terminal, shielded four-terminal, etc) suitable for the impedance range of the devices to be measured.

FAQ 2009-01-14

How can I order the upgrade kits for the 4285A?
The available upgrade kits are listed on the 4285A Option Upgrades page, which is linked to Keysight LCR Meters Upgrades homepage.

FAQ 2009-01-14

How can I replace the contact electrodes of the 16118A?
The contact electrodes of the 16118A cannot be replaced by user.

FAQ 2009-01-13

What are the differences between the 16048A and the 16048D?
The differences between the 16048A and 16048D are shown in the table below...

FAQ 2009-01-13

What should I care in order to ensure good measurement correlation between the 16196A/B/C/D and other Keysight test fixtures?

FAQ 2009-01-13

How can I get a 0603 size LOAD standard that can be used to perform LOAD correction using the 16196C and other SMD test fixtures?
Keysight part number 0699-6926 can be used as a LOAD standard. It is a 51-ohm chip resistor.

FAQ 2009-01-13

Can I use the 16048B with the 4285A for the cable extension?
Yes, the 16048B (Part Number 16048-60030) can be used with the 4285A. But, it is not easy to perform the cable correction using the 100-ohm resistor box (furnished with the 4285A).

FAQ 2009-01-13

What is the purpose of the grounding lead of the 16048D?
The grounding lead of the 16048D is used to interconnect this shielding conductor and the ground terminal on LCR meter's front panel.

FAQ 2009-01-13

Isn't the current 16034E equipped with a dual-post stopper while previous ones had the stopper attached to the right side of Hcur connector?
The 16034E currently has no stopper because all impedance analyzers that required the stopper became obsolescence by 2001.

FAQ 2009-01-13

What compensation should I perform when I use the 16048B with the 4285A?
It is recommended to set the Cable Length function of the 4285A to "1 m" and perform open/short/load compensation at the DUT contact terminals of the test fixture connected to the tip of the 16048B.

FAQ 2009-01-13

Can a DC bias current be applied to an inductor DUT when the 16065C is used with the 4263B?
No, the 16065C can only be used to apply a DC voltage bias.

FAQ 2009-01-13

How should open compensation be performed on the 16034E/G/H?
Locate the High and Low side contact pins the same distance apart as the length of the DUT by using the following procedure...

FAQ 2009-01-13

How can I obtain the open and short terminations which are not supplied with the 42030A?
The 42090A Open Termination and the 42091A Short Termination are available as the four-terminal-pair open/short reference terminations.

FAQ 2009-01-13

What is the part number of the tweezers contact tip used in the 16334A?
The contact tweezers tip is Keysight part number 16334-09002. A single 16334A requires two of the 16334-09002 tips.

FAQ 2009-01-12

Why is the capacitance measured for an air-dielectric with the 16452A unstable?
If the capacitance measured for an air-dielectric is unstable, check whether the 16452A electrodes are sufficiently clean or not.

FAQ 2009-01-12

Can I use the 42842C with the 4284A and the 42841A?
No, you can't. The 42842C is not designed to be used with the 4284A. The 42842C can only be used with the 4285A

FAQ 2009-01-12

What is the maximum DC bias output current of the 4285A with option 001?

FAQ 2009-01-12

Why is the capacitance measured for a liquid material with the 16452A unstable?

FAQ 2009-01-12

Назад ... 11 12 13 14 15 16 17 18 19 20 ... Следующие