Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

176-200 из 526

Упорядочить:
Why cannot I control TEST SET ATTEN PT1 and PT2 functions in ATTENUATOR MENU when the 87511A S-parameter test set is used with the 4395A?
The TEST SET ATTEN PT1 and TEST SET ATTEN PT2 functions cannot be controlled because the 87511A is not equipped with input attenuators.

FAQ 2010-07-02

Why is Sweep Delay Time of the 4294A prolonged when DC bias is set to ON?
The DC bias source inside the 4294A requires a certain settling time before starting a sweep measurement.

FAQ 2010-07-02

Why does measurement data exhibit a discontinuity at 5 MHz or 15 MHz and how can the 4294A get rid of this phenomenon?
The 4294A extends its measurement frequency range up to 110 MHz by terminating each measurement terminal with 50 ohm in order to eliminate the resonance of test leads (including leads inside the 4294A).

FAQ 2010-07-02

Can I have criteria or a list of non-applicable liquid materials for the 16452A?
Avoid measuring acidic, alkaline and ionic materials with the 16452A.

FAQ 2010-07-02

Can the 4294A measure a grounded DUT?
The 4294A can measure the grounded DUT when used with the 42941A Impedance Probe.

FAQ 2010-07-02

How can I replace the contact tip of the 16334A?
The replacement contact tip is orderable by part number 16334-09002.

FAQ 2010-07-02

Why is there a step (discontinuity) on the trace of noise floor around 10 MHz in 4395A's SA mode even when no signal is input into the test port?
This phenomenon is caused by a change in circuit operation of the 4395A at 10 MHz.

FAQ 2010-07-02

How is measurement accuracy calculated when the 42841A is used with the 4284A, 4285A or E4980A?
The measurement accuracy is the sum of the measurement instrument accuracy and additional error produced when the instrument is used with the 42841A and bias current test fixture.

FAQ 2010-07-02

Why is Rp or G measurement value unstable when pure water is measured with the 16452A?
There are two conceivable causes of unstable measurement results. One of primary causes is a change in temperature of pure water sample measured. The other is a slight pollution which resides on the electrode surfaces.

FAQ 2010-07-02

How wide range of resistivity can the 4339B measure when used with the 16008B?
The 4339B can measure surface resistivity up to 7 x 1017 Ω and volume resistivity up to 8 x 1018 Ω-cm, but it depends on the electrodes of the 16008B used.

FAQ 2010-07-02

What is input impedance of the 4339B?
Nominal input resistance is 1000 Ω .

FAQ 2010-07-02

How should I define or select the residual inductance values of Shorting Bars when performing Short compensation on the E4991A or the 4287A?
Nowadays, the authorized standards stipulate the dimensions of shorting devices and the Short Compensation method which uses the defined inductance values of the shorting devices. It is recommended to consider these authorized standards.

FAQ 2010-07-02

Why don't the E4991A and 4287A have Load compensation function?
Performing Load compensation in addition to Open/Short compensation is equivalent to performing Open/Short/ Load calibration at DUT contacts of test fixture (by using the working standard devices).

FAQ 2010-07-02

What are primary differences between the E4991A and 4291B?
The major difference is frequency range. E4991A: 3 GHz, 4291B: 1.8 GHz.

FAQ 2010-07-02

Can the E4980A perform open/short/load correction at user-specified spot frequency points while open/short correction at all frequency points is OF...
No, open/short/load correction at user-specified spot frequency points can be activated only when open/short correction at all frequency points is set to on.

FAQ 2010-07-02

Error message "PHASE LOCK LOOP UNLOCKED" could be displayed, when the 4294A using an external ref. osc (opt.1D5 or other 10 MHz output) is ON.
The message is removed when any key of the front panel except [Preset]. In this case, the unit works properly.

FAQ 2010-07-02

Does typical permittivity measurement accuracy includes all the uncertainties due to the E4991A with opt 002, 16453A and MUT insertion conditions?
Yes. All the uncertainties are included in the typical measurement accuracy.

FAQ 2010-07-02

Is it possible to separate the test head from the E4991A and interconnect them with cables?
Yes. It is possible with option E4991A-010 or option E4991A-007 only.

FAQ 2010-07-02

Can the 4338B measure internal resistance of a battery?
Yes, the 4338B can directly measure internal resistance of a battery.

FAQ 2010-06-14

How low resistance can the 4338B measure and resolve?
The effective resistance measurement range and resolution of the 4338B is down to 10 micro-ohms. The minimum display resolution of the 4338B is 0.1 micro-ohms.

FAQ 2010-05-14

What is max. DC output voltage when two 42841A units are used as a 40A system?

FAQ 2010-05-12

Is the E4991A option 010 needed only when a specific probe station is used with the E4991A?
No, the E4991A-010 is generally needed when a probe station is used with the E4991A.

FAQ 2010-05-12

What are the precautions when using the 4284A LCR Meter with the 42841A Bias Current Source and the 42842A/B Fixtures?

FAQ 2010-05-12

When fabricating a custom test fixture for the Keysight 4339B, what are the recommendations to extend the measurement and interlock cables?

FAQ 2010-05-11

Can I perform real time measurement with Keysight U1731B & U1732B Data Logger Software?
The Data Logger Software is to provide an indicative check on the unit and not intended for high timing accuracy measurement…

FAQ 2010-05-05

Назад 1 2 3 4 5 6 7 8 9 10 ... Следующие