这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

1-25 / 526

排序:
The temperature characteristic test sample program does not work on the 64-bit version of Excel.
Download and use the Tctest64.xlsm

FAQ 2019-08-21

Is 4338B Adjustment Program still available?
The 4338B adjustment program (04338-65005) that could be found in 4338B Service Manual no longer available…

FAQ 2017-09-26

How to measure output frequency of E4981A Capacitance Meter?
To measure the output frequency of E4981A Capacitance Meter, interface box (Keysight part number: 04294-61002) is required…

FAQ 2017-09-20

Where can I find information on E4980A/AL error messages?
E4980A/AL error messages are described in Appendix B of the Users Guide.

FAQ 2017-06-28

I am using an electronic load to draw current into my DUT, but when I draw current the voltage drops. Why is this happening?
A voltage drop will appear across this impedance as current flows through it in accordance with Ohm’s Law. Click on the question for additional information.

FAQ 2017-06-28

Is it possible to develop specific macros for E5061B to support TRL cal or the unknown thru method under a 9-term calibration method?
Yes, it is possible to perform a user developed 8-term calibration, like TRL, using an external program for the E5061B. Click on the question for additional information.

FAQ 2017-06-28

How to maintain 16195B?
The 16195B which consists of Open, Short, 50 Ω Load and Low-loss Capacitor terminations is calibration kit for LCR Meter/Impedance Analyzer and Network Analyzer (NA). The 16195B itself does not have warranted specification as independent product. Maintenance of the 16195B depends on what instrument you calibrate with 16195B.

FAQ 2017-03-15

E4991B 硬件、软件和固化软件升级
E4991B 阻抗分析仪可用升级选件的完整列表

FAQ 2016-07-26

4396B 选件升级
4396B 射频网络/频谱/阻抗分析仪,100 kHz 至 1.8 GHz/2 Hz 至 1.8 GHz

FAQ 2016-02-26

什么是增强型过载检测和电源跳闸功能?
从 2015 年秋季起,E5061B 选件 115/117/135/137/215/217/235/237 开始标配增强型过载检测和电源跳闸功能。E5061B 选件 3L5 不具备这种功能。

FAQ 2016-01-28

E5061B 硬件、软件和固化软件升级
E5061B ENA 系列网络分析仪可用升级选件的完整列表

FAQ 2016-01-27

微软终止支持 Windows XP,对我的 ENA 有何影响?
自 2014 年 4 月 8 日起,微软已终止对 Windows XP 操作系统的支持,本文将帮助您回答某些重要的问题。

FAQ 2015-07-27

E4990A 硬件、软件和固化软件升级
E4990A 阻抗分析仪可用升级选件的完整列表

FAQ 2015-07-16

How should I set the "Adapter Setting" of the 4294A when using the 16089A/B/C/D/E?
Please set to "NONE".

FAQ 2015-06-09

如何使用 ENA 执行 75 Ω 测量?
您可以将 ENA 的系统特征阻抗变为 75 Ω,然后执行 75 Ω 测量。

FAQ 2015-03-09

When automating markers on the ENA is it possible to programmatically query the indicated inductance or capacitance on a Smith Chart?
The inductance / capacitance information cannot be directly queried via the automation interfaces. The inductance (positive reactance, top half of the Smith Chart) or capacitance (negative reactance, lower half of the Smith Chart) is not available as an automation query.

FAQ 2014-08-11

微软终止支持 Windows XP,对我的 E4982A 有何影响?
自 2014 年 4 月 8 日起,微软已终止对 Windows XP 操作系统的支持。本文将帮助您回答某些重要的问题。

FAQ 2014-07-15

E4982A 硬件、软件和固化软件升级
E4982A 硬件、软件和固化软件升级

FAQ 2014-05-01

什么是 CPU / 存储器 / Windows 操作系统的历史记录?
CPU 类型/内存大小、存储器类型/容量、Windows 操作系统的历史记录等均在表格中列出。

FAQ 2014-04-28

What are the differences between the E4980A and 4284A?
Most of the E4980A functions are compatible with the 4284A's. Since some enhancements and updates of functionality are incorporated in the E4980A, there are primary differences summarized in the table.

FAQ 2014-04-07

通过只带有一个GP-IB接口的是德分析仪打印和采集屏幕图像,您是否可提供好的建议?

FAQ 2014-02-08

E4980A 和 42841A 之间的电缆的部件编号(P/N)是什么?
最新的电缆部件编号为 E4980-61640。

FAQ 2014-02-06

Replacing the 8508A vector voltmeter with the E5061B network analyzer
Measuring the phase difference of an external CW signals is a typical measurement application of the 8508A vector voltmeter.

FAQ 2013-10-14

How can I order the upgrade kit of the 4395A
The model numbers of available upgrade kits for the 4395A options are as follows.

FAQ 2013-06-24

How can I perform the calibration/compensation when I use the 16094A with a 7-mm connector extension cable?
It is recommended to perform the following compensation procedure...

FAQ 2013-06-05

1 2 3 4 5 6 7 8 9 10 ... 下一页