検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

1-25 / 58

並べ替え
What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.

FAQ 2019-08-28

FlexDCA: What Licenses Do I Have, And What Features Do They Enable?
FlexDCA: What Licenses Do I Have, And What Features Do They Enable?

FAQ 2018-12-10

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced FDD?
The X-Series upgrade path to LTE-Advanced FDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

Where do I find E6651A Mobile WiMAX™ Test Set Software and Firmware
Links to N64xxA and E665xA software and the neccessary firmware.

FAQ 2014-10-28

N8241AおよびN8242Aの工場アップグレード・オプションとは?
N8241AおよびN8242Aの工場アップグレード・オプションのリスト。

FAQ 2014-10-13

How do I update the operating system in an N9038A MXE EMI receiver from Windows XP to Windows 7?
See what is required to update the operating system in an N9038A MXE EMI Receiver...

FAQ 2014-04-02

86100Aまたは86100Bメインフレームの86100Cへの改造は可能でしょうか?
いいえ。86100A/Bから86100Cへのメインフレーム (ハードウェア) の改造は行えません...

FAQ 2013-11-27

E8257D PSGアナログ信号発生器のアップグレード
ハードウェア・アップグレード、測定器ソフトウェアに関する情報の検索

FAQ 2013-08-20

After purchasing an N9094AK upgrade, must the instrument be sent to a Keysight Service Center to be upgraded?
No. The N9094AK upgrades can easily be installed by the user...

FAQ 2013-04-25

How can I get 8960 Lab Application Annual Contract Subscription Release Downloads?
Get the latest downloads here

FAQ 2013-02-28

HTML HTML
Why do I need to pay installation/calibration charges for N4010A license-only upgrades?
The N4010A has several license-only upgrade paths, most of which enhance the base technology options that are already enabled in the unit. Click on the question above for a fuller description.

FAQ 2013-02-06

Why are some of the features shown in the Framescope user manual not available in software version 7.0.5?
Users might encounter different features when using Framescope software version 7.0.5 versus what is stated in the documentation.

FAQ 2012-11-28

Why must my N4010A instrument firmware be A.05.06.02 (or newer)?
This is the minimum firmware revision for a hardware change that was introduced during October 2012

FAQ 2012-10-30

IO ライブラリ・スイート:付属のスイート 14以降で以前のバージョンを使用できますか?
Keysight の測定器を 1台お持ちのお客様には、バージョンに関係なく、IO ライブラリの 1つのライセンスを使用する法的権利があります。

FAQ 2012-10-08

IO ライブラリ・スイート 15.0 ライセンスが付属していますか?
Keysight では、約 150種類のKeysight の測定器モデル、GPIB および I/O コンバータ製品.....

FAQ 2012-10-08

[サービス] 以前購入したオシロスコープやロジック・アナライザ用ソフトウェアのライセンス・キー、パスワードの回復方法は?
オーダ番号と認証番号が分かる場合、以下のページから該当する製品のライセンス・キーを得ることができます

FAQ 2012-04-04

Why must my N4010A instrument firmware be A.05.04.01 (or newer)?
This is the minimum firmware revision for a hardware change that was introduced during December 2011.

FAQ 2012-02-24

Why i can't find other languages help file setting in U160X A/B series HH oscilloscope?
In order to access to other language, please go to respective product support page in www.Keysight.com. Go to Driver & Software page, select Firmware Update.

FAQ 2011-09-12

Why are my N4010A DEVM test results different with firmware revision A.05.03.15?
Revision A.05.03.15 was a short-lived release that used a modified measurement algorithm. Please upgrade to revision A.05.03.16, which uses the correct measurement algorithm.

FAQ 2011-02-18

IO Libraries Suite: What is new with Keysight IO Libraries Suite 14.0?
Keysight IO Libraries Suite provides a new and improved set of tools for establishing, verifying, and troubleshooting instrument-to-PC connections.

FAQ 2010-10-30

Why does my E6651A fail Source Modulated Power Level Accuracy in TME?
This may be due to a compatibility issue between the E6651A firmware version and TME.

FAQ 2010-10-14

IO Libraries Suite: What are the differences between Keysight IO Libraries Suite versions 14.0 and 14.1?
The major enhancement that has been added to version 14.1 is compatibility with National Instruments NI-488.2 API or I/O Library.

FAQ 2010-09-08

IO Libraries Suite: What pieces of software do I need to install for the IO Libraries to work?
View the data sheet for the full list of requirements.

FAQ 2010-09-08

IO Libraries Suite: What has changed in version 14.2?
Version 14.2 includes defect fixes and makes two changes to improve the compatibility of Keysight 488 with third-party software.

FAQ 2010-09-08

1 2 3 次へ