Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

1-25 из 59

Упорядочить:
S8709A Virtual Drive Test Toolset - Technical Overview

Обзор технических характеристик 2020-10-13

PDF PDF 2.76 MB
S8709A Virtual Drive Test Toolset - Technical Overview
Keysight’s S8709A Virtual Drive Test Toolset is a real-world lab test environment for validating 5G devices under a wide range of network signaling and radio channel conditions. It offers a fully controlled test scenario enabling quick and systematic performance validation.

Обзор технических характеристик 2020-10-13

PDF PDF 2.80 MB
S8707A RF/RRM Carrier Acceptance Toolset - Technical Overview
Keysight’s S8707A RF/RRM Carrier Acceptance Toolset provides the performance and flexibility needed to effectively test the RF characteristics of 5G NR devices according to the industry requirements.

Обзор технических характеристик 2020-09-28

PDF PDF 4.10 MB
F9650A Compact Antenna Test Range - Data Sheet
The Keysight F9650A Over-The-Air (OTA) Compact Antenna Test Range (CATR) chamber provides a measurement environment for characterizing wireless and antenna system performance of devices at millimeter-wave (mmWave) frequencies. Use the chamber with Keysight test and measurement equipment in a range of applications including device R&D and 3rd Generation Partnership Project (3GPP)/Cellular Telecommunications Industry Association (CTIA) conformance test.

Техническая информация 2020-08-11

PDF PDF 443 KB
Keysight’s 5G Test Solutions Enable SK Telecom to Verify Performance of 5G Devices

Материалы для прессы 2020-07-30

Keysight First to Gain Validation of 5G USIM Protocol Conformance Test Cases by GCF

Материалы для прессы 2020-07-29

UXM 5G Test Application - Technical Overview
Keysight's UXM 5G Test Application network emulation software accelerates device development and acceptance. It provides a high level of customization for network parameters and testing scenarios.

Обзор технических характеристик 2020-07-20

PDF PDF 2.08 MB
S8708A 5G Advanced Performance Test Toolset - Technical Overview
The S8708A Advanced Performance Test Toolset is part of Keysight’s 5G Network Emulation Solution portfolio that addresses the entire device development workflow from early design to acceptance and manufacturing.

Обзор технических характеристик 2020-07-06

PDF PDF 2.19 MB
S8704A Protocol Conformance Toolset - Technical Overview
S8704A Protocol Conformance Toolset (PCT) gives you access to the latest 3GPP defined protocol conformance tests. It provides an easy-to-use Graphical User Interface in which you can create campaigns of tests, set PICS/PIXIT parameters, view logs and create reports. In this document we will describe the graphical user interface and functionality provided by Protocol Conformance Toolset in more detail. We will also describe the hardware platform on which Protocol Conformance Toolset is run.

Обзор технических характеристик 2020-06-24

PDF PDF 3.90 MB
M1740A mmWave Transceiver for 5G - Data Sheet
The M1740A mmWave transceiver for 5G is a versatile remote radio head covering multiple frequency bands. It is used as a key component of several Keysight 5G solutions to test at mmWave frequencies.

Техническая информация 2020-06-19

PDF PDF 776 KB
PROPSIM FS16 5G Channel Emulation Solution - Solution Brief
5G user experience depends on device performance in harsh mobile environments. Keysight’s channel emulators enable you to validate device and base station end-to-end real-world performance in the lab.

Совместное решение 2020-06-15

PDF PDF 10.10 MB
Nemo Outdoor - Brochure
This brochure introduces the key features and benefits of Nemo Outdoor

Брошюра 2020-06-15

PDF PDF 2.40 MB
S8706A Protocol Carrier Acceptance Toolset - Technical Overview
S8706A Protocol Carrier Acceptance Toolset provides comprehensive access to protocol carrier acceptance test plans mandated by the world’s major 5G mobile operators. In this document we will describe the graphical user interface and functionality provided by Protocol Carrier Acceptance Toolset in more detail. We will also describe the hardware platform on which Protocol Carrier Acceptance Toolset is run.

Обзор технических характеристик 2020-05-13

PDF PDF 1.20 MB
Enabling Device Troubleshooting - Technical Overview
Technical overview for enabling device troubleshooting for Network Emulation solutions

Обзор технических характеристик 2020-05-08

PDF PDF 2.79 MB
Keysight First to Gain Approval from 3GPP for 5G NR Protocol Test Cases that Support CA
Keysight’s 5G network emulation solution supports the widest range of protocol conformance test cases validated by the Global Certification Forum

Материалы для прессы 2020-05-04

S8705A RF/RRM DVT and Conformance Toolset - Technical Overview
S8705A is an integrated solution that enables RF performance testing of 5G devices against reference conformance and acceptance test plans (FR1 and FR2) and supports test cases for C-V2X.

Обзор технических характеристик 2020-04-15

PDF PDF 5.58 MB
Benchmark 5G Devices in the Lab
S8710A 5G Device Benchmarking Toolset enables standardized lab-based end-to-end automation of 5G device benchmarking with a predefined set of test cases, customizable scripts, and extensive reports.

Демонстрация 2020-02-11

Nemo 5G Device Analytics - Flyer

Брошюра 2020-02-06

PDF PDF 1.94 MB
S8710A Device Benchmarking Toolset - Technical Overview

Обзор технических характеристик 2020-02-05

PDF PDF 2.21 MB
Enables Major U.S. Mobile Operators to Accelerate 5G with Leading Number of 5G Device Test Cases
Keysight delivers more than 600 validated test cases to support 5G new radio (NR) device acceptance plans

Материалы для прессы 2020-01-30

Develop C-V2X with Confidence as 5G Evolves

Демонстрация 2020-01-23

SA8700 C-V2X Test Solution
This document provides information about how to configure for C-V2X Test Solution

Руководство по конфигурации 2020-01-14

Sky5® LiTE Complete Front-end System for 5G, tested with Keysight 5G Test Application Framework
Watch a video demonstration of Skyworks Sky5® LiTE solution. The video shows great performance on key RF parameters including transmit power, waveform performance and EVM. Results obtained through test with Keysight 5G Test Application Framework using Keysight E7515B UXM 5G Wireless Test Platform.

Демонстрация 2020-01-09

Qualcomm Extend 5G Collaboration to Accelerate Commercialization of DSS Technology

Материалы для прессы 2019-11-25

Keysight First to Achieve 3GPP C-V2X Radio Frequency Conformance Test Case Validation
Keysight solutions enable the automotive industry to accelerate commercialization of connected cars and autonomous vehicles

Материалы для прессы 2019-11-25

1 2 3 Следующие