이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

1-11 / 11

정렬방식:
How many carriers can the MXG support in Carrier Aggregation mode?
One MXG can support one instance of the Carrier Aggregation mode. One instance of the Carrier Aggregation mode supports 5 component carriers.

FAQ 2017-06-28

M8000 시리즈를 위한 30일 무료 체험판 라이선스
M8000 제품군 내의 모든 체험판 라이선스에 대한 개요 및 링크

FAQ 2017-01-31

All N603x Arbitrary Waveform Generators IVI and MATLAB Instrument Drivers
Supported models: N6030A, N6031A, N6032A, N6033A

FAQ 2014-08-12

What are the Factory Upgrade options for the N8241A and N8242A?
List of options for N8241A and N8242A factory upgrades.

FAQ 2014-05-01

What are the Factory Upgrade options for the M9330A?
List of options for M9330A factory upgrades.

FAQ 2014-05-01

On my E8267D, I get an error that the signal requires more repeats than supported, can I increase this limit with the internal baseband option?
No. To increase the number of pulse capacity either upgrade to an External Baseband option with the N8241A AWG or ...

FAQ 2012-12-30

What is the best configuration for wideband I/Q modulation?
An E8267D Option 016 or an N8212A Option 016 signal generator with an M8190A arbitrary waveform generator

FAQ 2012-12-28

What is the performance difference between the N8212A module with Option 016 and the N8241A arbitrary waveform generator synthetic instrument module?
The N8212A with Option 016 is based on the E8267D PSG signal generator with Option 016; the N8241A is based on the N6030A arbitrary waveform generator.

FAQ 2012-12-28

Keysight Driver Migration Tool

FAQ 2012-01-20

M8190A 12 GSa/s Arbitrary Waveform Generator
March 1st question and answer session

FAQ 2011-03-07

PDF PDF 178 KB
N8241A/N8242A Frequently Asked Questions

FAQ 2010-11-22