Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discutez avec un expert

Support technique

Mesure Electronique

Support by Product Model Number:

51-75 sur 106

Tri:
LabVIEW G Programming Information
This help file contains LabVIEW G programming guidelines and reference information for the M9330A Series Arbitrary Waveform Generator.

Fichier d'aide 2015-07-28

ZIP ZIP 1.24 MB
IVI Driver Reference
Keysight's IVI drivers simplify the creation and maintenance of instrument control applications in a variety of development environments.

Fichier d'aide 2015-07-28

ZIP ZIP 1.33 MB
Generating PAM-4 Signals using an M8195A AWG
Learn about using the M8195A Arbitrary Waveform Generator in conjunction with a 33 GHz real time scope to generate PAM-4 signals. As well as how to calibrate the set up for optimal frequency response. And some capabilities of the M8195A in terms of modifying and changing the characteristics of the PAM-4 signal.

Démonstration de base 2015-07-08

Fundamentals of Arbitrary Waveform Generation, AWG Primer - Reference Guide
This primer discusses characteristics and fundamentals of arbitrary waveform generation and the different implementations available in the market. It also shows examples how to generate digital, multi-level and PAM4 signals, wireless and modulated waveforms, multi-carrier as well as coherent optical signals.

Guide de références 2015-06-01

M8195A Arbitrary Waveform Generator - User's Guide (old version for rev. 1 hardware)
The M8195A is a 65 GSa/s Arbitrary Waveform Generator with the highest combination of speed, bandwidth and channel density. Flexible signal generation at up to 32 Gbaud. Clean and distorted signal to stress the device to the limits.

Manuel de l'utilisateur 2015-05-01

M8195A Arbitrary Waveform Generator OFC Video 2015
An overview of what an AWG is and what the advantages of using an AWG for optical applications are; which applications are supported by an AWG in the optical space and what the advantages of the Keysight M8195A over other AWG’s in the market are.

Démonstration de base 2015-04-20

Digital Design & Interconnect Standards - Brochure
Brochure shows Keysight’s high-speed digital solution set , a range of essential tools, measurement and simulation—that will help cut through the challenges of gigabit digital designs.

Brochure 2015-03-09

PDF PDF 7.71 MB
MIPI M-PHY, D-PHY and C-PHY Receiver Testing- Recorded webcast
MIPI M-PHY, D-PHY and C-PHY Receiver Testing- Recorded webcast

Démonstration de base 2014-11-03

AWG article - MWJ product feature
AWG article - MWJ product feature

Article 2014-10-14

M8195A Arbitrary Waveform Generator – Getting Started Guide
The M8195A is a 65 GSa/s Arbitrary Waveform Generator with the highest combination of speed, bandwidth and channel density. Flexible signal generation at up to 32 Gbaud. Clean and distorted signal to stress the device to the limits.

Guide de démarrage rapide 2014-10-01

M8195A 65GSa/s AWG – Press Release
Introduces 65-GSa/s High-Speed Arbitrary Waveform Generator

Dossier de presse 2014-09-10

Keysight M8195A AWG - The Digital and Arbitrary Signal Generator
Keysight M8195A AWG - The digital and arbitrary signal generator with the highest combination of speed, bandwidth and channel density The M8195A AWG is a high speed AWG with up to 65 GSa/s sample rate and 20 GHz bandwidth on up to 4 channels per module.

Démonstration de base 2014-09-08

Keysight M8195A AWG within the Mobile & Network Ecosystem
As devices and interfaces become faster and more complex, the M8195A AWG gives you the versatility to create the signals you need for digital applications, optical and electrical communication, advanced research, wideband radar and satcom.

Démonstration de base 2014-09-08

Microwave Frequency Up-Converters Extend Signal Simulation to 40 GHz – Synopsis
Microwave frequency up-converters extend signal simulation to 40 GHz from Synopsis and Keysight

Brefs de solution 2014-08-04

Wideband Digital Pre-Distortion with Keysight SystemVue & PXI Modular Instrument - Application Note
Digital Pre-Distortion (DPD) is essential for wideband communications systems based on LTE-Advanced and 802.11ac. Overcome DPD challenges with trusted commercial measurement and modeling tools.

Notes d’application 2014-08-01

Using Flexible Digital Modulation Testing for Satellite Regenerative Payloads - Application Note
This application note focuses on solutions for the issues that create risks in the integration of mixed-signal systems with a mix of software and hardware tools. Examples focus on measurements of error vector magnitude (EVM), which is a key figure of merit for modulated signals implemented in either analog or digital form.

Notes d’application 2014-08-01

Satellite Test Solution – AAI
Satellite Payload and Panel Test Solution from AAI and Keysight Technologies

Brefs de solution 2014-04-09

Enhancing microwave spectroscopy in astrophysics applications – Article
An arbitrary waveform generator is the key element in this faster and more accurate method.

Article 2013-11-15

A new approach for multi-emitter test signal generation – Article
A new capture and playback approach generates multi-emitter test signals using a combination of COTS test equipment and simulation software.

Article 2013-11-15

Meeting satellite testing challenges - Article
Satellites are now a critical part of the infrastructure supporting the incredible growth in demand for broadband data.

Article 2013-11-13

Understanding 802.11ad Physical Layer and Measurement Challenges Tutorial
View this 6-part recorded tutorial presented by Keysight experts for an overview of standards and market trends followed by an in-depth description of the physical-layer construction.

Manuel de l'utilisateur 2013-09-20

Press Releases for M8190A

Dossier de presse 2013-09-06

Press Release for M8192A
Infinite Playtime and Multichannel Support introduced for Arbitrary Waveform Generator

Dossier de presse 2013-09-05

M8190A Arbitrary Waveform Generator - Videos
M8190A Arbitrary Waveform Generator - Videos

Démonstration de base 2013-09-04

M8190A Waveform Generator - Software Examples and Video Resources - Demo
MATLAB software is available as an option from Keysight with the M8190A waveform generator to create your own arbitrary or standard waveforms, automate signal generation, and develop GUI-based applications. This M8190A resource page for MATLAB provides access to various M8190a including IQTools, a GUI-based application example for the M8190A created for instrument connection, waveform creation, and amplitude and phase correction. IQTools and the modifiable source code are provided when you order the MATLAB N6171A option with the M8190A so that you can extend IQTools to meet your specific testing needs.

Démonstration de base 2013-08-06

Précédente 1 2 3 4 5 Page suivante