您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

PXIe 機箱

依產品型號搜尋可用的支援:

1-25 / 28

排序:
Tested PC and PXI/AXIe Chassis Configurations - Technical Overview
This document provides a list of personal computers which are compatible with the M9005A, M9010A, M9018B, M9019A PXIe Chassis and the M9502A, M9505A, M9506A, M9514A AXIe Chassis.

技術總覽 2020-05-11

PDF PDF 1 MB
BIOS and Windows Settings for Modular Systems - Technical Overview
This technical note provides the detailed BIOS and Windows settings for modular systems using the tested computers that are compatible with Keysight Technologies, Inc. PXI/AXIe chassis.

技術總覽 2020-04-30

PDF PDF 531 KB
PXIe Chassis Family Security Guide
The security guide explains the procedure for declassifying the chassis.

參考指南 2020-02-20

PDF PDF 7.42 MB
M9005A Security Guide
The security guide explains the procedure for declassifying the chassis.

參考指南 2019-12-20

PDF PDF 7.21 MB
Resolve PXIe and AXIe Chassis Communication Problems
This guide helps you understand and troubleshoot PXIe and AXIe chassis connectivity issues.

參考指南 2019-12-05

PDF PDF 2.86 MB
Keysight PXIe Chassis Cooling Guidelines - White Paper
Module temperatures in a PXI system can impact operating conditions. It’s important to actively manage the environment inside your chassis.

應用手冊 2019-10-14

PDF PDF 702 KB
PXIe Chassis Family User Guide
This 150 page PDF document tells you how to use the M9010A, M9018B, and M9019A PXIe Chassis.

使用手冊 2018-09-06

PDF PDF 16.09 MB
PXIe Chassis Family Startup Guide
Installation and startup information for the PXIe Chassis Family

快速入門指南 2018-09-06

PDF PDF 2.51 MB
Keysight PXIe Chassis Fan Control Tool
Download this zipped folder containing the Fan Control Tool. The Fan Control Tool is a command line executable that controls the fan speed in a Keysight PXIe chassis. For many applications, the default chassis fan speed provides more cooling than required at the extra cost of fan noise. By changing the configuration from the default, you can significantly reduce fan noise. Use the Fan Control Tool to monitor the chassis temperatures and fan speeds to determine a balance of fan noise and cooling performance. After finding the appropriate setting, you can set the controller to run this tool and apply your setting every time the device boots up. Documentation and source code included.

分析工具 2018-09-05

ZIP ZIP 15.98 MB
Keysight PXIe Chassis Interactive Block Diagram
Download this zipped PDF of the Keysight PXIe Chassis Interactive Block Diagram and view using Adobe Reader. If you open the PDF using a browser, you can’t use the interactive features. This document provides detailed diagrams and descriptions of the structure, functions, and features of the M9010A, M9018B, and M9019A PXIe chassis. The Interactive Block Diagram is amazing and informative interactive media.

操作手冊 2018-05-31

ZIP ZIP 3.87 MB
PXIe Chassis Specification Guide
This 24 page PDF document contains detailed technical specifications and characteristics of the M9010A, M9018B, and M9019A PXIe Chassis.

產品型錄 2018-05-03

PDF PDF 827 KB
多機箱設計師
這套互動式工具可協助您配置和安裝 PXIe 和 AXIe 多機箱系統。

配置設定指南 2017-06-29

M9018B PXIe Chassis Soft Front Panel
This help file explains how to use the Soft Front Panel and also explains many of the chassis features.

輔助說明檔 2017-04-19

ZIP ZIP 3.54 MB
M9019A PXIe Chassis Soft Front Panel
This help file explains how to use the Soft Front Panel and also explains many of the chassis features.

輔助說明檔 2017-04-19

ZIP ZIP 3.68 MB
M9010A PXIe Chassis Soft Front Panel
This help file explains how to use the Soft Front Panel and also explains many of the chassis features.

輔助說明檔 2017-04-19

ZIP ZIP 2.64 MB
Chassis Family Driver Help Files
This zip file contains 6 help files. Two are for the PXIe Chassis Family driver IVI API; both IVI.NET and IVI-C. Two are for the Trigger Manager IVI API; both IVI.NET and IVI-C. Two are for the LabVIEW driver; one for the PXIe Chassis Family and the other for the Trigger Manager.

輔助說明檔 2017-04-19

ZIP ZIP 5.30 MB
M901x PXIe 機箱功率計算器
您可輸入周圍空氣溫度、高度、交流電源電壓等等,並且計算機箱模組可用的總功率。

分析工具 2017-03-27

Keysight PXIe Chassis Family Service Guide
Troubleshooting and diagnostics information for PXIe chasis

維修服務手冊 2017-03-01

PDF PDF 1.70 MB
Three new PXle Chassis - from low-cost to high-performance

新聞資料 2017-02-22

Keysight Technologies M9010A PXIe 主機箱 - 產品規格書
Keysight M9010A PXIe 10 插槽第三代主機箱能提供出色的靈活性、相容性和優異性能,外形更小巧,滿足桌面應用的苛刻要求。

產品型錄 2016-11-16

M9005A PXIe 主機箱整合式系統模組,5 插槽,3U - 產品規格書
Keysight M9005A PXIe 5 插槽主機箱其設計旨在提供低成本、適合工作臺使用的解決方案,同時支援 PXIe 相容性和性能。

產品型錄 2016-11-09

M9018B PCIe 和 M9019A PCIe 18 插槽 PXIe 機箱 - 應用說明
Keysight M9018B 和 M9019A PXIe 18 槽機箱能夠提供出色的靈活性、相容性和性能,滿足應用的苛刻要求。

產品型錄 2016-09-23

M9005A PXIe Chassis User Guide
M9005A PXIe Chassis User Guide. Provides installation and use instructions.

使用手冊 2016-07-01

PDF PDF 3.07 MB
Interface Modules and Adapters for PXI and AXIe Systems - Data Sheet
This document provides technical specifications, characteristics and other information about the series of PCIe host desktop adapters and PXI chassis system and cable modules

產品型錄 2016-04-13

2014 Global PXI Instrumentation Growth Excellence Leadership Award - Article Reprint
Frost & Sullivan honors Keysight as a growth leader in the PXI modular instrumentation market in 2014.

專文 2014-05-22

PDF PDF 598 KB

1 2 下一頁