您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

1-17 / 17

排序:
What specification adder should be applied when performing Ohms measurements with OCOMP off?
Information on applying the Ohms specification with OCOMP OFF and OCOMP ON.

FAQ 2014-04-27

Can I measure duty cycle or pulse width with the U1251A/U1252A Handheld Digital Multimeter?
Yes, you can measure duty cycle or pulse width with the U1251A and U1252A Handheld Digital Multimeter.

FAQ 2013-11-17

Under the unit function’s ACV and DCV, the display rate of U1271/2A indicates 7 times per second, can GUI DATA LOGGER capture all 7 readings?
No, the GUI DATA LOGGER is running on different acquisition method than the unit’s display rate, therefore the fastest update rate is 1 sample per second.

FAQ 2011-05-05

How does excessive heat and cold affect the accuracy of Keysight 34401A measurements?
This can be determined by using the temperature coefficients published in the User's Guide. Notice the "Temperature Coefficient/degree C" column…

FAQ 2010-07-23

When will Keysight USB modular instruments and USB Modular DAQs supports Windows 7?
For 32 bit Windows 7, the supportability of modular instruments and DAQs will happen...

FAQ 2010-07-18

What is the relationship between the “No. of Least Significant Digit” and the accuracy of a handheld meter?
The “No. of Least Significant Digit” affects the accuracy of a handheld meter....

FAQ 2010-02-21

What is the relationship between the “No. of Least Significant Digit” and the accuracy of a handheld multimeter?
The “No. of Least Significant Digit” affects the accuracy of a handheld multimeter....

FAQ 2010-01-07

What is the relationship between the "Count" and the accuracy of U3401A or U3402A Digital Multimeter?
One "count" is defined as a unit change (change of 1) in the last digit of the meter display…

FAQ 2009-10-20

What does "Display Counts" means in the U3401A/U3402A Digital Multimeter Data sheet?
Display counts give the largest number the multimeter's display can show….

FAQ 2009-09-29

Does the Measurement Manager (AMM) run on Window Vista operating system?
Yes. The Measurement Manager (AMM) rev. 1.8.3.0 and above will able to run on Windows Vista ...

FAQ 2009-06-10

Does the Keysight Measurement Manager (AMM) support regional language settings other than English (US)?
Yes, the Keysight Measurement Manager (AMM) supports regional language settings other than English (US)….

FAQ 2009-01-12

What is the maximum frequency that can be measured with the U1252A Digital Multimeter?
The U1252A Digital Multimeter has a frequency counter function that can measure frequency up to 20MHz.

FAQ 2008-09-24

What is the peak-to-peak voltage of the square wave that is generated by the U1252A Digital Multimeter?
The peak-to-peak value of the square wave that is generated by the U1252A Digital Multimeter is 2.8V.

FAQ 2008-09-24

Keysight 34401A 有 LAN IO 連接方式嗎?
沒有。但若需要區域網路 (LAN) 連結產品,請考慮 Keysight E5810A LAN 至 GPIB 閘道器。

FAQ 2005-05-18

What is the sample rate of the Keysight 34401A?
When configured for the fastest reading rate, the 34401A can sample at 1000 readings/second.

FAQ 2005-02-09

How do I calculate total measurement error on the Keysight 34401A?
The accuracy specifications for the Keysight 34401A are expressed in the form: '% of reading + % of range' which match the dominate sources of error, gain and offset.

FAQ 2005-02-09

What is the voltage limit that is considered open for diode testing?
The 34401A diode test function was designed specifically for silicon diodes. The cutoff voltage for diode testing is 0.8 VDC.

FAQ 2003-06-04