이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

1-25 / 150

정렬방식:
Why do OLED (Organic LED) displays dim over time?
OLED makes great contrast but its lifespan is highly dependent on user application: power on hours, contrasts settings, storage environment and operating environment.

FAQ 2019-09-25

34401A 는 "True RMS" AC 전압 과 AC 전류 측정을 합니까?
34401A의 "True RMS" AC 전압 과 AC 전류 측정

FAQ 2016-07-06

34401A에서 Guard 단자 제공 여부
34401A에서 Guard 단자가 있습니까?

FAQ 2016-07-06

명령어로 전면판/ 후면판을 선택 가능 여부
SW 명령어로 전면판/ 후면판을 선택할 수 있는지요?

FAQ 2016-07-06

DCV ratio 측정은 34401A 과 34461A 에서 동일한지요?
34401A 와 34461A의 DCVRatio 측정 결과

FAQ 2016-06-08

Does 34450A supports multiple measurements per trigger event?
No.

FAQ 2016-02-29

How do I find the calibration code and security code for my DMM?
The factory set security code is 'AT3446XA'. This is sometimes referred to as the calibration code.

FAQ 2015-11-21

Can I enable 34450A data logger feature with programming command?
No. To enable data logging, execute "Enable log" at front panel...

FAQ 2015-09-21

Why 34405A can't be detected in Windows 7?
There are two posibilities causing 34405A couldn't be detected. 1. IO Libraries Suit 15.1 or below...

FAQ 2015-09-21

What is the calibration password to unlock the instrument?
The security code is "AT3446XA"...

FAQ 2015-09-21

How to enable 34410A/34411A/L4411A browser web control work in Java 8?
To enable browser web control to work in Java 8, update instrument to firmware version 2.41...

FAQ 2015-09-21

Can 34460 & 34461A measure capacitance?
Yes. This feature is available when the DMM is upgrade to firmware revision 2.08 and above....

FAQ 2015-09-21

트리거된 로깅 데이터를 GUI DATA LOGGER로 전송할 수 있나요?
아니요

FAQ 2015-04-22

Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

키사이트, 애질런트 및 휴렛팩커드의 단종된 테스트 장비에 대한 매뉴얼은 어디에서 확인할 수 있습니까?
대부분의 키사이트 제품의 PDF 매뉴얼은 제품 페이지에서 확인하실 수 있습니다. 다른 벤더들도 예전 매뉴얼을 제공합니다.

FAQ 2014-08-01

What specification adder should be applied when performing Ohms measurements with OCOMP off?
Information on applying the Ohms specification with OCOMP OFF and OCOMP ON.

FAQ 2014-04-27

Keysight 34401A의 sample rate는 얼마인가요?
가장 빠른 읽기 비율로 구성했을 때 34401A는 초당 1,000번 읽기(1000readings/seconds) 샘플링을 할 수 있습니다

FAQ 2014-04-23

다이오드 테스트에서 open 상태로 간주되어 지는 한계전압은 얼마인가?
34401A 다이오드 테스트 기능은 실리콘 다이오드에 최적화하여 디자인되어 있습니다. 다이오드 테스트의 cutoff 전압은 0.8VDC입니다.

FAQ 2014-04-23

Why are USB modular instruments (U2700 Series) and USB DAQ modules (U2300, U2500, U2600 Series) not detectable by the E5810B?
Establish the connection between the USB modular Instrument and the PC directly, and then disconnect the device from the PC (while it’s still powered-on), and connect to E5810B.

FAQ 2014-04-17

Can I have multiple math functions (Null, Min-Max, dB, dBm, Limit) on at the same time on the 34401A?
No, the 34401A only allows one math function to be used at a time.

FAQ 2014-04-15

Does the 34405A Digital Multimeter have an external trigger capability?
No, the 34405A Digital Multimeter does not have an external trigger capability.

FAQ 2013-11-17

Can I change the amplitude level for the squarewave output function?
No, you cannot change the amplitude level …

FAQ 2013-11-17

Are there any calibration options available for the U1251A/U1252A Handheld Digital Multimeter?
Yes, there are a variety of calibration options available for the U1251A and U1252A Handheld Digital Multimeter…

FAQ 2013-11-17

Do the U1251A and U1252A Digital Multimeters come with connectivity cables?
No, the U1251A and U1252A Digital Multimeters do not come with connectivity cables. The cable is an optional accessory…..

FAQ 2013-11-17

Can I use the test probe leads marked with CAT III 1000V rating come together with the U1241A/U1242A/U1251A/U1252A/U1253A handheld Multimeter…
The test lead kit which currently marked with CAT III 1000V rating can be used with the multimeter at CAT IV 600V measurement environment...

FAQ 2013-11-17

1 2 3 4 5 6 다음