検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

1-25 / 166

並べ替え
Why do OLED (Organic LED) displays dim over time?
OLED makes great contrast but its lifespan is highly dependent on user application: power on hours, contrasts settings, storage environment and operating environment.

FAQ 2019-09-25

Does 34450A supports multiple measurements per trigger event?
No.

FAQ 2016-02-29

How do I find the calibration code and security code for my DMM?
The factory set security code is 'AT3446XA'. This is sometimes referred to as the calibration code.

FAQ 2015-11-21

Can 34460 & 34461A measure capacitance?
Yes. This feature is available when the DMM is upgrade to firmware revision 2.08 and above....

FAQ 2015-09-21

Why 34405A can't be detected in Windows 7?
There are two posibilities causing 34405A couldn't be detected. 1. IO Libraries Suit 15.1 or below...

FAQ 2015-09-21

What is the calibration password to unlock the instrument?
The security code is "AT3446XA"...

FAQ 2015-09-21

Is DCV ratio measurement for 34401A and 34461A identical?
Yes. 34461A is intended as direct replacement for 34401A. Hence, the ratio measurement...

FAQ 2015-09-21

Can I enable 34450A data logger feature with programming command?
No. To enable data logging, execute "Enable log" at front panel...

FAQ 2015-09-21

How to enable 34410A/34411A/L4411A browser web control work in Java 8?
To enable browser web control to work in Java 8, update instrument to firmware version 2.41...

FAQ 2015-09-21

Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

既に販売が完了したKeysight、AgilentおよびHewlett-Packard(HP)のテスト機器のマニュアルはどのように入手できますか?
ほとんどのKeysight製品にPDFマニュアルがあり、製品ページで入手することができます。Keysightのベンダも古いマニュアルを提供しています。

FAQ 2014-08-01

OCOMPをオフにして抵抗測定を実行する場合は、仕様は変更されますか?
OCOMP OFFおよびOCOMP ONのときの抵抗仕様に適用される情報。

FAQ 2014-05-23

Why are USB modular instruments (U2700 Series) and USB DAQ modules (U2300, U2500, U2600 Series) not detectable by the E5810B?
Establish the connection between the USB modular Instrument and the PC directly, and then disconnect the device from the PC (while it’s still powered-on), and connect to E5810B.

FAQ 2014-04-17

Can I measure temperature with the 34405A Digital Multimeter using a thermocouple probe?
No, you cannot use a thermocouple probe to measure temperature with the 34405A Digital Multimeter….

FAQ 2013-11-17

Can I use the test probe leads marked with CAT III 1000V rating come together with the U1241A/U1242A/U1251A/U1252A/U1253A handheld Multimeter…
The test lead kit which currently marked with CAT III 1000V rating can be used with the multimeter at CAT IV 600V measurement environment...

FAQ 2013-11-17

Can I export the interval logging data saved in the internal memory of my U1253A Handheld Multimeter?
Yes, you can export the interval logging data saved by upgrade your U1253A Firmware revision to V1.20…..

FAQ 2013-11-17

Can I change the amplitude level for the squarewave output function?
No, you cannot change the amplitude level …

FAQ 2013-11-17

3457AのGPIBコマンドリストはありませんか?
3457Aのマニュアルに記載がございますが、マニュアルは販売終了です。

FAQ 2013-11-17

Which language is the 34405A Digital Multimeter's User’s Guide available in?
The 34405A Digital Multimeter's User’s Guide is available in 7 languages….

FAQ 2013-11-15

What type of USB cable do the 34405A Digital Multimeter use?
The 34405A Digital Multimeter use the USB type-A to type-B cable.

FAQ 2013-11-15

U1270シリーズ・ハンドヘルド・マルチメータでAC+DC混成信号を測定しているときに、DC測定モードで不正なDC電圧値が表示される条件は?
DC測定モードに対してフィルタ(LPF)がオンになっていない場合に不正な値が生じることがあります。ACのVpeakがフルスケール・レンジの3倍を超えると、読み値のエラーの原因となります。1000 Vレンジでは、フルスケールの1.5倍です。

FAQ 2013-11-10

[仕様] USBモジュラ型測定器は、Windows7をサポートしていますか?
はい、最新のKeysight Measurement ManagerにてWindows7 32bitをサポートしています。

FAQ 2013-06-24

測定器を自動制御したいと思っています。何かトレーニングテキストやコースはありませんか?
キーサイトでは、自動制御プログラムを作られる方のために、トレーニングコースをご用意しています。

FAQ 2013-06-13

[プログラミング]34410A/34411A制御プログラムを作成するためのヒントはありますか?
34410A/34411Aの測定処理コマンドについては、下記のリンクを参考にしていただけます。

FAQ 2013-03-20

What can I do if the Keysight USB Modular Instrument driver installations failed to complete installation on a Windows 7 environment?
If you encountered the event mentioned above, follow the installation best practices steps below.

FAQ 2012-07-25

1 2 3 4 5 6 7 次へ