Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discutez avec un expert

Support technique

Mesure Electronique

Support by Product Model Number:

Affiner la liste

retirer tout le raffinement

Par type de contenu

1-3 sur 3

Tri:
ATE System Level Calibration and Its Impact on Cost, Quality and Schedule - White Paper
This paper proposes an alternative method to provide system level specification and system measurement calibration which will extend the system’s ability to be used for multiple products.

Notes d’application 2017-03-20

PDF PDF 651 KB
Getting the Calibration You Need - Application Note
Calibration is the process of measuring the actual performance of an IUT using lab instruments that have significantly better performance than the IUT. Selecting the right calibration provider is key.

Notes d’application 2015-04-24

Layout of Calibration Certificates And Measurement Reports - Application Note
This document explains what you can expect to see on your Calibration Certificates, including how measurement results are reported and when adjustments are done.

Notes d’application 2014-03-20