Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

1-14 из 14

Упорядочить:
What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.

FAQ 2019-08-28

Is there a 3D model of the InfiniiVision 2000/3000/3000T X-Series oscilloscopes?
Yes, see the IGES, SAP, and Step format file downloads.

FAQ 2015-02-18

Can I manually set the sample rate on my InfiniiVision oscilloscope?
Although the sample rate cannot be directly set on any InfiniiVision oscilloscope, it can be set indirectly by adjusting the oscilloscopes time per division setting.

FAQ 2012-10-30

What is the difference between the Auto and Normal trigger modes on InfiniiVision oscilloscopes?
In auto trigger mode, the trigger will be forced if the specified conditions are not met. In normal trigger mode, the trigger will never be forced and a trigger will only occur if the specified conditions are met.

FAQ 2012-10-17

All IntuiLink Tools for Keysight Oscilloscopes
Supported Models: Infiniium Series, 1000 Series, 2000 X-Series, 3000 X-Series, 5000 Series, 6000 Series, 7000 Series, and 54600 Series Oscilloscopes

FAQ 2012-09-26

How do I establish a peer-to-peer connection between my PC and an InfiniiVision 5000/6000/7000 Series oscilloscope?
There are two methods ...

FAQ 2012-03-27

How can I retrieve a license key or password for an oscilloscope or logic analyzer software option that I have previously purchased?
If you have your order number and certificate number, you can obtain the license key for your product at ...

FAQ 2011-10-23

InfiniiVision 2000/3000 X-Series Oscilloscopes Frequently Asked Questions
Frequently asked questions and answers about the Keysight InfiniiVision 2000/3000 X-Series oscilloscopes.

FAQ 2011-07-07

PDF PDF 194 KB
Do the InfiniiVision Series oscilloscopes provide the ability to switch off the Auto Scale feature?
Not on the front panel, but you can do it with remote programming commands.

FAQ 2011-03-14

Can the 6000 Series oscilloscopes make floating measurements?
Like most other digitizing oscilloscopes, the new 6000 Series is not designed to offer floating measurement by itself. With 6000 Series you can make floating or differential measurements using a differential probe.

FAQ 2010-09-20

How can I password protect my InfiniiVisoni scope on the LAN?
Select Configure Network, then select Modify Configuration.

FAQ 2009-04-18

Do the mean, min, and max values of the InfiniiVision oscilloscopes measurement statistics refer to one signal on the screen or all previously capt...
They refer to the "Count" number of captured waveforms ...

FAQ 2009-03-30

Can I automatically position the Y1 and Y2 cursors to the voltage values at X1 and X2?
Yes, using SCPI remote programming commands, follow these steps...

FAQ 2008-09-30

How often should I send in my oscilloscope for calibration?
Please consult your instrument's Service Guide or contact your local Keysight service center.

FAQ 2006-12-04