이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

1-25 / 25

정렬방식:
What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.

FAQ 2019-08-28

신호 및 스펙트럼 분석기 벤치탑/모듈러/핸드형 펌웨어 업데이트 센터
벤치탑 및 핸드형 모델의 신호 및 스펙트럼 분석기용 펌웨어 또는 소프트웨어 최신 버전 액세스.

FAQ 2019-07-11

How do I update my X-Series Signal Analyzer Benchtop Software
Software updates for the X-Series Signal Analyzers Benchtop (PXA/MXA/EXA/CXA/MXE/ PXE)

FAQ 2019-05-14

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced FDD?
The X-Series upgrade path to LTE-Advanced FDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

만약 Windows XP를 계속 사용한다면, 앞으로 오류수정 서비스를 받을 수 있을까요?
네. Keysight는 서비스 지원종료되기 전까지는 마지막으로 판매된 Windows XP 까지 유지보수 되도록 할 것입니다.

FAQ 2016-07-05

Keysight는 Windows® XP 옵션 업그레이드 판매를 계속 할 것인가요?
네. Keysight는 Windows® XP 옵션판매에 대해 종료할 계획이 없습니다.

FAQ 2016-07-04

몇몇 기능들은 오직 Windows 7에서만 지원이 될 예정인가요?
네. 새롭게 나올 기능들은 Windows 7 장비에서만 지원이 될 것으로 예상됩니다.

FAQ 2016-07-04

Does M9290A CXA-m PXIe Signal Analyzer support sweep mode for spectrum analysis?
Yes, the M9290A supports both sweep and FFT mode for spectrum analysis.

FAQ 2014-09-11

How do I update the operating system in an N9038A MXE EMI receiver from Windows XP to Windows 7?
PC4 (Dual-Core High Performance Processor) 및 W7X (Window 7 OS) Option을 구매하시면 Window 7으로 upgrade 가능합니다.

FAQ 2014-08-25

89600 VSA 의 어떤 버전이 Windows7 을 지원합니까?
A.12.xx 버전 이상의 모든 89601B는 Windows7을 지원합니다.

FAQ 2014-08-25

How does the Microsoft end of support for Windows XP affect my N9030A, N9020A and N9010A?
As of April 8, 2014 Microsoft has ceased supporting the Windows XP operating system. This document will help you answer some important questions.

FAQ 2014-04-22

How does the Microsoft end of support for Windows XP affect my N9038A?
These documents will help you with answers to important questions.

FAQ 2014-04-14

How long will Keysight support Windows XP Professional for Embedded Systems?
Windows XP will be supported until March 1, 2015.

FAQ 2014-01-30

Why is Keysight delivering OS upgrades on the Option SSD or Option PC6/PC7 processor?
Keysight’s licensing agreement prevents us from selling the operating system independent of physical hardware.

FAQ 2013-04-25

Is the firmware revision A.12.xx installer the same for both Windows XP and Windows 7?
Firmware revision A.12.xx installer for Windows XP is a separate file than the firmware revision A.12.xx installer for Windows 7. Both are available on the Download button for the instrument software.

FAQ 2013-04-25

What if I need secure scripts to utilize Windows 7 within my secure measurement lab?
Keysight will work with you to evaluate scripts we have developed and successfully deployed in other secure measurement labs.

FAQ 2013-04-25

How can an installed base customer with Windows XP Professional for Embedded Systems upgrade to Windows Embedded Standard 7?
For the PC4/PC5 processor, the upgrade is via the software kit on Option SSD. For older CPUs, the CPU hardware must first be upgraded to PC4/PC5.

FAQ 2013-04-25

Will Windows 7 work on my existing processor?
There is a minimum configuration/vintage of processors which are compatible with Windows 7 and these are denoted as PC4 and PC5 in the show system screen on your instrument

FAQ 2013-04-25

How do I know what operating system my instrument will have?
Your quote and order will indicate the operating system.

FAQ 2013-04-25

Will I be able to get all future minor enhancements if I remain on Windows XP?
When we stop selling Windows XP downgrades we will end enhancing Windows XP SW versions.

FAQ 2013-04-25

Can I use external mixing (Option EXM) with real-time?
Yes, you can use external mixing with real-time. The instrument software must A.14.54 or later.

FAQ 2013-02-07

Can I use noise floor extension (NFE) with real-time?
No, you cannot use noise floor extension with real-time.

FAQ 2013-02-07

X 시리즈(PXA/MXA/EXA/CXA) 신호 분석기에는 어떤 Anti-Virus 소프트웨어를 설치해야 합니까?
각 회사 내부 IT 부서에서 결정한 Anti-Virus 소프트웨어를 설치하십시요.

FAQ 2011-01-12

MXA/EXA 신호분석기에는 어떠한 연결 포트들이 있습니까?
.

FAQ 2009-09-11