Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

Уточнить список

убрать все фильтры

По теме

По типу содержания

По типу оборудования

1-25 из 28

Упорядочить:
Infiniium Oscilloscope Software
Infiniium oscilloscope software.

FAQ 2019-11-25

Is there a 3D model of the Infiniium 9000 Series oscilloscope?
Yes, see the Step format file download.

FAQ 2019-11-04

What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.

FAQ 2019-08-28

How do I downgrade my Infiniium oscilloscope from Windows 10 to Windows 7?
If you bought an Infiniium oscilloscope running Windows 10 and you want to run Windows 7 instead, this document explains how to do so.

FAQ 2017-12-14

Why is the segmented memory acquisition mode useful and which Infiniium oscilloscopes support it?
Segmented memory mode offers more efficient acquisition memory usage for storing waveforms with events of interest that are separated by long periods of time. All currently shipping Infiniiums and many older units support segmented memory.

FAQ 2013-09-18

Which Keysight oscilloscopes have a 10 MHz reference input/output?
6000 Series, 6000L Series, 7000A Series, 7000B Series, 9000 Series, 54850 Series (Output only), 80000A Series, 80000B Series, 90000A Series and 90000 X-Series

FAQ 2012-10-17

All IntuiLink Tools for Keysight Oscilloscopes
Supported Models: Infiniium Series, 1000 Series, 2000 X-Series, 3000 X-Series, 5000 Series, 6000 Series, 7000 Series, and 54600 Series Oscilloscopes

FAQ 2012-09-26

How do I get >8 bit vertical resolution on my Keysight real-time oscilloscope?
Most Keysight oscilloscopes give 8-bit vertical resolution at normal acquisition mode.

FAQ 2012-08-31

Why do the high-bandwidth 54850-series Infiniium scopes use a BNC connector?
The 54850-series Infiniium scopes use a "precision BNC" connector.

FAQ 2012-05-08

How do I establish a peer-to-peer connection between my PC and an InfiniiVision 5000/6000/7000 Series oscilloscope?
There are two methods ...

FAQ 2012-03-27

How can I retrieve a license key or password for an oscilloscope or logic analyzer software option that I have previously purchased?
If you have your order number and certificate number, you can obtain the license key for your product at ...

FAQ 2011-10-23

For the InfiniiMax probes, what effect does the "Signal being probed" setting have? Why do I have to specify single-ended or differential?
Infiniium scopes and InfiniiMax differential probe amplifiers have a unique method of applying DC offset which considers whether the signal being probed is single-ended or differential...

FAQ 2010-10-06

What replacement parts and accessories are available for the 113xA-series InfiniiMax probes?
The best place to find this information is in the most recent revision of the InfiniiMax Active Probes User´s Quick Start Guide.

FAQ 2010-06-07

Can I program a waveform captured by my oscilloscope into a Keysight arbitrary waveform generator?
Yes. The free IntuiLink Waveform Editor software will download waveform data from Keysight Infiniium, 6000 series, and 54600 series oscilloscopes and send the data to the a Keysight 33120A, 33210A, 33220A, or 33250A generator.

FAQ 2010-05-14

My InfiniiMax probe fails calibration or does not accurately pick up the cal signal when I use the E2655A test fixture. What could be wrong?
The first step in troubleshooting a failed probe calibration should be to compare the actual signal and the probed signal. If the probed signal does not track the actual signal well, it is most likely due to a poor connection.

FAQ 2010-03-09

How do I get the maximum available memory depth from my Infiniium oscilloscope?
The various Infiniium models offer between 32K and 128M points of memory per channel. The following guide shows you how to get the maximum available memory from your particular scope.

FAQ 2009-11-19

How do I put an Infiniium oscilloscope into XY mode?
All Infiniium models have a math function called "versus", which plots one channel or function versus another channel or function.

FAQ 2009-02-17

What digital probe cables and accessories are available for Keysight mixed-signal oscilloscopes (MSOs)?
The digital probe kit for all Keysight 6000-series and 54620/40-series MSOs is P/N 54620-61801. The digital probe kit for all 8000-series and 54830-series MSOs is P/N 54826-68701.

FAQ 2007-08-10

My Infiniium scope application is not running properly. Is there a way to reset it?
My Infiniium scope application is not running properly. Is there a way to reset it?

FAQ 2007-01-05

Why do I see more noise on my oscilloscope when a probe is connected?
When a probe is connected, the scope changes its attenuation setting so that it correctly displays the voltage coming from the probe.

FAQ 2006-12-04

When using TV trigger mode with a Keysight oscilloscope, can I trigger only on even or odd fields?
Yes. All current Keysight scopes with TV triggering are capable of exclusively triggering on odd or even fields.

FAQ 2006-12-04

How often should I send in my oscilloscope for calibration?
Please consult your instrument's Service Guide or contact your local Keysight service center.

FAQ 2006-12-04

Frequently Asked Questions N5433A and N5434A Keysight MSO FPGA Dynamic Probe for Altera
Keysight’s FPGA dynamic probe provides greater real-time measurement productivity for MSO- based validation of FPGAs and the surrounding system.

FAQ 2006-11-28

What is the amplitude accuracy of my oscilloscope?
When oscilloscope manufacturers specify vertical accuracy, they typically only mention bandwidth and DC accuracy. The bandwidth specification addresses the AC accuracy. Tighter AC accuracy specifications are very uncommon.

FAQ 2006-11-04

Can I automatically stop my Infiniium from acquiring new waveforms after a certain period of time or number of triggers?

FAQ 2004-11-18

1 2 Следующие