検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

1-25 / 108

並べ替え
InfiniiVisionオシロスコープ用自動計測サンプルプログラム(Excel VBA,Visual Basic,C#,VEE)
Excel VBA、Visual Basic、Visual C#を使ったオシロスコープの自動計測サンプルプログラムを紹介しています。

サンプル・プログラム 2018-07-01

Get Lister Data, VISA library, Python 3.5
This script is a reference and starting point for automating Lister data capture over USB.

サンプル・プログラム 2017-04-28

ZIP ZIP 4.21 KB
Get Waveform Data, VISA COM library, VBA
This sample program gets waveform data from the oscilloscope.

サンプル・プログラム 2017-04-28

ZIP ZIP 1.01 MB
Get Segmented Memory Time Tags and Measurement Results, VISA library, Python
This script figures out how many segments were acquired, flips through them, gathers the time tags and desired measurement results.

サンプル・プログラム 2017-04-28

ZIP ZIP 4.96 KB
Get Screen Image, VISA library, Python (2.7)
This script shows how to save a screen image from an InfiniiVision oscilloscope to a PC.

サンプル・プログラム 2017-04-28

ZIP ZIP 3.27 KB
Load Arbitrary Waveform Data into WaveGen, VISA library, Python
This example shows several methods for getting arbitrary waveform data into the waveform generator of a Keysight InfiniiVision X-Series oscilloscope. The oscilloscope must have the WaveGen license and support arbitrary waveforms.

サンプル・プログラム 2017-04-28

ZIP ZIP 6.08 KB
Get Segmented Memory Time Tags and Measurement Results, VISA COM library, VBA
This sample program assumes the oscilloscope has been set to capture N segments. The program lists the segment number and the relative time stamp of that segment. A Delay measurement is made between channels 1 and 2 within each segment and the measurement value from each segment is listed.

サンプル・プログラム 2017-04-28

ZIP ZIP 33.08 KB
Get InfiniiVision Oscilloscope Screen Image, LabVIEW
This sample program captures and saves a screen image from the InfiniiVilsion oscilloscope.

サンプル・プログラム 2017-04-28

ZIP ZIP 48.93 KB
Get Screen Image, VISA library, Python 3.5
This script shows how to save a screen image from an InfiniiVision oscilloscope to a PC.

サンプル・プログラム 2017-04-28

ZIP ZIP 2.32 KB
Save Multiple Waveforms to a Binary File with Averaging, VEE
This sample program saves multiple waveforms to a binary file with averaging.

サンプル・プログラム 2017-04-28

ZIP ZIP 4.06 KB
Get Waveform Data (Brute Force), VISA library, Python
This script shows how to pull the waveform data from the analog channels for already acquired data and save it to a computer. It shows how to determine which channels are on and have data, how much data, get the data into an array, scale data for each channel, and save/recall it to/from disk in both csv and Python Numpy formats.

サンプル・プログラム 2017-04-28

ZIP ZIP 13.62 KB
Get InfiniiVision X-Series Oscilloscope Screen Image, LabVIEW
This sample program captures and saves a screen image from the InfiniiVilsion X-Series oscilloscope.

サンプル・プログラム 2017-04-28

ZIP ZIP 65.53 KB
Get Waveform Data, VEE
This sample program gets waveform data from the oscilloscope.

サンプル・プログラム 2017-04-28

ZIP ZIP 4.08 KB
Get Segmented Memory Time Tags, Waveforms, and Measurement Results, VISA library, Python
This script can get waveforms and measurements from analog channels for segmented memory already acquired on an InfiniiVision oscillocope. It can also get time tags and produce an averaged segment for each analog channel.

サンプル・プログラム 2017-04-28

ZIP ZIP 8.17 KB
Get *IDN? Query, Screen Image, and Waveform Data Results, VISA COM library, VBA
This sample program performs three different tasks: 1) sends a *IDN? query to the instrument and reads back the ID string, 2) captures and saves a screen image from the oscilloscope, and 3) gets the oscilloscope's waveform data from channels 1 and 2.

サンプル・プログラム 2017-04-28

ZIP ZIP 1.30 MB
Acquisition Synchronization, Two Simple Methods, VISA library, Python
This script shows the two best synchronization methods for all InfiniiVision and InfiniiVision X-Series oscilloscopes. Benefits and drawbacks of each method are described.

サンプル・プログラム 2017-04-28

ZIP ZIP 338.73 KB
Get Waveform Data, LabVIEW
This sample program gets waveform data from the oscilloscope.

サンプル・プログラム 2017-04-28

ZIP ZIP 69.15 KB
Get Screen Image and Waveform Data and Save to USB Thumb Drive, VISA library, Python
This script shows how to save a screen image and waveform data to a USB stick, with error checking.

サンプル・プログラム 2017-04-28

ZIP ZIP 5.50 KB
Get *IDN? Query Results, VISA COM library, C#
This sample program sends a *IDN? SCPI query to an instrument to get its identification string. The result is displayed on a MS Windows Console.

サンプル・プログラム 2017-04-28

ZIP ZIP 41.79 KB
Save and Recall Setups, VISA library, Python
This script shows how to query the oscilloscope setup, save it to disk, recall it form disk, and use it to set up the oscilloscope again. This is also shown using the *LRN? query and with just trigger setups.

サンプル・プログラム 2017-04-28

ZIP ZIP 4.39 KB
Acquisition Synchronization, Two Simple Methods, MATLAB
This script shows how to properly initialize a Keysight InfiniiVision or InfiniiVision X-Series oscilloscope and synchronize an acquisition using the blocking :DIGitize command.

サンプル・プログラム 2017-04-28

ZIP ZIP 328.53 KB
Get Waveform Data (Elegant), VISA library, Python
This script shows how to pull the waveform data from the analog channels for already acquired data and save it to a computer. It shows how to determine which channels are on and have data, how much data, get the data into an array, scale data for each channel, and save/recall it to/from disk in both csv and Python Numpy formats.

サンプル・プログラム 2017-04-28

ZIP ZIP 13.93 KB
Python Reference Application for the N8844A Data Analytics Web Service's Programmatic Interface
This example program is for the N8844A Data Analytics Web Service's programmatic interface using the Python language.

サンプル・プログラム 2017-02-17

ZIP ZIP 5.01 KB
C# Reference Application for the N8844A Data Analytics Web Service's Programmatic Interface
This example program is for the N8844A Data Analytics Web Service's programmatic interface using the C# language.

サンプル・プログラム 2017-02-09

ZIP ZIP 3.01 MB
Java Reference Application for the N8844A Data Analytics Web Service's Programmatic Interface
This example program is for the N8844A Data Analytics Web Service's programmatic interface using the Java language.

サンプル・プログラム 2017-01-31

ZIP ZIP 13.64 KB

1 2 3 4 5 次へ