您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

1-18 / 18

排序:
What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.

FAQ 2019-08-28

Is calibration included in the 86100DU-WN7 Windows 7 upgrade?
86100DU-WN7 is a return to service center upgrade and does include calibration, in addition to a certificate of calibration and data.

FAQ 2017-06-28

Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

Does PC link 2.51 support Windows 7, 64 bits?
No

FAQ 2014-04-17

How do I transfer waveforms, screen images, and measurements from my InfiniiVision oscilloscope to a PC using IntuiLink Data Capture?
Keysight’s free IntuiLink Data Capture software provides an easy way to transfer deep-memory waveform data, screen images, and measurements from your oscilloscope to your PC via the USB, LAN, or GPIB interface.

FAQ 2011-06-06

我要如何將 Keysight 5000/6000/7000 系列 InfiniiVision 示波器上的螢幕畫面,儲存到 USB 儲存裝置上?
下列指示假設您的示波器使用系統軟體 05.00 或以上版本 (如需得知示波器的版本,請參見 公用程式 (Utility) | 服務 (Service) | 關於示波器 (About Oscilloscope) -> 系統版本 (System version) )。

FAQ 2010-09-15

How can I prevent a loading delay when using the Measurement Manager with Microsoft® .NET 2.0 on a computer that is connected to a LAN…
To prevent a loading delay when using the Measurement Manager (AMM) with Microsoft® .NET 2.0, follow the instructions below:….

FAQ 2010-08-09

When will Keysight USB modular instruments and USB Modular DAQs supports Windows 7?
For 32 bit Windows 7, the supportability of modular instruments and DAQs will happen...

FAQ 2010-07-18

I have purchased the Segmented Memory option, N5454A, for my InfiniiVision oscilloscope. However, I can’t find the feature in the menus. What can I...
You need to upgrade your oscilloscope to the latest firmware...

FAQ 2010-07-02

Can I use the Quick Print button to quickly save my waveforms into the USB thumbdrive?
Yes, but with software version 5.10 and above you have to enable the feature...

FAQ 2009-08-17

Does the Measurement Manager (AMM) run on Window Vista operating system?
Yes. The Measurement Manager (AMM) rev. 1.8.3.0 and above will able to run on Windows Vista ...

FAQ 2009-06-10

Does the Keysight Measurement Manager (AMM) support regional language settings other than English (US)?
Yes, the Keysight Measurement Manager (AMM) supports regional language settings other than English (US)….

FAQ 2009-01-12

是否能夠儲存先前的 TDR 量測波形,然後載入該波形,並與目前的 TDR 量測波形做比較?
是否能夠儲存先前的 TDR 量測波形,然後載入該波形,並與目前的 TDR 量測波形做比較?

FAQ 2008-08-03

是否可針對已儲存的波形進行量測?
是否可針對已儲存的波形進行量測?

FAQ 2008-08-03

是否能夠儲存多重 TDR 軌跡,然後在示波器上將其顯示為波形,並與目前的量測波形做比較?
可以將多重 TDR 軌跡儲存為內部格式,以供未來參考……

FAQ 2008-08-03

How do I update the Scope Connect software and 3000 Series oscilloscope firmware?
Follow these instructions.

FAQ 2007-04-26

我的 Infiniium 示波器應用程式運作不正常。如何重新設定?
詳情請參閱內文

FAQ 2005-04-20

Keysight Infiniium Oscilloscopes: Does the Keysight Infiniium Oscilloscope Work With VEE?

FAQ 2003-08-01