検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

1-25 / 33

並べ替え
FlexDCA: What Licenses Do I Have, And What Features Do They Enable?
FlexDCA: What Licenses Do I Have, And What Features Do They Enable?

FAQ 2018-12-10

What Information Should I Collect From FlexDCA Before Asking Keysight For Help?
What Information Should I Collect From FlexDCA Before Asking Keysight For Help?

FAQ 2018-12-10

Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

Why are USB modular instruments (U2700 Series) and USB DAQ modules (U2300, U2500, U2600 Series) not detectable by the E5810B?
Establish the connection between the USB modular Instrument and the PC directly, and then disconnect the device from the PC (while it’s still powered-on), and connect to E5810B.

FAQ 2014-04-17

[操作方法] PCから、オシロをWebブラウザ/LAN経由で遠隔コントロールするには、どのようにすれば良いでしょうか?
弊社のオシロスコープ(InfiniiVision、Infiniium)には、Webコントロール機能が内蔵されており、遠隔地からLANを経由してリモート制御する事が可能になっています。

FAQ 2013-10-28

86100C/86100Dデジタル・コミュニケーション・アナライザの消費電力の代表値は?
86100C/86100Dの代表的な測定の消費電力

FAQ 2012-09-25

What can I do if I fail to establish hardware connection after successfully installing Keysight USB modular instrument driver on a Win7 environment?
If you encountered the event mentioned above, follow the installation best practices steps below.

FAQ 2012-07-25

What can I do if the Keysight USB Modular Instrument driver installations failed to complete installation on a Windows 7 environment?
If you encountered the event mentioned above, follow the installation best practices steps below.

FAQ 2012-07-25

[仕様] 5485x/DSO80000/90000AシリーズのBNCコネクタは、高帯域でも使用できるのでしょうか?
5485x、DSO80000、DSO90000AシリーズInfiniiumオシロスコープは「プレシジョンBNC」コネクタを使用しています。

FAQ 2012-05-09

Why i can't find other languages help file setting in U160X A/B series HH oscilloscope?
In order to access to other language, please go to respective product support page in www.Keysight.com. Go to Driver & Software page, select Firmware Update.

FAQ 2011-09-12

Infiniimax電気プローブ(1130A/31A/32A/34A)は86100 DCAモジュールで使用できますか?
はい。N1022Aプローブ・アダプタを使用することにより、Infiniimaxプローブ(1130A/31A/32A/34A)を86100 DCAモジュールで使用できます。

FAQ 2011-07-23

[操作方法] ユーザ名とパスワードを入力せずにInfiniiumオシロスコープを使用するには?
デフォルト設定では、マシンに搭載されているWindows 95/98、Windows XPオペレーティング・システムはユーザ名とパスワードを使ってログインする必要があります。

FAQ 2010-10-06

VEE 9.0 has SCPI completion. How do I make my own SCPI command built-in with VEE?
Please refer to the attached Microsoft Word document for a step by step explanation...

FAQ 2009-11-12

I've written my own text format for SCPI in *.txt. How do I use these for SCPI completion within VEE 9.0. What tool should I use?
You can use the tool found within Keysight.com. Just search using the keyword "Keysight VEE SCPI...

FAQ 2009-11-12

U1600シリーズ・ハンドヘルド・オシロスコープ用のクイック・ヘルプ言語のダウンロード方法は?
U1600製品リファレンスCDから、希望する言語をダウンロードできます。以下の手順に従って、クイック・ヘルプ言語をダウンロードしてください。

FAQ 2009-05-03

Can you run DSO3000 Series oscilloscope Scope Connect software when logged in as a "Restricted user"?
No, you must be a "Standard user" or an "Administrator" ...

FAQ 2008-10-07

Do I need a J8130A in order to use the MSO6000 with option FRS?
Yes, the J8130A (VPT1000) is required in addition to order the option FRS on the MSO6000 in order to do FlexRay Measurements on the MSO6000. Without the VPT1000, there is no FlexRay functionality on the MSO6000. Keysight does provide an additional ...

FAQ 2008-02-19

If the J8130A must be purchased separately what are the required options to use it with the scope?
No extra options are required on the J8130A to run with the MSO6000. The plain J8130A product is sufficient. However, the J8130A has a few potential options that could be ordered if needed: -The option 001 allows the VPT1000 to be used as a Flex...

FAQ 2008-02-12

ロジック・アナライザにはどのようなプローブを使用できますか?
Keysightが提供するロジック・アナライザ・プローブには、以下の4種類の基本カテゴリがあります。...

FAQ 2007-06-01

InfiniiumオシロスコープのWebインタフェースに接続できません。どのようにトラブルシューティングしたらよいのでしょうか?
下記に、InfiniiumオシロスコープのWebイネーブル機能のトラブルシューティング時に有用な情報を示します。

FAQ 2005-07-19

16500B/16500Cシリーズの電源を投入してもシステムが起動しません。どうしたらいいのですか?
16500B/16500Cシリーズ本体に標準付属の System OS DiskのNo.1を使用して立ち上げて下さい。

FAQ 2005-06-15

Infiniiumオシロスコープにインストールされているオプションはどのようにすれば、わかりますか?
5483x/5x、DSO8xxxxのどのモデルの場合も、Help | About Infiniiumをクリックしてください。

FAQ 2005-05-15

InfiniiumのUSBポートを使用できますか? また、そのUSBポートはハイスピードに対応しますか?
Infiniiumのモデルによって異なりますが、USBポートを使用できる場合もあります。現在これを記載した時点ではUSBポート付きのInfiniiumオシロスコープはロースピードとフルスピードのみをサポートしています。

FAQ 2004-12-01

Which models of Infiniium scopes support the 1130-series InfiniiMax probes?
With the right software revision, any model of Infiniium scope will support the InfiniiMax probes ...

FAQ 2004-09-30

ユーザ名とパスワードを入力せずに1680/1690/16900シリーズ・ロジック・アナライザを使用するには?
デフォルト設定では、マシンに搭載されているWindows 2000およびWindows XPオペレーティング・システムはユーザ名とパスワードを使ってログインする必要があります。

FAQ 2004-07-13

1 2 次へ