这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

1-11 / 11

排序:
Can I operate 86107A over continuous frequency bands?
The 86107A can operate over the following continuous frequency range if the 86100A/B/C mainframe has firmware revision A04.10 or above.

FAQ 2013-12-12

86100C 和 86100D 数字通信分析仪的典型功耗是多少?
86100C 和 86100D 典型功耗测量

FAQ 2012-09-25

用于Infiniium示波器的1161A 10:1无源探头可使用何种等效电路?
以下是等效电路的简图。

FAQ 2011-06-07

When will Keysight USB modular instruments and USB Modular DAQs supports Windows 7?
For 32 bit Windows 7, the supportability of modular instruments and DAQs will happen...

FAQ 2010-07-18

Does the Measurement Manager (AMM) run on Window Vista operating system?
Yes. The Measurement Manager (AMM) rev. 1.8.3.0 and above will able to run on Windows Vista ...

FAQ 2009-06-10

Do the mean, min, and max values of the InfiniiVision oscilloscopes measurement statistics refer to one signal on the screen or all previously capt...
They refer to the "Count" number of captured waveforms ...

FAQ 2009-03-30

How can I access to the maximum memory depth (32M/16M) as stated in the U2701A/U2702A Modular Oscilloscope's data sheet?
You can see the effects of maximum memory depth 32/16 Mpts in zoom mode….

FAQ 2009-02-04

How do I calculate the dc vertical gain accuracy of a U2701A/U2702A USB Modular Oscilloscope?
The dc vertical gain accuracy of a U2701A/U2702A USB Modular Oscilloscope depends on the error values in the measured value....

FAQ 2009-02-04

Does the Keysight Measurement Manager (AMM) support regional language settings other than English (US)?
Yes, the Keysight Measurement Manager (AMM) supports regional language settings other than English (US)….

FAQ 2009-01-12

Why does the DC Gain Error formula in the DC Gain Accuracy procedure have factors of 0.60 and 0.75 in the DSO80000 Series Infiniiums but not the ot...
These factors are used in the DSO80000 Series Infiniiums because the DC gain is measured with input voltages that are less than full scale, but the spec is relative to a full scale input.

FAQ 2006-10-20

Can I use my Infiniium's USB ports and do they support Hi-speed communication?
Depending on the model of Infiniium you have, you may be able to use the USB ports.

FAQ 2004-11-18