Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

Уточнить список

убрать все фильтры

По теме

По типу содержания

По типу оборудования

51-75 из 414

Упорядочить:
What is the typical power consumption of the 86100C and 86100D Digital Communications Analyzer?
Typical measurements of 86100C and 86100D power consumption

FAQ 2012-09-25

How do I get >8 bit vertical resolution on my Keysight real-time oscilloscope?
Most Keysight oscilloscopes give 8-bit vertical resolution at normal acquisition mode.

FAQ 2012-08-31

What application software is available for 16900, 1680x, 1682x and 1680/1690 Series logic analyzers?
See the table for quickly seeing the application support available for Keysight U4000, 16900, 16800 and 1680/90 logic and protocol analyzers.

FAQ 2012-08-14

What can I do if I fail to establish hardware connection after successfully installing Keysight USB modular instrument driver on a Win7 environment?
If you encountered the event mentioned above, follow the installation best practices steps below.

FAQ 2012-07-25

What can I do if the Keysight USB Modular Instrument driver installations failed to complete installation on a Windows 7 environment?
If you encountered the event mentioned above, follow the installation best practices steps below.

FAQ 2012-07-25

How do I declassify or sanitize my 54800-series Infiniium oscilloscope?
Follow the procedure below to ensure that your oscilloscope no longer contains any user configurations or data.

FAQ 2012-05-09

Why do the high-bandwidth 54850-series Infiniium scopes use a BNC connector?
The 54850-series Infiniium scopes use a "precision BNC" connector.

FAQ 2012-05-08

Do the ENA provide a probe power connection for active probes?

FAQ 2012-04-17

How do I establish a peer-to-peer connection between my PC and an InfiniiVision 5000/6000/7000 Series oscilloscope?
There are two methods ...

FAQ 2012-03-27

Digital Channel Failures on MSO6000 Series and MSO7000 Series Oscilloscopes
A possible failure mechanism has been traced to the firmware on the oscillocopes ...

FAQ 2011-11-01

How can I retrieve a license key or password for an oscilloscope or logic analyzer software option that I have previously purchased?
If you have your order number and certificate number, you can obtain the license key for your product at ...

FAQ 2011-10-23

How can I find accessories for a Keysight product?
For instrument-specific accessories (such as probes for an oscilloscope), first go to the product page and then see the related accessories. For general-purpose accessories (such as rf & microwave test accessories, carts, and racks), go to the ...

FAQ 2011-10-07

Why i can't find other languages help file setting in U160X A/B series HH oscilloscope?
In order to access to other language, please go to respective product support page in www.Keysight.com. Go to Driver & Software page, select Firmware Update.

FAQ 2011-09-12

Can I use the electrical Infiniimax probes (1130A/31A/32A/34A) with the 86100 DCA modules?
Yes, the N1022A probe adapter allows the Infiniimax probes (1130A/31A/32A/34A) to be used with the 86100 DCA modules.

FAQ 2011-07-25

InfiniiVision 2000/3000 X-Series Oscilloscopes Frequently Asked Questions
Frequently asked questions and answers about the Keysight InfiniiVision 2000/3000 X-Series oscilloscopes.

FAQ 2011-07-07

PDF PDF 194 KB
What is the function of the "10 MHz REF" port on my 6000-series oscilloscope?
You can use this port as either an input for an external 10 MHz reference signal, or as an output for the internal reference signal.

FAQ 2011-06-22

What are the minimum and maximum pulse width trigger settings on a 6000 Series oscilloscope?

FAQ 2011-06-16

How do I transfer waveforms, screen images, and measurements from my InfiniiVision oscilloscope to a PC using IntuiLink Data Capture?
Keysight’s free IntuiLink Data Capture software provides an easy way to transfer deep-memory waveform data, screen images, and measurements from your oscilloscope to your PC via the USB, LAN, or GPIB interface.

FAQ 2011-06-06

How can I perform TDR measurements using the 86100D mainframe with the standard trigger option, 86100D-STR?
If you want to use two TDR modules in an 86100D with option STR then you either have to move the cable to the module that sends out the TDR pulses, or you have to use two cables (such as Keysight P/N 5062-6687) and a power divider (such as Keysight’s P/N 11636B) or power splitter (such as Keysight P/N 11667B). The common port should go into the trigger input.

FAQ 2011-04-25

Are the input channels on the U1602B and U1604B Handheld Oscilloscopes isolated?
No, both scope channels (channel 1 and channel 2) on the U1602B and U1604B Handheld Oscilloscopes are not isolated.

FAQ 2011-03-31

Can I upgrade to option 001(Host USB interface) for the U1600B Series Handheld Oscilloscopes after purchase?
No, you cannot upgrade to option 001 for the U1600B Series Handheld Oscilloscopes after purchase. This option has to be specified when placing an order as it cannot be retrofitted on completed or shipped units.

FAQ 2011-03-22

Do the InfiniiVision Series oscilloscopes provide the ability to switch off the Auto Scale feature?
Not on the front panel, but you can do it with remote programming commands.

FAQ 2011-03-14

Do the 1000 Series oscilloscopes provide the ability to switch off the Auto Scale feature?
Not on the front panel, but you can do it with remote programming commands.

FAQ 2011-03-14

Can U1602A/B and U1604A/B measure capacitance of 0.13nF?
Based on the datasheet, for 0.13nF, it falls in the range of 60nF. To calculate the range of fluctuation of the reading,…

FAQ 2010-12-20

What is the best way to ensure simultaneous triggering of multiple units of modular products?
Using the cardcage, U2781A is the best way of ensuring simultaneous triggering of multiple units

FAQ 2010-12-20

Назад 1 2 3 4 5 6 7 8 9 10 ... Следующие