이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

상세 분류

상세분류 제거

주제별

분야별 검색결과

제품 카테고리별

1-25 / 418

정렬방식:
What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.

FAQ 2020-05-22

Which printers are supported by the InfiniiVision oscilloscopes?
Here is a list of tested printers and other printers that are likely to work...

FAQ 2020-03-02

Is there a 3D model of the InfiniiVision DSOX1202A/G and EDUX1052A/G oscilloscopes?
Yes, see the IGES, SAP, Step, and PKG format file downloads.

FAQ 2020-03-02

Why the waveform signal does not intersect at the mid-section when the time/division scale is below 10ns in the KMM/BenchVue software for U2701/2A?
This is due to the hardware limitation.

FAQ 2020-02-12

Is there a 3D model of the InfiniiVision DSOX1204A/G oscilloscopes?
Yes, see the IGES, SAP, Step, and PKG format file downloads.

FAQ 2020-01-24

Is there a 3D model of the InfiniiVision 1000 X-Series oscilloscopes?
Yes, see the IGES, SAP, Step, and PKG format file downloads.

FAQ 2020-01-24

Is there a 3D model of the Infiniium 9000 Series oscilloscope?
Yes, see the Step format file download.

FAQ 2019-11-04

Are there 3D models of the Infiniium UXR-Series oscilloscopes?
Yes, see the Step format file downloads.

FAQ 2019-02-19

FlexDCA: What Licenses Do I Have, And What Features Do They Enable?
FlexDCA: What Licenses Do I Have, And What Features Do They Enable?

FAQ 2018-12-10

What Information Should I Collect From FlexDCA Before Asking Keysight For Help?
What Information Should I Collect From FlexDCA Before Asking Keysight For Help?

FAQ 2018-12-10

Is there a 3D model of the P9241A USB oscilloscopes?
Yes, see the IGES, Step, and PKG format file downloads.

FAQ 2018-09-21

How do I downgrade my Infiniium oscilloscope from Windows 10 to Windows 7?
If you bought an Infiniium oscilloscope running Windows 10 and you want to run Windows 7 instead, this document explains how to do so.

FAQ 2017-12-14

Is calibration included in the 86100DU-WN7 Windows 7 upgrade?
86100DU-WN7 is a return to service center upgrade and does include calibration, in addition to a certificate of calibration and data.

FAQ 2017-06-28

Is there a 3D model of the InfiniiVision 4000 X-Series oscilloscopes?
Yes, see the IGES, SAP, Step, and PKG format file downloads.

FAQ 2017-05-05

Is there a 3D model of the M924xA PXIe modular oscilloscopes?
Yes, see the IGES, SAP, Step, EASM, PKG, and PDF format file downloads.

FAQ 2017-03-23

XY Display Mode Example
The XY time mode converts the oscilloscope from a volts-versus-time display to a volts-versus-volts display using two input channels.

FAQ 2017-02-24

가장 저렴한 오실로스코프를 찾으십니까?
키사이트 1000 X-시리즈 오실로스코프는 믿을 수 없을 정도로 저렴한 가격대에 전문가급 기능성을 지원합니다.

FAQ 2017-02-07

Is there a 3D model of the Infiniium V-Series oscilloscopes?
Yes, see the Step format file downloads.

FAQ 2017-01-25

Infiniium Oscilloscope HDD/SDD in Secure Environments
This FAQ talks about how to deal with Infiniium oscilloscope HDD/SDD in secure environments if you need to send oscilloscopes in for calibration.

FAQ 2016-09-26

Is there a 3D model of the InfiniiVision 6000L Series oscilloscopes?
Yes, see the IGES, SAP, and Step format file downloads.

FAQ 2016-07-18

오실로스코프를 PC처럼 사용 관련
오실로스코프를 PC 로 활용 가능한지 여부

FAQ 2016-07-05

인피니엄 오실로스코프 프로브와 6000시리즈용과의 환 여부
프로브 호환 관련

FAQ 2016-07-05

오실로스코프 뒷면의 GND 처리
오실로스코프 뒷면의 GND 와 실내의 Earth 접지와 연결이 필요한지요?

FAQ 2016-07-05

Which printers are supported by the handheld oscilloscopes?
Keysight handheld oscilloscopes support PCL6, 5e,5c and Postscript level 3 emulation printer command languages.

FAQ 2015-11-09

고객이 6000L 스코프를 MSO 옵션으로 주문이 가능한가요?
그렇습니다. 고객이 DSO6014L(100MHz DSO)를 위한 MSO 업그레이드 키트 N2914A 또는 DSO6054L/6104L을 위한 MSO 업그레이드 키트인 N2915A로 주문이 가능합니다. 이 두 가지 옵션은 고객이 직접 설치하는 옵션입니다.

FAQ 2015-04-20

1 2 3 4 5 6 7 8 9 10 ... 다음