Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discutez avec un expert

Support technique

Mesure Electronique

Support by Product Model Number:

1-15 sur 15

Tri:
Infiniium Advanced Remote Collaboration Surpasses In-Person Test
Geographically diverse design teams, increasing technical complexity, and limited equipment assets demand dramatically higher bench test efficiency and effectiveness. Only a completely reimagined test workflow, supported by advanced remote collaboration software can deliver this.

Étude de cas 2020-05-13

Pushing the Boundaries to Achieve Ultra-broadband Communications at True Terahertz Frequencies
See how researchers at the University at Buffalo achieved the first ever system to transmit and receive communications at 1.025 terahertz.

Bulletin d'information 2018-12-10

PDF PDF 23 KB
The Difference Between Digitizers and Oscilloscopes for Wideband Measurements

Article 2017-09-20

Full Function Oscilloscopes for ATE Systems

Article 2017-09-20

Make accurate and fast design decisions with data analytics
Make accurate and fast design decisions with data analytics

Article 2017-08-25

2015 Global Digital Oscilloscopes Growth Award
Understand how Frost & Sullivan evaluates and decides on the winner for this award

Article 2016-01-05

PDF PDF 1.06 MB
Jitter Analysis: The Dual-Dirac Model, RJ/DJ, and Q-Scale - White Paper
This paper provides a complete description of the dual-Dirac model, how it is used in technology standards and a summary of how it is applied on different types of test equipment.

Article 2014-06-14

PDF PDF 515 KB
2014 Global PXI Instrumentation Growth Excellence Leadership Award - Article Reprint
Frost & Sullivan honors Keysight as a growth leader in the PXI modular instrumentation market in 2014.

Article 2014-05-22

PDF PDF 598 KB
Digital Oscilloscope
What is a digital oscilloscope? See the main characteristics of digital oscilloscopes.

Article 2013-07-25

What is waveform update rate and why does it matter?
Explore this often overlooked oscilloscope performance specification to learn how to determine an oscilloscope’s update rate and what a fast update rate can mean for you.

Article 2013-06-03

The Fifth Harmonic: Tradeoffs Between Sampling and Real-Time Oscilloscopes
When determining the required system bandwidth some vendors will use a “fifth harmonic” rule of thumb; however it is important to understand typical conditions at the receiver to accurately determine the amount of bandwidth you will need.

Article 2009-01-19

Eye-Diagram Analysis Speeds DDR SDRAM Validation

Article 2009-01-06

Validating the Physical and Protocol Layers in DDR Memory Interfaces

Article 2009-01-06

Is the 5th Harmonic Still Useful for Predicting Data Signal Bandwidth?
This article, published in High Frequency Electronics, compares using the 5th harmonic to using the system rise/fall times to determine the required bandwidth for your system. The article begins on page 18.

Article 2009-01-01

Simplify DDR Validation with SI Methods

Article 2008-01-06