Here’s the page we think you wanted. See search results instead:

 

Discutez avec un expert

Technical Support

Electronic Measurement

Support by Product Model Number:

Refine the List

retirer tout le raffinement

By Type of Content

Par catégorie de produit

1-19 of 19

Sort:
Playback of M9392A Recorded Files on the M9381A PXI Vector Signal Generator
Example program for the M9391A PXI Vector Signal Generator. This program will load waveforms captured by the M9392A PXI Vector Signal Analyzer into the M9381A PXI Vector Signal Generator for playback. A document will describe the procedure and the programming instructions for loading and playing back of these waveform files.

Programming Example 2012-11-06

ZIP ZIP 319.72 KB
Direct I/O: Set Up Frequency Sweep With SRQ On Completion
Configure the signal generator to execute a frequency sweep. On completion of the frequency sweep an SRQ interrupt is generated.

Programming Example 2005-04-01

Direct I/O: Download Waveform and Save to Excel (Read Me)
Code sample documentation.

Programming Example 2005-04-01

Direct I/O: Control Power, Frequency, FM Modulation - Save Settings (Read Me)
Code sample documentation.

Programming Example 2005-04-01

Direct I/O: Download Waveform and Save to Excel
Mathematically construct a complex baseband signal and downloaded to the arbitrary waveform generator within the ESG-C/PSG vector signal generator. On completion of signal download, the I and Q vectors are saved to an Excel file.

Programming Example 2005-04-01

Direct I/O: Set Up Frequency Sweep With SRQ On Completion & Save to Excel (Read Me)
Code sample documentation.

Programming Example 2005-04-01

Direct I/O: Download Waveform
Mathematically construct a complex baseband signal and downloaded to the arbitrary waveform generator within the ESG-C/PSG vector signal generator.

Programming Example 2005-04-01

Direct I/O: Control Power, Frequency, FM Modulation - Save Settings
Control the signal generator's power, frequency, and FM modulation, and store the settings.

Programming Example 2005-04-01

Direct I/O: Control Power, Frequency, and FM Modulation (Read Me)
Code sample documentation.

Programming Example 2005-04-01

Direct I/O: Set Up Frequency Sweep With SRQ On Completion & Save to Excel
Configure the signal generator to execute a frequency sweep. On completion of the frequency sweep an SRQ interrupt is generated. The data is stored to Excel.

Programming Example 2005-04-01

Direct I/O: Control Power, Frequency, and FM Modulation
Control the signal generator's power, frequency, and FM modulation.

Programming Example 2005-04-01

Direct I/O: Set Up Frequency Sweep With SRQ On Completion (Read Me)
Code sample documentation.

Programming Example 2005-04-01

Direct I/O: Download Waveform (Read Me)
Code sample documentation.

Programming Example 2005-04-01

E8257C Programming over LAN Using To/From Socket
This VEE Pro program demonstrates how to communicate to an E8257C over the LAN using To/From Sockets. This contributed application is supplied as is, with no warranty or support.

Programming Example 2004-05-01

Upload Instrument State using *LRN (Read Me)
Code sample documentation.

Programming Example 2004-05-01

E8257C Programming over LAN Using To/From Socket (Read Me)
Code sample documentation.

Programming Example 2004-05-01

Upload Instrument State using *LRN
This VEE Pro program demonstrates how to upload an instrument state using the *LRN command and download the state again. This contributed application is supplied as is, with no warranty or support.

Programming Example 2004-05-01

Upload Instrument State using *LRN (Read Me)
Code sample documentation.

Programming Example 2004-05-01

E8257C Programming over LAN Using To/From Socket (Read Me)
Code sample documentation.

Programming Example 2004-05-01