这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

1-20 / 20

排序:
MATLAB M9384B Measurement Guide Programming Examples
MATLAB M9384B Measurement Guide Programming Examples

编程实例 2019-09-10

Playback of M9392A Recorded Files on the M9381A PXI Vector Signal Generator
Example program for the M9391A PXI Vector Signal Generator. This program will load waveforms captured by the M9392A PXI Vector Signal Analyzer into the M9381A PXI Vector Signal Generator for playback. A document will describe the procedure and the programming instructions for loading and playing back of these waveform files.

编程实例 2012-11-06

ZIP ZIP 319.72 KB
Direct I/O: Set Up Frequency Sweep With SRQ On Completion & Save to Excel
Configure the signal generator to execute a frequency sweep. On completion of the frequency sweep an SRQ interrupt is generated. The data is stored to Excel.

编程实例 2005-04-01

Direct I/O: Set Up Frequency Sweep With SRQ On Completion (Read Me)
Code sample documentation.

编程实例 2005-04-01

Direct I/O: Download Waveform (Read Me)
Code sample documentation.

编程实例 2005-04-01

Direct I/O: Download Waveform and Save to Excel
Mathematically construct a complex baseband signal and downloaded to the arbitrary waveform generator within the ESG-C/PSG vector signal generator. On completion of signal download, the I and Q vectors are saved to an Excel file.

编程实例 2005-04-01

Direct I/O: Set Up Frequency Sweep With SRQ On Completion & Save to Excel (Read Me)
Code sample documentation.

编程实例 2005-04-01

Direct I/O: Control Power, Frequency, FM Modulation - Save Settings
Control the signal generator's power, frequency, and FM modulation, and store the settings.

编程实例 2005-04-01

Direct I/O: Download Waveform and Save to Excel (Read Me)
Code sample documentation.

编程实例 2005-04-01

Direct I/O: Control Power, Frequency, FM Modulation - Save Settings (Read Me)
Code sample documentation.

编程实例 2005-04-01

Direct I/O: Control Power, Frequency, and FM Modulation (Read Me)
Code sample documentation.

编程实例 2005-04-01

Direct I/O: Control Power, Frequency, and FM Modulation
Control the signal generator's power, frequency, and FM modulation.

编程实例 2005-04-01

Direct I/O: Set Up Frequency Sweep With SRQ On Completion
Configure the signal generator to execute a frequency sweep. On completion of the frequency sweep an SRQ interrupt is generated.

编程实例 2005-04-01

Direct I/O: Download Waveform
Mathematically construct a complex baseband signal and downloaded to the arbitrary waveform generator within the ESG-C/PSG vector signal generator.

编程实例 2005-04-01

E8257C Programming over LAN Using To/From Socket (Read Me)
Code sample documentation.

编程实例 2004-05-01

Upload Instrument State using *LRN (Read Me)
Code sample documentation.

编程实例 2004-05-01

E8257C Programming over LAN Using To/From Socket
This VEE Pro program demonstrates how to communicate to an E8257C over the LAN using To/From Sockets. This contributed application is supplied as is, with no warranty or support.

编程实例 2004-05-01

Upload Instrument State using *LRN
This VEE Pro program demonstrates how to upload an instrument state using the *LRN command and download the state again. This contributed application is supplied as is, with no warranty or support.

编程实例 2004-05-01

Upload Instrument State using *LRN (Read Me)
Code sample documentation.

编程实例 2004-05-01

E8257C Programming over LAN Using To/From Socket (Read Me)
Code sample documentation.

编程实例 2004-05-01