検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

1-17 / 17

並べ替え
How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced FDD?
The X-Series upgrade path to LTE-Advanced FDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

【VSA】【SG】RF信号をキャプチャして信号源で再生することはできますか?
はい。ベクトル・シグナル・アナライザを使用することで、RFキャプチャ信号を信号源から再生することが可能です。

FAQ 2016-02-03

Does the N7620 software support the LXI synthetic instruments?
Yes.

FAQ 2014-04-07

Can I use Signal Studio for pulse building with Windows® 7?
Windows 7 works with N7620B.

FAQ 2012-12-28

Can multiple software applications communicate with a single N6030A arbitrary waveform generator at the same time?
Only one software application can communicate with the N6030A at a time.

FAQ 2012-12-28

What is the OS (operating system) of the X-Series signal generators?
Windows® CE

FAQ 2012-04-30

Will a PCI-X slot work for the N5101A Baseband Studio PCI Card?
Yes, PCI-X should be backward compatible with conventional PCI 2.2.

FAQ 2010-09-08

What is the meaning of this statement from the data sheet: "The acoustic noise is louder than typical Keysight equipment."
The instrument has a set of fans to remove internally generated heat. These fans generate ...

FAQ 2010-05-07

If I already have an E4438C-406 Bluetooth® license, can I upgrade to N7606B Signal Studio Software Bluetooth® without any extra charges?
Yes, you can upgrade to the N7606B Signal Studio Software free of charge.

FAQ 2009-06-09

Why when using the parallel interleave mode and 1 clock per sample, the data seems to be clocked on the opposite clock edge than what the GUI state...
This is a known issue and has been noted for future consideration. The workaround is...

FAQ 2009-02-12

Are National Instruments software drivers available for Keysight signal generators?
Yes. LabView drivers are available from the National Instruments website for many current and discontinued Keysight signal generators.

FAQ 2009-01-12

Why is an incorrect version of Signal Studio N7613A, N7612B, and N7606B shown when I use the “Add or Remove Programs” window in “Control Panel” on ...
This Signal Studio version number discrepancy can be ignored, please proceed with your application removal. This error will be corrected with the next version roll.

FAQ 2008-12-02

Can I install Signal Studio license files on the ESG or MXG over GPIB?
No. Signal Studio licenses, perpetual, transportable and time-based cannot be installed using GPIB.

FAQ 2008-10-13

Why doesn't Signal Studio N76xxB software recognize a N76xxA license?
All N76xxB Signal Studio products should recognize the licenses of their equivalent N76xxA products...

FAQ 2008-02-25

I remotely changed my 8648X modulation from Pulse to AM, but the display still indicates 'PULSE'. Is the 8648X outputting an AM or PM modulation?
The AM modulation is activated now. The annotation can be corrected using a short program.

FAQ 2007-09-24

11759C Software in a DOS window

FAQ 2002-06-27