Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

Refine the List

remove all refinements

By Topic

By Type of Content

By Product Category

1-23 of 23

Sort:
When I use the 30-day trial license of the Signal Studio for WiMAX™, how can I check the number of days remaining on temporary license?
Press the front panel keys: Utility > Instrument Adjustments > Instrument Options > Waveform Licenses

FAQ 2013-01-28

What is a 30-day free trial license and how does it work?
The 30-day free trial period allows the user to try out our latest Signal Studio software products prior to purchase.

FAQ 2012-12-30

After the 30-day trial license is activated, can I suspend the trial period for future use?
No, the trial license is valid for 30 consecutive days, after which, you will have to purchase a permanent license to continue using the software.

FAQ 2012-12-28

Can I renew or extend the 30-day trial license after expiration?
After the trial license expires on an instrument, it cannot be renewed or extended.

FAQ 2012-12-28

How is the time remaining for a trial license tracked?
You can track the time remaining on the trial license from the front panel of the ESG/PSG by pressing Utility > Instrument Adjustments > Instrument Options > Waveform Licenses.

FAQ 2012-12-28

If I purchased a license for one signal generator, is that license transferable between signal generators?
Yes, transportable licenses are now available under the new Keysight licensing model.

FAQ 2012-12-28

For waveform 5-pack licenses, what alternatives are available for customers that require additional waveform evaluation time after the initial 30-d...

FAQ 2012-12-13

For waveform 5-pack licenses, can the customer download a waveform generated with the 30-day license?
Yes, if a waveform was created using the 30-day trial, it can be downloaded to any MXG/ESG with unused waveform 5-pack license slots.

FAQ 2012-12-11

Is there a 30-day trial license for this application?
Only selected Signal Studio software applications have the 30-day free trial license available, while others allow a free evaluation of the software interface only.

FAQ 2012-12-11

Do I have to upgrade my N7620A licenses?
You may want to upgrade your N7620A licenses to N7620B licenses so that they can be managed using the Keysight License Manager.

FAQ 2012-10-28

Will the N7620B software recognize my N7620A licenses?
The N7620B software recognizes all N7620A licenses except for the N8241A, N6030A, and N9330A external Arbs.

FAQ 2012-10-28

How do I manage my N7620A licenses?
The N7620A software allows you to view your original N7620A licenses.

FAQ 2012-10-28

How do I upgrade my N7620A licenses?
Contact the customer contact center at Keysight Technologies.

FAQ 2012-10-28

Why doesn't the Keysight License Manager connect to my ESG?
Your ESG needs firmware revision C.04.84 or above...

FAQ 2012-03-02

Is Signal Studio software licensed to the PC or signal generator?
Signal Studio software is licensed to the signal generator. More...

FAQ 2012-02-19

For waveform 5-pack licenses, can a customer purchase a perpetual or time-based Signal Studio license for one MXG/ESG to evaluate waveforms, and th...
Yes, any licensed MXG/ESG can be used to evaluate the waveforms – not just the MXG/ESG with the waveform 5-pack license option.

FAQ 2010-09-24

For waveform 5-pack licenses, is there any protection against accidentally overwriting a licensed waveform?
No, we recommend keeping a copy of the licensed waveform for archival purposes.

FAQ 2010-09-19

For waveform 5-pack licenses, since a waveform can be copied and renamed, is there protection from a user inadvertently licensing the same signal?
Yes, there is protection against using a license slot on a redundant signal. A unique identifier is associated and stored with each signal created by Signal Studio applications. It is this identifier that is licensed on the MXG or ESG signal gen...

FAQ 2010-09-08

For waveform 5-pack licenses, is there a grace-period where I can still revoke/replace a waveform once it has been licensed?
Once the waveform is licensed, that license is permanent and cannot be revoked or replaced.

FAQ 2010-09-08

For waveform 5-pack licenses, can a customer generate a waveform in Signal Studio software not connected to a MXG/ESG, export to a location on thei...
Yes, this method can be used when customers only want to tweak waveform parameters and not evaluate RF performance beforehand.

FAQ 2010-09-08

For waveform 5-pack licenses, once a waveform is licensed, can it be copied and stored for archival purposes?
Yes, a licensed waveform can be copied and renamed for archival purposes. Be aware that the waveform can still only played on the ESG or MXG to which it has been licensed.

FAQ 2010-09-08

For waveform 5-pack licenses, can the 30-day license attached to each waveform 5-pack license be activated whenever the customer wants –or– do the ...
The 30-day license for the evaluation of waveforms (Option D01) may be activated at anytime, although they must be used one at a time.

FAQ 2010-09-08

For waveform 5-pack licenses, is there a way to have password protection against licensing a 5-pack waveform to prevent someone from inadvertently ...
No, this will be considered as an enhancement request for future releases.

FAQ 2010-09-08