Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

126-150 of 361

Sort:
Can you change the attenuation on external I and Q individually on the N5182B MXG or N5172B EXG X-Series signal generators?
Yes, improved over the first-generation MXG.

FAQ 2012-04-30

Does Option 320 require that I have a pulse modulation option such as UNW on the X-Series signal generators?
Yes, Option 320, pulse train generator, requires Option UNW, narrow pulse modulation.

FAQ 2012-04-30

Can you bypass the internal reference chain with clean rubidium source on the X-Series signal generators?
The 10 MHz path is very clean and works with an external reference. The 1-50 MHz tunable path is noisier, see the data sheets for more details.

FAQ 2012-04-30

What does the S/N mode affect negatively on the X-Series signal generators? Why not leave it on all the time?
The harmonics can degrade with S/N mode on.

FAQ 2012-04-30

How can I generate TETRA and DECT signal for basic interference testing in many compliance test houses, which are bursted, just like the real standard
You can use PRAM to simulate spectrally correct signals for TETRA and DECT for bursted signals. See the X-Series User’s Guide for further information.

FAQ 2012-04-30

Can the user scale the output attenuation in IQ mod for N5182B MXG or N5172B EXG signal generator?
Yes, by using runtime scaling or IQ attenuator.

FAQ 2012-04-30

Do the new sources de-crypt waveforms in the same way as the legacy sources? Can we just use pre-existing waveforms?
Yes. First-generation MXG N5182A Signal Studio N76xxB waveforms will play in new sources. Exception will be N7613A Signal Studio for Fixed WiMAX which has the legacy N76xxA structure.

FAQ 2012-04-30

Is the pulse generator specification still the same with ALC On/Off on the X-Series signal generators?
Yes, it still cuts off at <2µs, however, open loop power accuracy has improved with or without power search being run. In most cases, you will see tenths of dB accuracy without running power search. This is a significant improvement over first-generation MXG.

FAQ 2012-04-30

Do we offer an external divider option to cover the heterodyne band phase noise performance on the X-Series signal generators?
We have the 70429A-K95 divider that can be used as an external divider for frequencies <250 MHz.

FAQ 2012-04-30

Can we upgrade N5181A or N5182A first-generation MXG to an N5181B or N5181B MXG X-Series signal generator?
No, there is not a hardware upgrade path from the first-generation MXG to MXG X-Series signal generator.

FAQ 2012-04-30

Will we be able to have more than 2 USB power sensors on the X-Series signal generators?
Yes, we are able to connect to 4.

FAQ 2012-04-30

Does Option UNY, enhanced low phase noise, require Option UNX, low phase noise,on the X-Series signal generators?
No, they are independent options with different levels of phase noise performance above 3 GHz.

FAQ 2012-04-30

Are the function generators all inside the MXG and EXG X-Series signal generators?
Yes, with Option 303, multifunction generator. See the data sheets for full capabilities.

FAQ 2012-04-30

Can I use custom digital modulation in ARB mode?
Yes, but the data will be a fixed, random pattern.

FAQ 2012-04-30

Will Options 430, 431 and 432 require Option 656 but not require Option 660 for ARB capability?
Yes, this is true for the N5182B MXG or N5172B EXG X-Series signal generators.

FAQ 2012-04-30

Is there a SCPI logger/history for commands sent to the X-Series signal generators?
Yes. Press Utility, I/O Config, SCPI Log/Help to find selections for this feature.

FAQ 2012-04-30

What are the plans to upgrade the N5102A DSIM, if I want it to go to 160 MHz BW on the N5182B MXG or N5172B EXG X-Series signal generators?
DSIM will be able to run up to 200MSa/sec.

FAQ 2012-04-30

Is the tuning speed the same as switching speed on the X-Series signal generators?
Yes, switching speed is the same as tuning speed.

FAQ 2012-04-30

What is the OS (operating system) of the X-Series signal generators?
Windows® CE

FAQ 2012-04-30

Can you master/slave MXG and EXG or must they all be the same model number?
You can master/slave first generation MXG N5182A with the N5182B MXG and N5172B EXG X-Series signal generators. The N5172B or N5182B must be the master.

FAQ 2012-04-30

Will the N5171B and N5172B EXG X-Series signal generator have an OCXO option for improved drift rate?
No

FAQ 2012-04-30

Does N5181B or N5182B MXG Option UNY/UNX have backward code compatibility with E8663D or 8663D signal generators?
Yes, the N5181B and N5182B MXG Option UNY/UNX has the same SCPI as PSG E8663D. E8663D is the replacement of 8663D with BWCC (backward code compatibility).

FAQ 2012-04-30

Using the E8267D PSG Vector Signal Generator in a System
Browse through this index of resources generated to ease your test system design challenge

FAQ 2012-03-30

I downloaded the Service Support Software for the E44xxB ESG-A/D from our website. The software is asking for a username and password. What is the...
The E44xxB ESG-A/D Service Support Software username and password are provided.

FAQ 2012-03-13

What is the polynomial to generate the PN9 sequence in the ESG-D Series RF signal generator?
We follow the ITU standards for PN sequences.

FAQ 2012-03-13

Previous 1 2 3 4 5 6 7 8 9 10 ... Next