Here’s the page we think you wanted. See search results instead:

 

Discutez avec un expert

Technical Support

Electronic Measurement

Support by Product Model Number:

251-275 of 832

Sort:
How do I optimize my cdmaOne ACPR measurement for the third offset (2.75 MHz offset, 1 MHz bandwidth) in the E4406A and PSA Series cdmaOne personal...
By changing the default number of FFTs segments to 5 and upgrading to the 14 bit digital IF (E4406A only) you can substantially improve your results.

FAQ 2012-05-28

How do I upgrade the E4406A VSA Series 321.4 MHz IF Output Option 300?
This option can be upgraded at your local Keysight Service Center. (Click on this FAQ for more information)

FAQ 2012-05-28

How do I upgrade the E4406A VSA Series Base Band I/Q Inputs Option B7C?
This option can be upgraded at your local Keysight Service Center. (Click on this FAQ for more information)

FAQ 2012-05-28

How do I perform WCDMA Power Control measurements on the E4406A or PSA Series Spectrum Analyzers?
Reverse link power control measurements can be made using the W-CDMA (Option BAF) power control measurement. Power control analysis on the downlink can be done in the Code Domain Power measurement using the Symbol Power vs. Time view.

FAQ 2012-05-28

Where can I find detailed specifications for the E4406A, PSA Series, ESA Series Spectrum Analyzers?
We publish both an abbreviated Data Sheet and complete Specifications Guide for these analyzers. You can find the complete specifications guide by looking under Manuals, Guides, and Notifications at the bottom of each product web page.

FAQ 2012-05-28

Does the E4406A or PSA Series Spectrum Analyzer provide GSM trigger to time zero (T0) timing in order to test Enhanced Observed Time Difference Tec...
Yes, the EDGE / GSM measurement personalities for the E4406A and PSA Series provide precise nanosecond timing between an external trigger and the training sequency T0 transition point. (click here for more details).

FAQ 2012-05-28

What cdmaOne (Option BAC) radio standards and band classes are supported by the E4406A and PSA Series for the ACP and Spur Close measurements?
Radio standards IS-95A, J-STD-008, IS-97D and IS-98D are supported. The following Band Classes are supported to comply with IS-97D and IS-98D requirements: Band Class 0 (800MHz), Band Class 1 (1900MHz), Band Class 3 (JTACS), Band Class 4 (Korean ...

FAQ 2012-05-28

How many options can be loaded into my E4406A with A.06.03 firmware at one time?
With a 48 MB flash memory board, you can fit up to seven measurement personalities. To determine what will fit, add up the memory sizes of the personalities that you want. If the total is less than 19,225 kB then they will fit.

FAQ 2012-05-28

What transit case do I order for my E4406A VSA Series Analyzer?
The dimensions of the E4406A are 426 mm x 177 mm x 452 mm (16 3/4 in x 7 in x 17 7/8 in) without the removable feet. There are two System II Cabinet Style Transit Cases that Keysight sells that best fit the E4406A. (Click here for more info)

FAQ 2012-05-28

How do I upgrade the E4406A VSA Series Firmware and Measurement Personalities?
The E4406A firmware and measurement personalites can be upgraded via the LAN or crossover cable. (Click on this FAQ for more information)

FAQ 2012-05-28

Can I get a temporary license key for my PSA Series, ESA Series, or EMC Series Analyzer?
No. At this time, we do not have temporary licenses. License keys for these instruments are generated based on the serial number, model number, and Host ID.

FAQ 2012-05-28

Do the E4406A and PSA Series support Complementary Cumulative Distribution Function (CCDF) measurement for cdmaOne?
Yes. The Power Statistics CCDF measurement is not in the cdmaOne personality (Option BAC), but it does come standard in the Basic measurement personality for E4406A and in the Spectrum Analysis mode for PSA and can be used to measure cdmaOne sign...

FAQ 2012-05-26

When attempting to make a Modulation Accuracy (Rho) measurement in the cdmaOne personality I get the error message, "Cannot correlate to input sign...
The Modulation Accuracy (Rho) measurement in the cdmaOne personality requires that you only have the pilot carrier turned on for your base station. If other code channels are turned on, you will get this error message.

FAQ 2012-05-26

For my Spectrum Analyzer, where can I find a conversion guide between IVI-COM and SCPI?
The linked spreadsheet provides a mapping between IVI-COM and SCPI

FAQ 2012-05-26

Do the E4406A, PSA Series and 89600 VSA Software report Peak Code Domain Error for W-CDMA and cdma2000?
Yes. The screen capture below shows a W-CDMA Modulation Accuracy measurement on the E4406A and PSA Series, and Peak Code Domain Error is reported in the results table.

FAQ 2012-05-26

Which Application Notes are Most Relevant to the PSA Series Spectrum Analyzer?
This page contains links to application notes that are relevant to PSA Series spectrum analyzers.

FAQ 2012-05-11

How do I make the signal list compare measurements made with the detectors used to different limit lines in my MXE EMI Receiver?
Meas Setup, Detectors (Measure)...

FAQ 2012-05-10

How do a take a sweep with both the Quasi-Peak and EMI Average detector at the same time with an MXE EMI Receiver?
Switch to EMI Receiver mode...

FAQ 2012-05-10

Why do I get a Meas Uncal message when I select either the Quasi-Peak or EMI Average detector for taking a full band sweep with the MXE EMI Receiver?
Sweeptime has reached its maximum. See complete FAQ for further details...

FAQ 2012-05-10

Why do I get the "Align 20 Hz to 3.6 GHz Required" message every time I turn my MXE on?
You don't. Wait for it to warm back up...

FAQ 2012-05-09

How often do I need to run the RF Preselector alignments in my MXE?
Every 14 days or when the temperature changes by 3 degrees...

FAQ 2012-05-09

Why do the high-bandwidth 54850-series Infiniium scopes use a BNC connector?
The 54850-series Infiniium scopes use a "precision BNC" connector.

FAQ 2012-05-08

How can I clear the memory on an 8566B, 8567A, or 8568B Spectrum Analyzer for security reasons?
See content for details on this subject....

FAQ 2012-03-29

Does 89600 VSA software (89601) support the Bluetooth® Difference Error Vector Magnitude (DEVM) test?
The 89601 Option AYA does not provide DEVM results for Bluetooth basic measurement. Keysight recommends using N9081A Bluetooth measurement application.

FAQ 2012-03-27

How do I transfer the screen image on my PSA, ESA, or EMC analyzer to a PC using Keysight VEE?
See content for complete details and an example program...

FAQ 2012-03-16

Previous ... 11 12 13 14 15 16 17 18 19 20 ... Next