이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

1-19 / 19

정렬방식:
Signal Integrity Analysis Series Part 1: Single-Port TDR, TDR/TDT, and 2-Port TDR - Application Note
This Application Note focuses on part 1: those which use a single-port TDR, those which use TDR/TDT, and those which use 2-port TDR.

어플리케이션 노트 2019-04-25

USB 2.0 Compliance Testing with Infiniium Oscilloscopes - Application Note
This Application Note discusses the solution for the USB 2.0 test suite. The Keysight solution is the only one-box solution that uses the official USB-IF scripts for precompliance ans compliance testing.

어플리케이션 노트 2019-01-29

An Overview of the Electrical Validation of 10BASE-T, 100BASE-TX, and 1000BASE-T - Application Note
The technology used in these ports, commonly known as “LAN” or “NIC” ports, is usually one of the 10BASE-T, 100BASE-TX, and 1000BASE-T standards or a combination of them.

어플리케이션 노트 2018-07-25

Probing a Midpoint of a Transmission Line that is Not Load Terminated - White Paper
With the advent of variable on die termination (i.e. ODT) many systems like low power double data rate memory (LPDDR) have the ability to either terminate a line in its characteristic impedance for high speed operation or terminate it with an open for lower speed operation. Many times there is a desire to probe the transmission line to monitor the signals on the line. When the transmission line is terminated in close to its characteristic impedance, the signals can be readily observed. However, if the line is terminated in an impedance that is not close to the characteristic impedance then it may not be possible to accurately measure the signals.

어플리케이션 노트 2018-07-03

PDF PDF 1.98 MB
How to Test USB Power Delivery (PD) Over Type-C - Application Note
USB Type-C power delivery creates possibilities for USB connected devices with higher, bi-directional power and power for non-USB devices with ALT mode. Learn more about verification/compliance.

어플리케이션 노트 2017-11-01

Decoding NFC-F Communication Based on Manchester-encoded ASK Modulation - Application Note
See step-by-step instructions on how to setup oscilloscopes to properly decode and trigger on NFC-F poller and listener communication for two specific cases.

어플리케이션 노트 2017-04-28

PDF PDF 2.27 MB
기본 오실로스코프 기초 - 어플리케이션 노트
이 어플리케이션 노트에서는 기본 오실로스코프 기초에 대해 개괄적으로 설명하며 오실로스코프의 정의와 사용 방법에 대해 배울 수 있습니다.

어플리케이션 노트 2017-04-25

저렴한 오실로스코프를 구매할 때 흔히 저지르는 5가지 실수 - 어플리케이션 노트(영어)
적은 예산으로 알맞은 오실로스코프를 선택하는 것은 특히 어려운 일입니다. 지불한 비용만큼의 가치를 보장하고 저비용 오실로스코프를 구매할 때 흔히 저지르는 5가지 실수를 예방하십시오.

어플리케이션 노트 2017-01-31

표준 오실로스코프 프로브에 익숙해지기 - 어플리케이션 노트
가장 정밀한 오실로스코프 측정을 위해 측정을 시작하기 전에 패시브 프로브 작동의 이론과 프로브 보상의 이점에 대해 알아보십시오.

어플리케이션 노트 2017-01-23

NFC Device Turn-on and Debug - Application Note
This app note shows how to use an InfiniiVision scope to trigger on NFC communication, demodulate the captured RF waveform, and perform various parametric measurements on the demodulated waveform.

어플리케이션 노트 2017-01-09

PDF PDF 1.88 MB
NFC-A and -B Sideband Measurements - Application Note
This app note shows how to use FFT peak search on an InfiniiVision X-Series scope to measure the amplitude (power levels) and frequency of NFC sidebands, subcarrier and carrier.

어플리케이션 노트 2017-01-09

PDF PDF 2.12 MB
How to Test USB Type-C Alt Mode and the Standards Running Across It - Application Note
This application note discusses how Alt mode works with power delivery circuitry to transmit/receive unique data signals/more power, so Type-C can be used for many USB & non-USB, device connections/control.

어플리케이션 노트 2016-04-29

Time Domain Reflectometry Theory - Application Note
When compared to other measurement techniques, time domain reflectometry provides a more intuitive and direct look at the DUT's characteristics.

어플리케이션 노트 2015-01-30

SATA II Drive TX/RX Testing & Cable SI Testing Using the 86100C DCA-J - Technical Overview
SATA II Drive Tx/Rx Testing & Cable SI Test using 86100C DCA-J. Product Note 86100-8

어플리케이션 노트 2014-08-02

PDF PDF 1.94 MB
등가 시간 샘플링 오실로스코프와 실시간 오실로스코프의 차이는?

어플리케이션 노트 2008-07-08

지터 스펙트럼 및 위상 노이즈 분석을 통한 지터 문제 해결
제품 노트

어플리케이션 노트 2007-05-09

키사이트 86100C DCA-J(PN 86100C-1)를 사용한 고정밀 지터 분석

어플리케이션 노트 2007-03-07

Signal Integrity Analysis Series Part 2: 4-Port TDR/VNA/PLTS - Application Note
This Application Note focuses on part 2: those which use a 4-port TDR/VNA/PLTS.

어플리케이션 노트 2007-02-21

PDF PDF 2.75 MB
Differential Time-Domain Reflectometry Module for a Digital Oscilloscope and Communications Analyzer
Differential Time-Domain Reflectometry Module for a Digital Oscilloscope and Communications Analyzer

어플리케이션 노트 2007-01-24