这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

1-7 / 7

排序:
S-Parameter File for the N5448B Cable Assembly
Inside this .zip file is an S-parameter file to be used with InfiniiSim to correct for the signal loss of the N5448B cable assembly.
先前版本

驱动程序 当前版本: n/a | 2018-10-17

S-Parameter File for the N2823A Cable Assembly
Inside this .zip file is an S-parameter file to be used with InfiniiSim to correct for the signal loss of the N2823A cable assembly.
先前版本

驱动程序 当前版本: n/a | 2018-10-17

S-Parameter Files for the N2114A/N2115A DDR4 BGA Interposers
This .zip file contains the and the S-parameter files for using the N2114A/N2115A DDR4 BGA interposers with InfiniiSim.
先前版本

驱动程序 当前版本: n/a | 2017-03-09

S-Parameter File for the N7015A Type-C High-Speed Test Fixture
Inside this .zip file is an S-parameter file to be used with InfiniiSim to correct for the signal loss of the N7015A Type-C high-speed test fixture.
先前版本

驱动程序 当前版本: n/a | 2015-10-12

E5813A PC Driver (Version v2.00.0)
Networked 5-port USB Hub PC Windows Driver (Version v2.00.0).
先前版本

驱动程序 当前版本: v2.00.0 | 2008-01-31

E5805A PC Driver (Version v2.88)
USB/4-port RS232 PC Driver
先前版本

驱动程序 当前版本: v2.88 | 2005-05-26

VXIPlug&Play Driver for E444xA PSA Series and E440xB/E4411B ESA Series Spectrum Analyzers
Includes Universal instrument driver and readme
先前版本

驱动程序 当前版本: A.02.00 | 2002-09-24