您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

縮小範圍

移除所有細分

依主題

依內容類型

依產品分類

1-16 / 16

排序:
How do I upgrade my X-Series Signal Analyzer to LTE-Advanced FDD?
The X-Series upgrade path to LTE-Advanced FDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

How do I update the operating system in an N9038A MXE EMI receiver from Windows XP to Windows 7?
See what is required to update the operating system in an N9038A MXE EMI Receiver...

FAQ 2014-04-02

Which version of the CPRI standard is the N5120A compliant to?
The N5120A is compliant up to v1.1.

FAQ 2013-09-27

Will Windows 7 work on my existing processor?
There is a minimum configuration/vintage of processors which are compatible with Windows 7 and these are denoted as PC4 and PC5 in the show system screen on your instrument

FAQ 2013-04-25

After purchasing an N9094AK upgrade, must the instrument be sent to a Keysight Service Center to be upgraded?
No. The N9094AK upgrades can easily be installed by the user...

FAQ 2013-04-25

How do I control instruments such as 82357A, E5810A, and 82350B using the GPIB interface?
There are several approaches to control instruments via the GPIB interface...

FAQ 2010-10-04

Serial BERT Software
Find all the latest software and firmware for the Serial BERT including: N4902B, N4906A, N4906B, and N4917A.

FAQ 2010-06-24

N5532A 感測器模組的頻率範圍為何?
100 kHz 至 4.2 GHz、10 MHz 至 18 GHz、30 MHz 至 26.5 GHz,與 30 MHz 至 50 GHz。

FAQ 2010-04-13

Does E5805A or E5813A driver supports Linux operating systems?
No, E5805A or E5813A does not support Linux operating systems

FAQ 2009-10-20

Why when using the parallel interleave mode and 1 clock per sample, the data seems to be clocked on the opposite clock edge than what the GUI state...
This is a known issue and has been noted for future consideration. The workaround is...

FAQ 2009-02-12

Why doesn't Windows® detect new hardware when I plug the E5813A USB Hub into the computer?
The new hardware is not detected when you plug the E5813A USB Hub into the computer because the PC driver may not be installed properly....

FAQ 2009-01-12

Is it possible to get an error log of incorrectly sent remote commands to my PSA, E4406A, EMC, or ESA Series Spectrum Analyzer?
Yes. PSA, E4406A and the ESA Series (with firmware A.08.00 and later) support this. You may turn Verbose error logging on through the front panel or remotely, SYST:ERR:VERBOSE ON

FAQ 2008-11-21

是否能夠儲存多重 TDR 軌跡,然後在示波器上將其顯示為波形,並與目前的量測波形做比較?
可以將多重 TDR 軌跡儲存為內部格式,以供未來參考……

FAQ 2008-08-03

是否可針對已儲存的波形進行量測?
是否可針對已儲存的波形進行量測?

FAQ 2008-08-03

是否能夠儲存先前的 TDR 量測波形,然後載入該波形,並與目前的 TDR 量測波形做比較?
是否能夠儲存先前的 TDR 量測波形,然後載入該波形,並與目前的 TDR 量測波形做比較?

FAQ 2008-08-03