検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

1-16 / 16

並べ替え
How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced FDD?
The X-Series upgrade path to LTE-Advanced FDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

How do I update the operating system in an N9038A MXE EMI receiver from Windows XP to Windows 7?
See what is required to update the operating system in an N9038A MXE EMI Receiver...

FAQ 2014-04-02

Which version of the CPRI standard is the N5120A compliant to?
The N5120A is compliant up to v1.1.

FAQ 2013-09-27

GPIBインタフェース(82357A、E5810A、82350B)を使って、GPIB経由でPC上から計測器を自動計測する方法を教えてください。
GPIBインタフェース(82357A、E5810A、82350B)を使って....

FAQ 2013-06-19

After purchasing an N9094AK upgrade, must the instrument be sent to a Keysight Service Center to be upgraded?
No. The N9094AK upgrades can easily be installed by the user...

FAQ 2013-04-25

Will Windows 7 work on my existing processor?
There is a minimum configuration/vintage of processors which are compatible with Windows 7 and these are denoted as PC4 and PC5 in the show system screen on your instrument

FAQ 2013-04-25

シリアル BERT ソフトウェア
シリアル BERT N4900 シリーズ用の現在のソフトウェアが、そのドキュメントと一緒に用意されています。

FAQ 2012-07-09

N5532Aセンサ・モジュールの周波数レンジはどれ位ですか?
100 kHz~4.2 GHz、10 MHz~18 GHz、30 MHz~26.5 GHz、30 MHz~50 GHzです。

FAQ 2010-04-25

Does E5805A or E5813A driver supports Linux operating systems?
No, E5805A or E5813A does not support Linux operating systems

FAQ 2009-10-20

Why when using the parallel interleave mode and 1 clock per sample, the data seems to be clocked on the opposite clock edge than what the GUI state...
This is a known issue and has been noted for future consideration. The workaround is...

FAQ 2009-02-12

Why doesn't Windows® detect new hardware when I plug the E5813A USB Hub into the computer?
The new hardware is not detected when you plug the E5813A USB Hub into the computer because the PC driver may not be installed properly....

FAQ 2009-01-12

Is it possible to get an error log of incorrectly sent remote commands to my PSA, E4406A, EMC, or ESA Series Spectrum Analyzer?
Yes. PSA, E4406A and the ESA Series (with firmware A.08.00 and later) support this. You may turn Verbose error logging on through the front panel or remotely, SYST:ERR:VERBOSE ON

FAQ 2008-11-21

複数のTDRトレースを保存し、波形としてオシロスコープに表示して、現在の測定と比較することはできますか?
複数のTDRトレースを内部フォーマットで保存し、後で参照することも可能...

FAQ 2008-08-03

以前のTDR測定波形を保存しておいて、現在のTDR測定と比較するためにロードすることは可能ですか?
以前のTDR測定波形を保存しておいて、それをオシロスコープにロードして現在の測定と比較することができます。

FAQ 2008-08-03

保存波形に対して、自動測定ができますか?
波形メモリに波形をロードすると、波形上のマーカを使用して、自動測定ができます。

FAQ 2008-08-03