이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

76-100 / 166

정렬방식:
9kHz까지 E5071C의 저주파수를 포함하는 ECal이 있습니까?
예, N4431B 4포트 ECal은 현재 9kHz까지 지원합니다.

FAQ 2009-11-16

Does E5805A or E5813A driver supports Linux operating systems?
No, E5805A or E5813A does not support Linux operating systems

FAQ 2009-10-20

Why am I not able to update my E5810A firmware via Keysight FTP at ftp://ftp.keysight.com/pub/e5810/ ?
Firmware revision A.01.07 and above are able to update via ftp

FAQ 2009-09-29

IO Libraries Suite: NI-488.2 및 Keysight IO Libraries Suite를 활용하는 어플리케이션을 사용하고 있는데 또 따로 설치해야 하는 소프트웨어가 있나요?

FAQ 2009-08-23

IO Libraries Suite: 키사이트 GPIB 카드나 컨버터를 NI-488.2로 작성한 타사 소프트웨어와 함께 사용할 수 있습니까?
예. IO Libraries Suite 14.1 출시로 그리고 계속해서 이후 버전 출시로, 이제 키사이트 GPIB 카드나 컨버터를 NI-488.2로 작성한 타사 소프트웨어와 함께 사용할 수 있습니다.

FAQ 2009-08-23

ENA에서, 임베디드 GPIB 인터페이스를 사용해서 파워 미터 교정을 제어하고 수행할 수 있습니까?
키사이트 82357A/B USB/GPIB 인터페이스가 필요합니다.

FAQ 2009-08-16

How to update E5810A firmware?
The firmware update instructions can be found on the User's Guide and E5810A Web Access Help......

FAQ 2009-08-06

How do I configure the E5813A Event Logging features in the E5813A LAN/USB Gateway Configuration Utility?
The E5813A Event Logging features are for internal diagnostic/troubleshooting of the device......

FAQ 2009-08-06

How can I identify if the MWA software is installed on my ENA?
The registered key code of the MWA is stored in the ENA directory.

FAQ 2009-07-15

What is the limitation of the evaluation mode of the MWA software?
The number of measurements is limited with the evaluation mode of the MWA back-end application.

FAQ 2009-07-15

Can we set up a set of different tests (i.e. different limit tests) with the MWA software?
Yes, you can manage up to ten different measurement setups on the same device with the MWA.

FAQ 2009-07-15

Can we control the MWA software from an external PC?
Yes, some functions on the MWA are supported for the remote control.

FAQ 2009-07-15

What are the replacement parts of the accessories furnished with the 41800A?

FAQ 2009-07-15

How can I update the MWA software on my ENA to the latest revision?
The latest revision of the MWA can be downloaded from Keysight web page.

FAQ 2009-07-15

How do I confirm if my measurements can be performed with the selected configuration of the E5092A?
The MWA software for the ENA recognizes the architecture of the E5092A, and automatically detects measurement paths that can not be performed with the selected switching configuration.

FAQ 2009-07-15

Can I convert my MWA file of the E5091A Multiport Test Set for utilizing with the E5092A Configurable Multiport Test Set?
Yes, you can convert your MWA file for the E5092A by selecting the equivalent configuration to the E5091A.

FAQ 2009-07-15

내 GPIB 카드에 맞는 IO 라이브러리를 웹 사이트 어디에서 찾을 수 있습니까?

FAQ 2009-06-23

Is there a sample file of the MWA software that I can customize for my DUT?
Yes, MWA files of some example devices can be downloaded from Keysight web page.

FAQ 2009-06-22

The N1021B kit contains shorts and loads. Why would I need an N1024A TDR Calibration kit?
The N1024A is a complete set of premium male and female shorts, male and female loads, a pair of broadband cables and a torque wrench ...

FAQ 2009-06-18

How does Keysight specify the bandwidth of the N1021B probe?
The one-way bandwidth of the probe can be estimated using a simplified equation ...

FAQ 2009-06-18

Can the N1021B differential TDR probe be ordered outside of the kit by itself?
Keysight decided to offer new differential TDR probes only as part of the N1021B probe kit ...

FAQ 2009-06-18

I'd like to make my own fixture to hold the N1021B probe. What do I need to know?
The N1021B probe body has two holes spaced 6.35 mm (1/4") apart and threaded for M2.5 screws. Maximum torque is 0.56 Newton-meter (5 lbf-in).

FAQ 2009-06-18

How does the angle between the N1021B probe and the target affect measurements?
It is best to hold the probe perpendicular to the DUT ...

FAQ 2009-06-18

What happens if I probe somewhere in the middle of differential traces? (N1021B differential TDR probe)
The net effects of probing in the middle of traces are (1) you will greatly attenuate the transmitted signal, (2) you will cause a big discontinuity in the line that will send a reflection back to the source, and (3) the signal viewed using the TD...

FAQ 2009-06-18

Why should I calibrate the N1021B differential TDR probe at its connector side as opposed to its tips?
Calibration requires a short to ground for each single-ended portion of a differential signal. Because the differential probe does not have ground at the tips, it is not possible to calibrate to the tips of the probe ...

FAQ 2009-06-18

이전 1 2 3 4 5 6 7 다음