이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

1-25 / 167

정렬방식:
Is there a 3D model of the InfiniiVision DSOX1202A/G and EDUX1052A/G oscilloscopes?
Yes, see the IGES, SAP, Step, and PKG format file downloads.

FAQ 2020-03-02

Is there a 3D model of the InfiniiVision DSOX1204A/G oscilloscopes?
Yes, see the IGES, SAP, Step, and PKG format file downloads.

FAQ 2020-01-24

Is there a 3D model of the InfiniiVision 1000 X-Series oscilloscopes?
Yes, see the IGES, SAP, Step, and PKG format file downloads.

FAQ 2020-01-24

Does Keysight offer teaching courseware on Industry 4.0 and IoT?
Keysight U380xA IoT Applied Courseware series offers a ready-to-teach package that includes hands-on industry relevant experiences and real-world applications such as Smart Home, Smart City, Smart Automobile and Industry 4.0. Click to find out more.

FAQ 2018-10-25

What upgrade options are needed to update my Windows operating system, processor board or solid state drive on my X-Series signal analyzer?
Details about X-Series signal analyzer operation system, processor and solid state drive dependencies

FAQ 2018-08-13

How do I remove the root login password on the U3800A Intel Edison?
If the password is misplaced or lost, you will need to reflash Intel Edison firmware. Otherwise, you can remove the password from Edison’s system file.

FAQ 2018-07-25

How do I get replacement parts for individual items in the training kit?
Here are the parts that need to be purchased from Keysight at www.keysight.com/find/parts

FAQ 2018-02-26

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced FDD?
The X-Series upgrade path to LTE-Advanced FDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

Is there a 3D model of the InfiniiVision 4000 X-Series oscilloscopes?
Yes, see the IGES, SAP, Step, and PKG format file downloads.

FAQ 2017-05-05

Is it possible to get an error log of incorrectly sent remote commands to my PSA, E4406A, EMC, or ESA Series Spectrum Analyzer?
Yes. PSA, E4406A and the ESA Series (with firmware A.08.00 and later) support this. You may turn Verbose error logging on through the front panel or remotely, SYST:ERR:VERBOSE ON

FAQ 2016-07-05

What is the operating temperature range for 34138A test lead set?
The operating temperature range is limited to the DMM model with which it is used....

FAQ 2015-08-21

Is there a 3D model of the InfiniiVision 2000/3000/3000T X-Series oscilloscopes?
Yes, see the IGES, SAP, and Step format file downloads.

FAQ 2015-02-18

Is E5810B remote USB interface supported in NI MAX environment?
No. E5810B remote USB interface is not supportable in NI MAX environment. The E5810B remote USB interface only detectable in Keysight IO libraries Suite.

FAQ 2014-12-10

How do I update the operating system in an N9038A MXE EMI receiver from Windows XP to Windows 7?
PC4 (Dual-Core High Performance Processor) 및 W7X (Window 7 OS) Option을 구매하시면 Window 7으로 upgrade 가능합니다.

FAQ 2014-08-25

키사이트, 애질런트 및 휴렛팩커드의 단종된 테스트 장비에 대한 매뉴얼은 어디에서 확인할 수 있습니까?
대부분의 키사이트 제품의 PDF 매뉴얼은 제품 페이지에서 확인하실 수 있습니다. 다른 벤더들도 예전 매뉴얼을 제공합니다.

FAQ 2014-08-01

Why are USB modular instruments (U2700 Series) and USB DAQ modules (U2300, U2500, U2600 Series) not detectable by the E5810B?
Establish the connection between the USB modular Instrument and the PC directly, and then disconnect the device from the PC (while it’s still powered-on), and connect to E5810B.

FAQ 2014-04-17

How can I make NI LabVIEW communicate with Keysight 82357B USB/GPIB Interface?
Keysight IO Libraries install as secondary VISA side by side with NI VISA. Keysight IO Libraries Keysight 488 Options enable. In NI MAX, ensure Passport for Tulip (NIVisaTulip.dll) enable.

FAQ 2014-04-17

교정 키트 토크 렌치를 위한 인증(및 재인증) 프로세스는 무엇입니까?

FAQ 2014-03-24

What’s the difference between E5810B and E5810A?
Please refer to the table for side-by-side comparison below

FAQ 2013-10-25

N5120A 에서 지원하는 CPRI 규격은 어떤 버젼입니까?
N5120A 는 CPRI standard v1.1 까지 지원됩니다.

FAQ 2013-09-27

E8257D 업그레이드 표
E8257D PSG 아날로그 신호 발생기 업그레이드 표

FAQ 2013-08-20

ENA에서 멀티포트테스트세트 없이 MWA 소프트웨어를 사용할수 있나요?
네 사용 할 수 있습니다.

FAQ 2013-07-17

How do I remotely program my spectrum or vector signal analyzer?
Instructions, examples, and references for remotely programming your spectrum analyzer

FAQ 2013-05-16

After purchasing an N9094AK upgrade, must the instrument be sent to a Keysight Service Center to be upgraded?
No. The N9094AK upgrades can easily be installed by the user...

FAQ 2013-04-25

1 2 3 4 5 6 7 다음