这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

1-25 / 166

排序:
Does Keysight offer teaching courseware on Industry 4.0 and IoT?
Keysight U380xA IoT Applied Courseware series offers a ready-to-teach package that includes hands-on industry relevant experiences and real-world applications such as Smart Home, Smart City, Smart Automobile and Industry 4.0. Click to find out more.

FAQ 2018-10-25

What upgrade options are needed to update my Windows operating system, processor board or solid state drive on my X-Series signal analyzer?
Details about X-Series signal analyzer operation system, processor and solid state drive dependencies

FAQ 2018-08-13

How do I remove the root login password on the U3800A Intel Edison?
If the password is misplaced or lost, you will need to reflash Intel Edison firmware. Otherwise, you can remove the password from Edison’s system file.

FAQ 2018-07-25

How do I get replacement parts for individual items in the training kit?
Here are the parts that need to be purchased from Keysight at www.keysight.com/find/parts

FAQ 2018-02-26

Is there a 3D model of the InfiniiVision 1000 X-Series oscilloscopes?
Yes, see the IGES, SAP, Step, and PKG format file downloads.

FAQ 2017-07-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced FDD?
The X-Series upgrade path to LTE-Advanced FDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

Is there a 3D model of the InfiniiVision 4000 X-Series oscilloscopes?
Yes, see the IGES, SAP, Step, and PKG format file downloads.

FAQ 2017-05-05

What is the operating temperature range for 34138A test lead set?
The operating temperature range is limited to the DMM model with which it is used....

FAQ 2015-08-21

Is there a 3D model of the InfiniiVision 2000/3000/3000T X-Series oscilloscopes?
Yes, see the IGES, SAP, and Step format file downloads.

FAQ 2015-02-18

Is E5810B remote USB interface supported in NI MAX environment?
No. E5810B remote USB interface is not supportable in NI MAX environment. The E5810B remote USB interface only detectable in Keysight IO libraries Suite.

FAQ 2014-12-10

Why are USB modular instruments (U2700 Series) and USB DAQ modules (U2300, U2500, U2600 Series) not detectable by the E5810B?
Establish the connection between the USB modular Instrument and the PC directly, and then disconnect the device from the PC (while it’s still powered-on), and connect to E5810B.

FAQ 2014-04-17

How can I make NI LabVIEW communicate with Keysight 82357B USB/GPIB Interface?
Keysight IO Libraries install as secondary VISA side by side with NI VISA. Keysight IO Libraries Keysight 488 Options enable. In NI MAX, ensure Passport for Tulip (NIVisaTulip.dll) enable.

FAQ 2014-04-17

How do I update the operating system in an N9038A MXE EMI receiver from Windows XP to Windows 7?
See what is required to update the operating system in an N9038A MXE EMI Receiver...

FAQ 2014-04-02

对校准套件扭力扳手进行认证(和再认证)的过程是怎样的?
目前,是德尚不提供我们的校准套件中包含的任何类型扭力扳手的“数据”。对新采购和再认证的校准套件均是如此。即使是被要求“使用数据校准”时,也不提供扭力扳手的数据。

FAQ 2014-03-24

网络分析仪和频谱分析仪打印机兼容能力指南
这些参考资料提供关于下列Keysight网络分析仪(1)和频谱分析仪(2)的打印机兼容性信息。

FAQ 2014-01-31

What’s the difference between E5810B and E5810A?
Please refer to the table for side-by-side comparison below

FAQ 2013-10-25

Which version of the CPRI standard is the N5120A compliant to?
The N5120A is compliant up to v1.1.

FAQ 2013-09-27

E8257D 升级表
E8257D PSG 模拟信号发生器升级表

FAQ 2013-08-20

我可以在哪里找到是德科技、安捷伦和惠普的已停产测试与测量设备手册?
是德科技的大部分产品页面都能提供 PDF 版本手册。另外,其他厂商也可能提供旧版手册。

FAQ 2013-05-29

如何对频谱或矢量信号分析仪进行远程编程?
下面的信息可能会给您对是德频谱分析仪进行远程编程提供有益的帮助。

FAQ 2013-05-16

我现有的处理器是否支持 Windows 7 系统?
处理器应当符合 Windows 7 系统的最低配置/型式要求,在仪器的显示系统屏幕上以 PC4 和 PC5 表示。

FAQ 2013-05-08

现有客户在购买了 N9094AK-PC4 或 N9094AK-SSD 选件后,是否要把仪器送往当地的 SSU 服务中心进行升级?
不是。N9094AK-PC4 和 N9094AK-SSD 升级选件均配备了镜像 SSD。

FAQ 2013-05-08

Which probe positioners are available to hold the N1021B?
The adapter provided with the N1021B is generic enough to work with robot arms or common industry positioners ...

FAQ 2012-07-06

For my PSA Series Spectrum Analyzer, what is recommended to do if my instrument is having trouble saving files or the instrument firmware is unexpe...
This issue may be caused by a corrupt firmware file or may be caused by a defect in firmware. Please first try upgrading the instrument’s firmware to the latest version posted on the Keysight web. This issue may also be caused by a hardware probl...

FAQ 2012-05-30

1 2 3 4 5 6 7 下一页