이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

1-25 / 137

정렬방식:
What is Frequency Response Analysis
Learn what frequency response analysis is and why it is so important with today’s electronics to ensure performance requirements are met.

어플리케이션 노트 2020-05-14

Keysight Solution for Power Storage and Conversion Testing
There is a growing need to test power across all industries such as IoT, medical, automotive, and industrial. Properly powering up a test device is critical to evaluating a design. At the same time, properly loading down a test device is just as important. Things like DC-DC converters and batteries require both a power source and a loading mechanism to perform various tests. While both common solutions involve the power source and the load as separate instruments, Keysight has you covered with a fully integrated source and load solution. The N6700 power platform allows the test engineer to power up and load down a device properly in a single sweep with seamless interaction between the two operations.

어플리케이션 노트 2020-04-07

Multiport and Multi-site Test Optimization Techniques - Application Note
This app note gives an overview of multiport and multi-site test capabilities, how different multiport test solutions compare, and what should be considered when configuring a multi-site test station.

어플리케이션 노트 2020-03-24

Spectrum and Signal Analyzer Measurements and Noise Application Note 1303
Noise is the classical limitation of electronics. In this application note, the characteristics of noise and its direct measurement are discussed in detail.

어플리케이션 노트 2020-02-27

PDF PDF 3.57 MB
Practical Temperature Measurements - Application Note
This application note explores the more common temperature measurement techniques and introduces procedures for improving their accuracy.

어플리케이션 노트 2019-11-14

PDF PDF 6.20 MB
Recognizing and Reducing Data Acquisition Switching Transients - White Paper
Low impedance sources can produce large and fast current transients when switching; creating problems with adjacent channels, transients in the ground circuit that upset digital logic connected to the DUT, or causing the switch unit to reset or hang. This application note describes several techniques to reduce these switching transients.

어플리케이션 노트 2019-09-27

PDF PDF 3.12 MB
Automotive FMCW Analysis with U3851A RF Microwave Courseware
Frequency Modulated Continuous Wave (FMCW) is widely use automotive industry. In this document, we will discuss about FMCW simulation with SystemVue and real-world measurement with the prototyping kit.

어플리케이션 노트 2019-07-16

PDF PDF 1.47 MB
Drive Down the Cost of Test Using the ENA Series Vector Network Analyzers - Application Note
Discussion of the contributions of the Keysight ENA series vector network analyzer to drive down the cost of test in production lines. Including an in depth analysis of the total cost of ownership.

어플리케이션 노트 2019-06-04

Signal Integrity Analysis Series Part 1: Single-Port TDR, TDR/TDT, and 2-Port TDR - Application Note
This Application Note focuses on part 1: those which use a single-port TDR, those which use TDR/TDT, and those which use 2-port TDR.

어플리케이션 노트 2019-04-25

PDF PDF 10.50 MB
Understanding the Fundamental Principles of Vector Network Analysis - Application Note 1287-1
This application note explores the fundamental principles of vector network analysis. The discussion includes the common parameters (S-parameters). RF fundamentals such as transmission lines and the Smith chart will also be reviewed.

어플리케이션 노트 2019-04-04

Power Handling Capability of Electromechanical Switches
This application note discusses the power handling of the hot switching and cold switching of EM switches.

어플리케이션 노트 2019-02-13

USB 2.0 Compliance Testing with Infiniium Oscilloscopes - Application Note
This Application Note discusses the solution for the USB 2.0 test suite. The Keysight solution is the only one-box solution that uses the official USB-IF scripts for precompliance ans compliance testing.

어플리케이션 노트 2019-01-29

Metrology-Grade Measurement Challenges - Application Note
This application note analyzes the sources that contribute to measurement uncertainties and summarizes how to achieve the most accurate measurement results with the Keysight N5531X.

어플리케이션 노트 2018-12-20

PDF PDF 819 KB
Probe soldering guidelines for Keysight InfiniiMax probes - Application Note
There are various ways to connect test instrumentation probes to devices under test(DUTs). One such method is soldering, which provides a reliable connection and minimizes parasitic probing effects by keeping wire lengths and connections as short as possible. Many of Keysight's high performance oscilloscopes probes utilize soldered connections.

어플리케이션 노트 2018-10-07

PDF PDF 7.73 MB
An Overview of the Electrical Validation of 10BASE-T, 100BASE-TX, and 1000BASE-T - Application Note
The technology used in these ports, commonly known as “LAN” or “NIC” ports, is usually one of the 10BASE-T, 100BASE-TX, and 1000BASE-T standards or a combination of them.

어플리케이션 노트 2018-07-25

Probing a Midpoint of a Transmission Line that is Not Load Terminated - White Paper
With the advent of variable on die termination (i.e. ODT) many systems like low power double data rate memory (LPDDR) have the ability to either terminate a line in its characteristic impedance for high speed operation or terminate it with an open for lower speed operation. Many times there is a desire to probe the transmission line to monitor the signals on the line. When the transmission line is terminated in close to its characteristic impedance, the signals can be readily observed. However, if the line is terminated in an impedance that is not close to the characteristic impedance then it may not be possible to accurately measure the signals.

어플리케이션 노트 2018-07-03

PDF PDF 1.98 MB
Bandwidth Boosting Techniques for the Infiniimax Probe Amp and Probe Head - Application Note
Keysight InfiniiMax differential probes are DSP corrected to have a flat magnitude and phase response to provide the highest possible accuracy. The bandwidth chosen to correct to is typically around 3dB non-corrected bandwidth. Usually, extending the bandwidth much beyond that point will increase the noise floor, and if pushed even further, can cause unrealistic noise artifacts. However, the N5381A/B solder-in probe head in combination with the InfiniiMax 1169A/B probe amp is an excellent candidate for extending the bandwidth beyond the 3dB point because the N5381A/B is peaked past the normal 12 GHz bandwidth, and the peaking of the probe head can help compensate for the roll-off of the probe amp bandwidth.

어플리케이션 노트 2018-06-21

PDF PDF 4.96 MB
Optimizing Dynamic Range for Distortion Measurements - Application Note
This application note covers high dynamic range measurement techniques for the new PSA Performance Spectrum Analyzer Series. The note describes the best way to use the PSA series to make distortion measurements such as ACP, intermodulation, and harmonic distortion.

어플리케이션 노트 2018-03-12

PDF PDF 2.11 MB
Measuring Frequency Response with E5061B LF Network Analyzer
This application note describes fundamentals on low frequency network analysis by featuring the E5061B LF-RF network analyzer. Here we mainly discuss simple low frequency 2-port device measurements and associated topics.

어플리케이션 노트 2018-02-22

신호 분석 측정 기초, 노이즈 플로어 최적화, 해상도 대역폭 등(영어)
탁월한 통찰력을 위해 신호 분석을 최적화하기 위한 측정 기초를 알아보십시오.

어플리케이션 노트 2017-12-13

The Application of Handheld Spectrum Analyzers in Interface Testing - Application Note

어플리케이션 노트 2017-12-05

고정밀 TDR(Time Domain Reflectometry) (영어)
TDR(Time Domain Reflectometry)은 콤포넌트, 인터커넥트 및 전송선의 신호 경로 품질과 임피던스를 확인하기 위한 확실한 기법입니다.

어플리케이션 노트 2017-12-02

Choosing the Best Passive and Active Oscilloscope Probes for Your Tasks - Application note
Selecting the right probe for your application is the first step toward making reliable oscilloscope measurements, and each probe has an application for which it performs best.

어플리케이션 노트 2017-12-02

Demystifying RCRC and RC probes - Application Note
An ideal probe would provide an exact replica of a signal being probed. However, the probe becomes a part of the circuit under test, because the probe introduces probe loading to the circuit.

어플리케이션 노트 2017-12-01

PDF PDF 1.27 MB
InfiniiMax Probes Impact on Lead-Free (ROHS) Compliance - Application Note
Some Keysight InfiniiMax oscilloscope probe heads are intended for soldering to the device under test.

어플리케이션 노트 2017-12-01

PDF PDF 565 KB

1 2 3 4 5 6 다음