Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

1-25 из 138

Упорядочить:
Can the state of channel be stored while it is still being actively monitored?
No. The instrument can store the configuration for all channels only while monitoring is OFF. Only measurement attributes of the currently-selected functions (range, resolution, etc) will be preserved in the stored states. If channel monitoring is ON during store / auto-recall execution, the instrument will not function correctly. To restore the instrument back to its initial working state, all modules slotted into the instrument must be removed and the auto-recall function turned OFF. Please refer to the user manual / service manual regarding the usage of the store/auto-recall function.

FAQ 2017-11-13

What are the recommended power supplies used for U9391C/F/G?
Power supply

FAQ 2017-08-07

What are the Keysight equivalent model numbers for Centellax BERT products and test accessories?
Click on the question for full details of the equivalent model numbers.

FAQ 2017-07-13

How do I display the mixer conversion loss of M1970 Series or M1971 Series Harmonic Mixer on an X-Series Signal Analyzer?
There is no way to display the conversion loss values from these mixers on screen. There is a hard copy of the conversion loss data supplied with each mixer that can be referenced.

FAQ 2017-06-28

How many peripheral modules (M9379A, M9341A/B, M9161D, M9111A) are supported on M9485A?
M9485A supports one M9341A/B and up to 6 M9111A. There is no software limitation for M9379A and M9161D.

FAQ 2017-05-25

What is the current rating of the Y113xA cables?
The Y1135A and Y1136A cables are 50 conductor, 24 AWG cables with 25 shielded twisted pairs with PVC insulation. They can be used with the 34921A, 23A, 25A, 31A, 32A, 33A, 37A, 38A, 51A, and 52A plug-in modules for the 34980A. However, they do not support the full rated total current of the 34937A and 34938A. The Y1137A and Y1138A cables are 78 conductor cables 28 AWG conductors with 39 shielded twisted pairs. They can be used with the 34922A, 24A, 34A, 39A, and 34950A plug-in modules.

FAQ 2016-12-13

Torque Wrench used with M1971E

FAQ 2016-10-01

What is the difference between the two RF cables attached to the U7227A/C/F?
Mechanical dimension and color for the RF cable.

FAQ 2015-10-26

Does the new RF cable affect the RF performance of the U7227A/C/F USB preamplifier?
RF performance of the U7227A/C/F with new RF cable

FAQ 2015-10-26

Why is there a different type of RF cable attached to the U7227A/C/F?
Different type of RF cable attached to the U7227A/C/F.

FAQ 2015-10-26

Where can I find manuals for discontinued and obsolete Hewlett-Packard, Agilent and Keysight test equipment?
Most Keysight products have PDF manuals that can be found on product pages. Other vendors also supply old manuals.

FAQ 2014-08-01

How do you clear the 34980A multifunction switch/measure mainframe and modules, L44xxA series LXI switch and control instruments memories?
Please refer to the documents for a comprehensive listing of memory installed into these products.

FAQ 2014-04-07

Can the L4490A/L4491A mainframe be password protected when using LAN?
Yes, instructions for using password protection can be found in the web interface.

FAQ 2014-04-07

Are SMA connectors suitable for low PIM measurements?
Type N and DIN 7/16 are currently the most common interfaces used for low PIM applications. Both are popular for PIM measurements due to their low PIM and higher power handling. However, the SMA connector is also another option for low PIM applications. Keysight’s low PIM RF switches use SMA connectors, which can handle 120 watts of average power at 4.2 GHz for cold switching. The base material for the center connector and housing is BeCu, which is free of ferromagnetic material that ensures low PIM.

FAQ 2014-03-03

Can you advise of alternatives to printing and acquiring screen images from the various Keysight Analyzers equipped with only a GP-IB interface?
There are several way to retrieve screenshots.

FAQ 2014-02-18

My Keysight LXI based SICL / LAN instrument is timing out on the LAN connection under automation control. Is it possible to avoid this LAN timeout?
Yes, please access the LXI based instruments web server by entering the instruments IP address into a web browser. If the LAN has timed out it maybe necessary to cycle the power button.

FAQ 2014-01-28

Which 34980A Switch Modules are supported by the IviSwtch api?
All modules except the 34945A, 34950A, 34951A, 34952A, 34959A...

FAQ 2014-01-22

What components are included in the Keysight Y1159A cable kit?
The Keysight Y1159A is a 16 pin IDC to 16 pin IDC cable kit for the Y1150A, Y1151A, Y1152A, Y1153A, Y1154A and / or the Y1155A distribution boards. (See Chart)

FAQ 2013-12-11

What components are included in the Keysight Y1157A cable kit?
The Keysight Y1157A is a 9 pin DSUB to 10 pin IDC cable kit for the Y1150A, Y1152A and / or the Y1154A distribution boards. (See Chart)

FAQ 2013-12-11

What components are included in the Keysight Y1158A cable kit?
The Keysight Y1158A is a 10 pin IDC to 10 pin IDC or 10 pin IDC to 14 pin IDC cable kit for the Y1153A and / or the Y1154A distribution boards. (See Chart)

FAQ 2013-12-11

What is the maximum total length of the RJ45 control cable for connecting multiple 34945EXTs?
The maximum total length of the RJ45 control cables is 140 feet.

FAQ 2013-05-06

How do I view the 3D models that come with the L4490A/L4491A?
The L4490A/L4491A comes with .easm, .igs and .stp files that can be imported into your modeling application.

FAQ 2013-03-13

Where do I get Java to display the 34980A web interface?
The Java Virtual Machine code is needed to run the Keysight 34980A web page features. A free download of the Java Virtual Machine (JVM) can be obtained by going to the following web site.

FAQ 2012-12-17

Will the external mixer Option EXM support the 11974 Series preselected mixers?
There are no plans to support the 11974 Series preselected mixers with the N9030A PXA.

FAQ 2012-10-25

How can I order replacement protective caps for waveguide flanges?
Order information for replacement protective caps for waveguide flanges.

FAQ 2012-10-23

1 2 3 4 5 6 Следующие