検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

1-25 / 161

並べ替え
モニタ・モードONの状態でステート保存できますか?
いいえ、できません。34980Aでは、モニタ・モードがOFFの状態でのみステート保存することができます。 ステート保存では、現在設定されている機能(レンジ、分解能など)のみを保存することができます。 もし、モニタ・モードがONの状態で保存し、自動リコール・モードを設定した場合、34980Aは正常に起動することができなくなります。正常に起動する状態に戻すためには、全てのモジュールをスロットから取り外し、34980A起動後、自動リコール・モード機能をOFFにする必要があります。

FAQ 2017-11-21

What are the recommended power supplies used for U9391C/F/G?
Power supply

FAQ 2017-08-07

What are the Keysight equivalent model numbers for Centellax BERT products and test accessories?
Click on the question for full details of the equivalent model numbers.

FAQ 2017-07-13

How do I display the mixer conversion loss of M1970 Series or M1971 Series Harmonic Mixer on an X-Series Signal Analyzer?
There is no way to display the conversion loss values from these mixers on screen. There is a hard copy of the conversion loss data supplied with each mixer that can be referenced.

FAQ 2017-06-28

How many peripheral modules (M9379A, M9341A/B, M9161D, M9111A) are supported on M9485A?
M9485A supports one M9341A/B and up to 6 M9111A. There is no software limitation for M9379A and M9161D.

FAQ 2017-05-25

What is the current rating of the Y113xA cables?
The Y1135A and Y1136A cables are 50 conductor, 24 AWG cables with 25 shielded twisted pairs with PVC insulation. They can be used with the 34921A, 23A, 25A, 31A, 32A, 33A, 37A, 38A, 51A, and 52A plug-in modules for the 34980A. However, they do not support the full rated total current of the 34937A and 34938A. The Y1137A and Y1138A cables are 78 conductor cables 28 AWG conductors with 39 shielded twisted pairs. They can be used with the 34922A, 24A, 34A, 39A, and 34950A plug-in modules.

FAQ 2016-12-13

Torque Wrench used with M1971E

FAQ 2016-10-01

Does the new RF cable affect the RF performance of the U7227A/C/F USB preamplifier?
RF performance of the U7227A/C/F with new RF cable

FAQ 2015-10-26

Why is there a different type of RF cable attached to the U7227A/C/F?
Different type of RF cable attached to the U7227A/C/F.

FAQ 2015-10-26

What is the difference between the two RF cables attached to the U7227A/C/F?
Mechanical dimension and color for the RF cable.

FAQ 2015-10-26

既に販売が完了したKeysight、KeysightおよびHewlett-Packard(HP)のテスト機器のマニュアルはどのように入手できますか?
ほとんどのKeysight製品にPDFマニュアルがあり、製品ページで入手することができます。Keysightのベンダも古いマニュアルを提供しています。

FAQ 2014-08-01

Can the L4490A/L4491A mainframe be password protected when using LAN?
Yes, instructions for using password protection can be found in the web interface.

FAQ 2014-04-07

How do you clear the 34980A multifunction switch/measure mainframe and modules, L44xxA series LXI switch and control instruments memories?
Please refer to the documents for a comprehensive listing of memory installed into these products.

FAQ 2014-04-07

Are SMA connectors suitable for low PIM measurements?
Type N and DIN 7/16 are currently the most common interfaces used for low PIM applications. Both are popular for PIM measurements due to their low PIM and higher power handling. However, the SMA connector is also another option for low PIM applications. Keysight’s low PIM RF switches use SMA connectors, which can handle 120 watts of average power at 4.2 GHz for cold switching. The base material for the center connector and housing is BeCu, which is free of ferromagnetic material that ensures low PIM.

FAQ 2014-03-03

GP-IB インタフェースだけしかない色々なキーサイト製のアナライザ の測定結果をプリンタに印刷する以外に別の手段はありませんか?
Keysight Intuilink は多くの汎用計測器に接続性を提供する無料で提供されるキーサイトのアプリケーションソフトです。

FAQ 2014-02-08

My Keysight LXI based SICL / LAN instrument is timing out on the LAN connection under automation control. Is it possible to avoid this LAN timeout?
Yes, please access the LXI based instruments web server by entering the instruments IP address into a web browser. If the LAN has timed out it maybe necessary to cycle the power button.

FAQ 2014-01-28

Which 34980A Switch Modules are supported by the IviSwtch api?
All modules except the 34945A, 34950A, 34951A, 34952A, 34959A...

FAQ 2014-01-22

Keysight Y1159Aケーブル・キットにはどのようなコンポーネントが含まれていますか?
Keysight Y1159Aは、Y1150A、Y1151A、Y1152A、Y1153A、Y1154A、Y1155A分配ボード用の16ピンIDC-16ピンIDCケーブル・キットです。Y1159Aキットの構成品目は次のとおりです。

FAQ 2013-12-11

Keysight Y1157Aケーブル・キットにはどのようなコンポーネントが含まれていますか?
Keysight Y1157Aは、Y1150A、Y1152A、Y1154A分配ボード用の9ピンDsub-10ピンIDCケーブル・キットです。Y1157Aキットの構成品目は次のとおりです。

FAQ 2013-12-11

Keysight Y1158Aケーブル・キットにはどのようなコンポーネントが含まれていますか?
Keysight Y1158Aは、Y1153AまたはY1154A分配ボード用の10ピンIDC-10ピンIDCまたは10ピンIDC-14ピンIDCケーブル・キットです。Y1158Aキットの構成品目は次のとおりです。

FAQ 2013-12-11

[仕様] プローブを高温環境下、低温環境下にて使用したい場合、どのようにしたら良いでしょうか?
低温、高温環境での使用には、InfiniiMaxプローブとN5450A InfiniiMax極限温度延長ケーブルを組み合わせて御使用ください。

FAQ 2013-11-26

[アクセサリ] オシロのプローブの本体、アクセサリを紛失/破損してしまいました。保守部品は購入できますか?
購入できる物と出来ない物がございます。

FAQ 2013-10-29

[仕様]N2795A/N2796Aは同時に何本使えますか。
機種によって使用できる数が異なります。

FAQ 2013-06-17

複数の34945EXTを接続するためのRJ45制御ケーブルの最大全長は?
RJ45制御ケーブルの全長(最大)は約42.7 mです。

FAQ 2013-05-13

How do I view the 3D models that come with the L4490A/L4491A?
The L4490A/L4491A comes with .easm, .igs and .stp files that can be imported into your modeling application.

FAQ 2013-03-13

1 2 3 4 5 6 7 次へ