Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discutez avec un expert

Support technique

Mesure Electronique

Support by Product Model Number:

Affiner la liste

retirer tout le raffinement

Par type de contenu

1-15 sur 15

Tri:
How TestOps Speeds Electronic Design and Test - White Paper
TestOps speeds electronic design and test by reducing time-to-market and enhancing team collaboration and productivity. Similar to DevOps, TestOps is not a new technology, but a new way to work.

Notes d’application 2019-04-11

Removing Time-To-Market Barriers for Design and Test Engineers
Keysight survey reveals data sharing enabled by an integrated product development solution significantly improves time-to-market across the entire product development workflow.

Notes d’application 2019-03-26

Extensible VEE Object (EVO) Developer's Guideline - Application Note
Keysight VEE provides a way to extend Keysight VEE functionality by introducing Extensible VEE Object (EVO). Each EVO has its own GUI control and execution behavior, and is similar to generic VEE object.

Notes d’application 2019-01-28

PDF PDF 1.43 MB
FPGA Implementation of a LUT-Based Digital Pre-Distortion - Application Note
This application note demonstrates the implementation of a signal transformation using a lookup table (LUT). This program transforms a sawtooth signal into a sinusoidal.

Notes d’application 2017-12-01

FPGA Implementation of a LUT-Based Input Processing - Application Note
This application note demonstrates the implementation of a signal transformation using a lookup table (LUT). It implements a piecewise first-order linear approximation of a nonlinear function.

Notes d’application 2017-12-01

Using MATLAB to Create Keysight Signal and Spectrum Analyzer Applications - Application Note
Learn to use MATLAB software to configure, control, and acquire data from X-Series signal and spectrum analyzers, and then use scripts to create, modify and execute custom analyzer applications.

Notes d’application 2017-12-01

PDF PDF 9.69 MB
FPGA Implementation of a Digital-PLL Using FPGAflow - Application Note
This application note demonstrates the capabilities of Keysight M3300A AWG and digitizer PXIe combo module to implement closed-loop controls

Notes d’application 2017-01-05

Creating Hardware Handler in C/C++ for Keysight TestExec SL
A hardware handler enhances the Keysight TestExec SL's ability to control devices by communicating directly with the instrument's driver. This application note describes how to create hardware handlers for the TestExec SL.

Notes d’application 2009-09-10

PDF PDF 181 KB
Configuring Signal and Load Switching Using Keysight TestExec SL
This application note describes how users of the Keysight TestExec SL software can easily configure and set up switching for the increasing number of channels on units under test with the Switch Manager feature in the software.

Notes d’application 2009-08-13

PDF PDF 286 KB
Database Connectivity Guide for TestExec SL
This application note outlines the importance of proper data logging in a database and discusses best practices to import extensible markup language (XML) files from TestExec into a database.

Notes d’application 2009-07-16

PDF PDF 434 KB
Customizing the Keysight TestExec SL Operator Interface using Visual Basic
This application note describes how users of the Keysight TestExec SL software can customize the operator user interface using Visual Basic.

Notes d’application 2009-07-07

PDF PDF 312 KB
Automotive Power Window Regulator Testing - Application Note
Automotive power window regulator tests require the use of accurate data acquisition devices, as they cover a wide range of parameters such as window movement, acceleration of the window movement in both directions, maximum range of movement, torque exerted at the start, the end stall torque, and motor load characteristics.

Notes d’application 2008-06-30

PDF PDF 280 KB
Small Engine Dynamometer Testing - Application Note
Performing Dynamometer Testing on Combustion Engines

Notes d’application 2008-06-01

PDF PDF 443 KB
Strain Measurement Application Using U2300A Series with Keysight VEE Pro - Application Note
This application note describes how users can make strain and vibration measurements using the Keysight USB DAQ for reliability and strength characterization of concrete and metal structures.

Notes d’application 2007-05-18

PDF PDF 208 KB
Speeding Production Line Test Development and Execution at Motorola AEIG
This application note documents use of TestExec SL to decrease test development time and increase throughput in a case study with Motorola.

Notes d’application 2004-02-11

PDF PDF 214 KB