这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

1-25 / 31

排序:
Sample Project Files for Automated NFC Test Software
Sample project files for the Automated NFC Test Software. To view: (1) extract files on the controller PC, (2) run the NFC Test App, (3) open the extracted .proj file.

编程实例 2016-07-25

ZIP ZIP
[实施方法] USB C 型电缆-连接器组件一致性测试

编程实例 2015-11-24

[实施方法] PCI Express 3.0 Tx/Rx 阻抗和回波损耗测试
[实施方法] PCI Express 3.0 Tx/Rx 阻抗和回波损耗测试

编程实例 2015-07-15

[实施方法] 以太网电缆测试

编程实例 2015-04-07

[实施方法] DisplayPort 1.3 电缆-连接器组件一致性测试
[实施方法] DisplayPort 1.3 电缆-连接器组件一致性测试

编程实例 2015-02-27

实施方法] USB 3.1 电缆-连接器组件一致性测试
实施方法] USB 3.1 电缆-连接器组件一致性测试

编程实例 2015-02-06

HDMI 源端/接收端阻抗测试

编程实例 2014-11-06

[实施方法]以太网发射机/接收机回波损耗测试

编程实例 2014-11-06

[Method of Implementation] MIPI D-PHY TxRx Interface S-parameter and Impedance Test

编程实例 2014-10-10

[实施法] BroadR-Reach 链路分段一致性测试

编程实例 2014-08-28

[Method of Implementation] USB 2.0 Cable-Connector Assembly Compliance Test

编程实例 2014-06-26

[Method of Implementation] SATA RXTX Impedance Compliance Test

编程实例 2014-04-28

[Method of Implementation] SATA SI Compliance Test

编程实例 2014-04-28

[Method of Implementation] MIPI M-PHY TxRx Interface S-parameter and Impedance Test

编程实例 2014-04-08

E5063A Sample Programs in Help
This is sample program files which are shown in the E5063A Help. See the E5063A Help for more detail.

编程实例 2014-02-01

[实现方法] HDMI 电缆组件一致性测试
[实现方法] HDMI 电缆组件一致性测试

编程实例 2013-11-03

[实施方法] DisplayPort 1.2b 电缆-连接器组件一致性测试
[实施方法] DisplayPort 1.2b 电缆-连接器组件一致性测试

编程实例 2013-04-18

[实施法] MHL 电缆至连接器组件一致性测试

编程实例 2013-03-28

[Method of Implementation] PCI Express 3.0 PCB Differential Trace Impedance Test

编程实例 2013-03-25

[Method of Implementation] USB 3.0 Cable-Connector Assembly Compliance Test

编程实例 2013-01-16

E5071C-TDR Sample Programs in Help
This is the sample program files which are explained in the E5071C help. See the E5071C help (Option TDR) for more detail.

编程实例 2010-08-18

ZIP ZIP 122 KB
E5061B Sample Programs in Help
This is sample program files which are shown in the E5061B Help. See the E5061B Help for more detail.

编程实例 2010-06-29

Desktop EasyEXPERT Application Test: Basic IV measurement for the Keysight E5270B and E5260A series
Sample application test of the E5270B and E5260 Series switching matrix for the Desktop EasyEXPERT Software

编程实例 2009-09-30

Automate and acquire measurements from Keysight N9020A
Automate, acquire real measurement data and benefit from the speed of Keysight N9020A.

编程实例 2008-07-30

ZIP ZIP 7.20 KB
Direct I/O: Set Up and Bandwidth Measurement
Set up the spectrum analyzer and measure the occupied bandwidth on CDMA2000.

编程实例 2005-04-01

1 2 下一页