テクニカルサポート
絞込み
トピック
-
全てのトピック
- ライセンス
コンテンツのタイプ
- FAQ (22)
製品カテゴリ
-
全ての製品カテゴリ
-
ソフトウェア
-
アプリケーション・ソフトウェア
- オシロスコープ・ソフトウェア (2)
- ネットワーク・アナライザ・ソフトウェア (2)
- 89600 VSAソフトウェア (2)
- Signal Studioソフトウェア (18)
- Keysightロジック・アナライザ・ソフトウェア (1)
-
アプリケーション・ソフトウェア
-
ソフトウェア
1-22 / 22
FlexDCA: What Licenses Do I Have, And What Features Do They Enable?
FlexDCA: What Licenses Do I Have, And What Features Do They Enable?
FAQ 2018-12-10 |
|
Is it possible to add the N9080B-2TP with the N9080B-1FP installed on the X-Series Analyzer? Should the N9080B-2FP be used instead?
Yes, this is possible. A combination of fixed and transportable licenses can be used.
FAQ 2017-06-28 |
|
無料の試用版はどこにありますか?
製品ファミリごとに、無料の試用版を検索できます。
FAQ 2014-08-14 |
|
How does the 89601BU "update and subscription service" work?
Option 200 is mandatory and you cannot use the 89600 VSA software without having Option 200 installed. Software version.....
FAQ 2014-01-27 |
|
WiMAX用Signal Studioの30日間のトライアル・ライセンスの使用中、このテンポラリ・ライセンスを使用できる残りの日数は、どのようにすると確認できますか?
E4438CまたはE8267Dのフロント・パネル・キーを次の順で押します
FAQ 2013-01-28 |
|
How do I enable the free 30-day trial license?
To obtain a trial license for Signal Studio B models (e.g. N7615B), download the Signal Studio software and visit the Keysight Software Licensing trial license request page for that model.
FAQ 2012-12-30 |
|
What is a 30-day free trial license and how does it work?
The 30-day free trial period allows the user to try out our latest Signal Studio software products prior to purchase.
FAQ 2012-12-30 |
|
After the 30-day trial license is activated, can I suspend the trial period for future use?
No, the trial license is valid for 30 consecutive days, after which, you will have to purchase a permanent license to continue using the software.
FAQ 2012-12-28 |
|
How is the time remaining for a trial license tracked?
You can track the time remaining on the trial license from the front panel of the ESG/PSG by pressing Utility > Instrument Adjustments > Instrument Options > Waveform Licenses.
FAQ 2012-12-28 |
|
Can I renew or extend the 30-day trial license after expiration?
After the trial license expires on an instrument, it cannot be renewed or extended.
FAQ 2012-12-28 |
|
If I purchased a license for one signal generator, is that license transferable between signal generators?
Yes, transportable licenses are now available under the new Keysight licensing model.
FAQ 2012-12-28 |
|
Is there a 30-day trial license for this application?
Only selected Signal Studio software applications have the 30-day free trial license available, while others allow a free evaluation of the software interface only.
FAQ 2012-12-11 |
|
How do I install my N7620B licenses?
All N7620B licenses are managed with the Keysight License Manager.
FAQ 2012-10-28 |
|
How do I upgrade my N7620A licenses?
Contact the customer contact center at Keysight Technologies.
FAQ 2012-10-28 |
|
Do I have to upgrade my N7620A licenses?
You may want to upgrade your N7620A licenses to N7620B licenses so that they can be managed using the Keysight License Manager.
FAQ 2012-10-28 |
|
How do I manage my N7620A licenses?
The N7620A software allows you to view your original N7620A licenses.
FAQ 2012-10-28 |
|
What do the N7620B upgrade licenses cost?
All N7620B license upgrades are free.
FAQ 2012-10-28 |
|
Will the N7620B software recognize my N7620A licenses?
The N7620B software recognizes all N7620A licenses except for the N8241A, N6030A, and N9330A external Arbs.
FAQ 2012-10-28 |
|
I have the basic functionality license for N7620A and I want to get the advanced capability license. What should I do?
Install the N7620B software and get the N7620B-QFP, or N7620B-QTP advanced capability license
FAQ 2012-10-28 |
|
ENAソフトウェア・オプションの試用ライセンスはありますか?
モデルによって異なります。
FAQ 2011-10-16 |
|
How is a Signal Studio application license installed?
A Signal Studio license is installed using the License Manager software utility available for download and on the CD shipped with the Signal Studio software.
FAQ 2010-09-08 |
|
Signal StudioソフトウェアはPCに対してライセンスされていますか、信号発生器に対してライセンスされていますか?
Signal Studioソフトウェアは信号発生器用にライセンスされています。
FAQ 2007-09-14 |
|