您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

1-25 / 191

排序:
Signal Generator Firmware Update Center
Download signal generator firmware, release notes, upgrade guide and FAQs.

FAQ 2019-07-19

BenchVue Licenses Included with Instruments FAQ
FAQ about the BenchVue licenses

FAQ 2019-05-16

How do I activate my BenchVue license that was included with my instrument?
For licenses that are included with your instruments follow these steps...

FAQ 2019-05-16

How do I upgrade my N9935A/36A/37A/38A/60A/61A/62A FieldFox Handheld Microwave Spectrum Analyzer?
N9935A/36A/37A/38A/60A/61A/62A FieldFox Handheld Microwave Spectrum Analyzer Trial Option Licenses and Upgrades

FAQ 2019-01-17

FlexDCA: What Licenses Do I Have, And What Features Do They Enable?
FlexDCA: What Licenses Do I Have, And What Features Do They Enable?

FAQ 2018-12-10

What Information Should I Collect From FlexDCA Before Asking Keysight For Help?
What Information Should I Collect From FlexDCA Before Asking Keysight For Help?

FAQ 2018-12-10

Are there VNA setup files for the HDMI 2.1 category 3 connector?
Yes, there are setup files for the E5071C ENA vector network analyzer and the PXI vector network analyzers.

FAQ 2018-11-27

89600 VSA 和 89600 WLA 軟體支援哪些硬體平台?
此處列出了當前軟體版本所支援的量測硬體,包括硬體前端。

FAQ 2018-09-25

89601B VSA software and X-Series signal analyzer software compatibility matrix
Supported versions listed here

FAQ 2018-03-20

When using OFDM mode in N7610B Signal Studio for Short Range Communications, is User File data supplied by an external file started with MSB or LSB?
The first bit in the file is used first. So this can be thought of as the MSB is used first.

FAQ 2017-06-28

How do I create a Mono FM Signal using N5182B MXG ARB?
You can configure N7611B Signal Studio Broadcast Radio to play a mono/FM signal.

FAQ 2017-06-28

Can a CalPod system be used with the N1500A software?
No, the CalPod and N1500A Software are not compatible.

FAQ 2017-06-28

For signals requiring wider bandwidth, how can Keysight’s LTE Signal Studio waveform creation products be used to increase carrier spacing?
Set the FFT length to 8192 and a sample rate of 800 MHz. Subcarrier spacing = sampleRate/FFT size

FAQ 2017-06-28

How many carriers can the MXG support in Carrier Aggregation mode?
One MXG can support one instance of the Carrier Aggregation mode. One instance of the Carrier Aggregation mode supports 5 component carriers.

FAQ 2017-06-28

Is it possible to add the N9080B-2TP with the N9080B-1FP installed on the X-Series Analyzer? Should the N9080B-2FP be used instead?
Yes, this is possible. A combination of fixed and transportable licenses can be used.

FAQ 2017-06-28

What are the new Wave 2 features for Mobile WiMAX™ 802.16 system profiles?
Read about IO-MIMO and IO-BF (beamforming) profiles...

FAQ 2016-12-02

In N7625B, how many instances of carriers and carrier aggregations do the software support?
One connected signal generator can support one instance of Carrier Aggregation mode. One instance of Carrier Aggregation can support 5 component carriers.

FAQ 2016-07-08

Why isn’t the unit being discovered by VSA software hosted inside the instrument itself?
Check to see if Keysight Technologies is returned from the analyzer as part of the *IDN query.

FAQ 2016-07-08

30-Day Free Trial for X-Series Measurement Applications for X-Series Modular Instruments
30-day trial license available for the X-Series measurement applications for X-Series modular signal analyzers.

FAQ 2016-06-09

高速數位應用部署方法(MOI)

FAQ 2016-04-14

如何將 E5063A ENA 系列網路分析儀升級?
有關硬體和軟體選項的升級資訊

FAQ 2016-02-08

我要如何將 E5061B ENA 系列網路分析儀升級?
硬體與軟體選項升級資訊

FAQ 2016-01-27

如何升級我的 N9913A/14A/15A/16A/17A/18A/50A/51A/52A FieldFox 手持式微波分析儀?
N9913A/14A/15A/16A/17A/18A/50A/51A/52A FieldFox 手持式微波分析儀試用選項授權和升級。

FAQ 2015-08-20

E5072A 硬體、軟體,以及韌體升級
E5072A ENA 系列網路分析儀升級選項完整清單

FAQ 2015-07-27

Can Y-Applications and V-Applications co-exist on the same E6640A EXM?
Yes, you may have both Y-Apps and V-Apps on the same EXM.

FAQ 2015-02-27

1 2 3 4 5 6 7 8 下一頁