이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

1-25 / 202

정렬방식:
Signal Generator Firmware Update Center
Download signal generator firmware, release notes, upgrade guide and FAQs.

FAQ 2020-06-19

How do I update my X-Series Signal Analyzer Benchtop Software
Software updates for the X-Series Signal Analyzers Benchtop (PXA/MXA/EXA/CXA/MXE/ PXE)

FAQ 2020-03-17

Noise Figure FAQ for Network Analyzers
Frequently asked questions about the PNA-X Series Source-Corrected Noise Figure Measurement (Option 029)

FAQ 2020-01-09

What sets DMX apart from the applications that are built into the VNA already?
FAQ for DMX

FAQ 2019-10-16

What VNA models work with DMX?
FAQ for DMX

FAQ 2019-10-16

What problem is DMX trying to solve?
FAQ for DMX problem solving

FAQ 2019-10-16

What is BenchVue Software?
Additional information about BenchVue software.

FAQ 2019-05-28

JSPX?ID=2850571&CC=US&LC=ENG JSPX?ID=2850571&CC=US&LC=ENG
BenchVue Licenses Included with Instruments FAQ
FAQ about the BenchVue licenses

FAQ 2019-05-16

How do I activate my BenchVue license that was included with my instrument?
For licenses that are included with your instruments follow these steps...

FAQ 2019-05-16

FlexDCA: What Licenses Do I Have, And What Features Do They Enable?
FlexDCA: What Licenses Do I Have, And What Features Do They Enable?

FAQ 2018-12-10

What Information Should I Collect From FlexDCA Before Asking Keysight For Help?
What Information Should I Collect From FlexDCA Before Asking Keysight For Help?

FAQ 2018-12-10

Are there VNA setup files for the HDMI 2.1 category 3 connector?
Yes, there are setup files for the E5071C ENA vector network analyzer and the PXI vector network analyzers.

FAQ 2018-11-27

Where can I find software downloads for PathWave Test?
Go to http://www.keysight.com/find/pathwave-test-latest-downloads

FAQ 2018-06-12

VSA software and X-Series signal analyzer software compatibility matrix
Supported versions listed here

FAQ 2018-03-20

For signals requiring wider bandwidth, how can Keysight’s LTE Signal Studio waveform creation products be used to increase carrier spacing?
Set the FFT length to 8192 and a sample rate of 800 MHz. Subcarrier spacing = sampleRate/FFT size

FAQ 2017-06-28

How many carriers can the MXG support in Carrier Aggregation mode?
One MXG can support one instance of the Carrier Aggregation mode. One instance of the Carrier Aggregation mode supports 5 component carriers.

FAQ 2017-06-28

When using OFDM mode in N7610B Signal Studio for Short Range Communications, is User File data supplied by an external file started with MSB or LSB?
The first bit in the file is used first. So this can be thought of as the MSB is used first.

FAQ 2017-06-28

How do I create a Mono FM Signal using N5182B MXG ARB?
You can configure N7611B Signal Studio Broadcast Radio to play a mono/FM signal.

FAQ 2017-06-28

Is it possible to add the N9080B-2TP with the N9080B-1FP installed on the X-Series Analyzer? Should the N9080B-2FP be used instead?
Yes, this is possible. A combination of fixed and transportable licenses can be used.

FAQ 2017-06-28

CalPod system을 N1500A 소프트웨어와 함께 사용 할 수 있습니까?
아니요. CalPod와 N1500A 소프트웨어는 호환되지 않습니다.

FAQ 2017-01-24

What are the new Wave 2 features for Mobile WiMAX™ 802.16 system profiles?
Read about IO-MIMO and IO-BF (beamforming) profiles...

FAQ 2016-12-02

In N7625B, how many instances of carriers and carrier aggregations do the software support?
One connected signal generator can support one instance of Carrier Aggregation mode. One instance of Carrier Aggregation can support 5 component carriers.

FAQ 2016-07-08

Why isn’t the unit being discovered by VSA software hosted inside the instrument itself?
Check to see if Keysight Technologies is returned from the analyzer as part of the *IDN query.

FAQ 2016-07-08

신호안에 펄스가 없는 구간을 추가할 수 있는 방법이 있나요?
네. 펄스 패턴에 "Off Time"을 추가할 수 있으며 원하는 펄스 조건에 맞게 시간조정도 가능합니다.

FAQ 2016-07-05

30-Day Free Trial for X-Series Measurement Applications for X-Series Modular Instruments
30-day trial license available for the X-Series measurement applications for X-Series modular signal analyzers.

FAQ 2016-06-09

1 2 3 4 5 6 7 8 9 다음