Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

51-75 of 195

Sort:
How does the 89601BU "update and subscription service" work?
Option 200 is mandatory and you cannot use the 89600 VSA software without having Option 200 installed. Software version.....

FAQ 2014-01-27

What is the RF Test Blog?
RF engineers know that making good measurements is a challenge. The RF Test Blog was created as a resource for RF engineers to find ways to make better RF measurements.

FAQ 2013-12-17

What are the remote control commands to switch between FlexDCA and the legacy user interface?
The :SYSTem:FCONfig command can be used to switch between the possible user interfaces.

FAQ 2013-12-12

Can I upgrade my 86100A, 86100B or 86100C mainframe to obtain an 86100D?
The 86100D has major hardware differences that make an upgrade uneconomical. Keysight regularly offers trade-in and other incentive programs for DCA mainframes. Contact your local representative for details about the current trade-in program available for your unit.

FAQ 2013-11-27

What is the E8267D Option 016?
E8267D Option 016 is a PSG with differential inputs designed specifically for the N6030A arbitrary waveform generator outputs.

FAQ 2013-10-20

Which version of the CPRI standard is the N5120A compliant to?
The N5120A is compliant up to v1.1.

FAQ 2013-09-27

How do I change the 10 MHz reference source if Signal Studio for pulse building doesn’t detect the reference?
Most of the time, Signal Studio will recognize the reference; however, it can be changed in the download -> customize menu.

FAQ 2013-05-16

Are there any options to adjust the pulse definitions within Signal Studio for pulse building?
No, at the moment the rise and fall times are defined by their 0-100 percent points and the pulse width is defined to be the 100-100 percent point.

FAQ 2013-05-16

Where can I find information or example programs using the API for Signal Studio?
The Signal Studio for pulse building help file has information and example programs under the API control chapter.

FAQ 2013-05-16

Is it possible to adjust the phase offset using degrees instead of radians?
Yes. Select View -> Customize Pattern Item Table and toggle the ‘phase offset in degrees’ button

FAQ 2013-05-16

Is there a way to put insert a missing pulse into the signal?
Yes, you can add a “Off time” object to the pulse pattern and change the duration to meet your pulse requirements.

FAQ 2013-05-16

Which 89600 VSA version is supported by firmware release A.12.xx on Windows 7?
All 89601B versions should work with firmware release A.12 for Windows 7.

FAQ 2013-04-25

How can I get 8960 Lab Application Annual Contract Subscription Release Downloads?
Get the latest downloads here

FAQ 2013-02-28

HTML HTML
When I use the 30-day trial license of the Signal Studio for WiMAX™, how can I check the number of days remaining on temporary license?
Press the front panel keys: Utility > Instrument Adjustments > Instrument Options > Waveform Licenses

FAQ 2013-01-28

How do I get the manuals and release notes for the 8960 (E5515C/E)?
Online User's Guide Index

FAQ 2013-01-18

How do I make measurements with the 8960 (E5515C/E)?
Keysight 8960 Online User's Guides

FAQ 2013-01-18

Unsigned assembly error with 89600 VSA software version 16.00
This FAQ descibes how to correct the unsigned assembly error with version 16.00

FAQ 2013-01-14

How much jitter is there when using an external trigger?
Unless the trigger signal is synchronized to the Arb sample clock, you will see jitter equal to the sample period for the internal Arb and equal to 8 sample periods for the N6030A.

FAQ 2012-12-30

Is there a way to simulate jitter in my pulse pattern?
Yes, Signal Studio for pulse building allows you to add jitter on the pulse width and pulse repetition interval.

FAQ 2012-12-30

Can I turn off the N6030A arbitrary waveform generator predistortion from the N7620B Signal Studio for Pulse Building to get more power?
No. The N7620B software does not allow the N6030A predistortion to be turned off.

FAQ 2012-12-30

How do I enable the free 30-day trial license?
To obtain a trial license for Signal Studio B models (e.g. N7615B), download the Signal Studio software and visit the Keysight Software Licensing trial license request page for that model.

FAQ 2012-12-30

On my E8267D, I get an error that the signal requires more repeats than supported, can I increase this limit with the internal baseband option?
No. To increase the number of pulse capacity either upgrade to an External Baseband option with the N8241A AWG or ...

FAQ 2012-12-30

Does the Signal Studio for Pulse Building software run on a National Instruments embedded PXI controller like the one that comes with the N6030A?
Yes, it does. However, the Keysight I/O Libraries may need to be installed as a secondary VISA and then the NI Tulip DLL may need to be enabled.

FAQ 2012-12-30

Is there an easy way to save a pulse pattern and send it to another person?
Yes, simply save the entire .pbp or you can export the pattern using the “export pattern” function.

FAQ 2012-12-30

Why does my ESG report errors when I try to download waveforms using a National Instruments GPIB card with certain Signal Studio applications?
If errors reported by the ESG include “ -113 undefined header” and “-101 invalid character”, you need to download and install a patch for the Keysight IO Libraries.

FAQ 2012-12-30

Previous 1 2 3 4 5 6 7 8 Next