Technical Support
Electronic Measurement
Refine the List
By Topic
- Calibration (7)
- Configuration & Installation (18)
- Display Messages/Error Codes (2)
- Licensing (22)
- Measurement & Instrument Fundamentals (22)
- Measurement Techniques (22)
- Operating System & Software (22)
- Operation & Functionality (52)
- Other Information (1)
- Parts & Accessories (5)
- Product & Firmware Updates & Upgrades (22)
- Product Theory of Operation (2)
- Programming & Data Transfer (3)
- Service & Maintenance (2)
- Specifications & Accuracy (2)
- Troubleshooting (3)
By Industry/Technology
By Type of Content
- FAQ (195)
By Product Category
-
All Product Categories
-
Software
- Application Software
-
Software
126-150 of 195
Does 89600 VSA software (89601) support the Bluetooth® Difference Error Vector Magnitude (DEVM) test?
The 89601 Option AYA does not provide DEVM results for Bluetooth basic measurement. Keysight recommends using N9081A Bluetooth measurement application.
FAQ 2012-03-27 |
|
What is preventing the 89600 VSA software, running on a PC, from connecting to an X-Series signal analyzer?
Procedure for connecting from 89600 VSA software to an X-Series signal analyzer.
FAQ 2012-03-16 |
|
Is a W-CDMA Test uSIM included with the W-CDMA TA and LA?
The W-CDMA Test uSIM is included with the E6703C W-CDMA Lab Application. It is not included with E1963A Test Application.
FAQ 2012-03-02 |
|
Can or will the N9081A and W9081A support Bluetooth® 4.0?
Yes, the N9081A and W9081A support the low energy measurements enabled by Bluetooth 4.
FAQ 2012-03-02 |
|
How do the 89400 and 89600 families of vector signal analyzers (VSA) perform carrier-locking on a digitally-modulated signal?
First, the center frequency must be set to the carrier frequency within ±3% of the symbol rate...
FAQ 2012-02-25 |
|
Is Signal Studio software licensed to the PC or signal generator?
Signal Studio software is licensed to the signal generator. More...
FAQ 2012-02-19 |
|
Is 4-port calibration using the 2-port ECal module supported on ENA Option TDR?
No.
FAQ 2012-02-02 |
|
Why is the peak power for Transmit Analysis 3.78 dBm, but with Zero span it is 3.66 dBm?
It is measured in the IQ domain, not in power domain, so there is no VBW function. The most important factor is the bucket width.
FAQ 2012-01-10 |
|
Can the Keysight X-Series signal analyzer with N9081A Bluetooth® measurement application measure Bluetooth hopping signals?
The short answer for this question is “no”. Fundamentally, frequency hopping is needed for testing the functional capability of the Bluetooth device.
FAQ 2012-01-10 |
|
When does the BER test apply in the N9081A Bluetooth® measurement application?
The BER test only applies for EDR with a PRBS9 signal pattern.
FAQ 2012-01-10 |
|
Why does the Bluetooth® ACP measurement take 15 minutes to complete?
The time needed for the ACP measurement is due to the requirements of the Bluetooth-test specification.
FAQ 2012-01-10 |
|
Can I demodulate and analyze 802.11ac wide bandwidth signals with my N9030A PXA Signal Analyzer once it has 160 MHz analysis bandwidth?
Once the insturment has 160 MHz analysis bandwidth, it will be possible to analyze wide bandwidth 802.11ac signals using the February, 2012 89601B VSA software release with Option BHJ.
FAQ 2011-11-14 |
|
What are the specifications for N9030A PXA's 160 MHz analysis bandwidth?
The specifications will remain the same up to 140 MHz and nominal values will be provided for analysis bandwidth above 140 MHz.
FAQ 2011-11-14 |
|
What is required to run EasyEXPERT 4.2 or later?
Click the above link for details.
FAQ 2011-10-26 |
|
What is required to run EasyEXPERT 3.2 to 4.11?
The software requirements of EasyEXPERT 3.2 to 4.11 are as follows.
FAQ 2011-10-26 |
|
Does Keysight provide the upgrade product for OS of B1500A/B1505A from XP to Windows 7?
Yes, there is an upgrade product from XP to Windows 7 embedded.
Please contact your sales representative or a contact center of your country.
FAQ 2011-10-26 |
|
How can I tell if my N9030A Signal Analyzer is licensed for 160 MHz analysis bandwidth?
On your instrument, press [System}, {Show}, {System} on the front panel. If your instrument is licensed for 160 MHz analysis bandwidth, you will see both options "N9030A-B1X, Analysis bandwidth, 140 MHz" and option "N9030A-B1Y, Analysis bandwidth extension, 160 MHz" listed.
FAQ 2011-10-18 |
|
Can I measure a dual conversion mixer on the ENA?
If the LO frequencies are fixed, dual conversion mixers can be measured with option 008 (Frequency-Offset Mode).
FAQ 2011-10-17 |
|
Can the ENA perform Vector Mixer Calibration (VMC) with Fixed RF or Fixed IF measurement?
No. It is not possible to perform Fixed RF measurements (RF: Fixed, LO and IF: Swept) with VMC.
FAQ 2011-10-17 |
|
When I perform both the calibration with frequency offset off and the scalar-mixer calibration with frequency offset on, which one is valid?
If the frequency offset function is turned on, the scalar mixer calibration data is used.
FAQ 2011-10-17 |
|
Can the ENA make mixer measurements?
Yes. With option 008 (Frequency-Offset Mode), you can measure frequency-converting devices, such as mixers.
FAQ 2011-10-16 |
|
Is there an outline to achieving a simplified mixer conversion loss measurement on the ENA?
Option 008, Frequency offset, is required for mixer measurements utilizing these analyzers.
FAQ 2011-10-16 |
|
On mixer measurement with the ENA and external signal source, should I connect frequency references of the ENA and external signal source?
Yes.
FAQ 2011-10-16 |
|
Is there a trial license for the ENA software option?
It depends on models...
FAQ 2011-10-16 |
|
When the frequency-offset is turned on, the number of sweeps during measurement increases. Is this the normal operation for the ENA?
Yes.
FAQ 2011-10-16 |
|