検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

1-25 / 30

並べ替え
Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

[仕様] USBモジュラ型測定器は、Windows7をサポートしていますか?
はい、最新のKeysight Measurement ManagerにてWindows7 32bitをサポートしています。

FAQ 2013-06-24

GPIBインタフェース(82357A、E5810A、82350B)を使って、GPIB経由でPC上から計測器を自動計測する方法を教えてください。
GPIBインタフェース(82357A、E5810A、82350B)を使って....

FAQ 2013-06-19

How can previously created data in BenchLink II be exported?
Open a previously saved configuration file with data and then export the data as a Text (.txt) file or Comma Separated values (.csv) file.

FAQ 2012-11-05

[仕様] Keysight Measurement Managerは、Windows Vistaでサポートされていますか?
はい、Keysight Measurement Manager バージョン 1.8.3.0以上にて、Windows Vista(Service Pack 1、Business, Ultimate, Enterprise, Basic, Home Premium Editionの各種パッケージ)をサポートしています。

FAQ 2010-11-03

[仕様] Keysight Measurement Manager (AMM) は、英語以外の言語設定もサポートしますか。
はい、Keysight Measurement Manager (AMM) は、英語以外の言語設定もサポートします。

FAQ 2010-11-02

Why won't Help (.hlp) files view properly with Windows Vista?
In order to view 32-bit Help (.hlp) files with Windows® Vista, you must download the WinHlp32.exe Help program from the Microsoft web site at http://go.microsoft.com/fwlink/?LinkID=82148.

FAQ 2010-10-12

What drivers will be provided with modular products?
IVI-COM, IVI-C and LabVIEW (G), are provided with all Keysight modular products...

FAQ 2010-10-06

Where can customers download instrument drivers? (LabVIEW, Visual-studio.net,…)
The instrument drivers are provided with each instrument on a CD...

FAQ 2010-10-06

Why does the error message "Failed to retrieve available devices. Please make sure the connection to Keysight IO libraries is available" appear…
The message "Failed to retrieve available devices. Please make sure the connection to Keysight IO libraries is available" appear because….

FAQ 2010-08-09

How can I prevent a loading delay when using the Measurement Manager with Microsoft® .NET 2.0 on a computer that is connected to a LAN…
To prevent a loading delay when using the Measurement Manager (AMM) with Microsoft® .NET 2.0, follow the instructions below:….

FAQ 2010-08-09

Why is my acquired data for U2300A and U2500A shifted? eg. Column 2 data is in column 1, column 3 data is in column 2, and so on.
Install DAQ hardware driver version 1.05 and above.

FAQ 2010-08-09

Why do I not see all the data points on my graph tab?
When viewing your readings from the Graph Tab, some times not all of your data is displayed.

FAQ 2009-11-05

How to speed up my computer processing time while running the BenchLink DataLogger software continuously for a long period of time?
Do not leave the Quick Graph tab active in the BenchLink DataLogger...

FAQ 2009-08-19

How do I avoid getting "The memory could not be "read"" error upon closing the software?
It’s most likely this issue is caused by a bad memory...

FAQ 2009-08-19

How do I avoid getting “Out of memory” exception errors when using the BenchLink DataLogger software?
Do not leave the Quick Graph tab active in the BenchLink DataLogger...

FAQ 2009-08-19

Is U2300A and U2500A series DAQ supported in Linux environment?
No. U2300A and U2500A are not supportable in Linux environment.

FAQ 2009-08-06

What is the required operating system for the U2300A Series Modular Multifunction Data Acquisition (DAQ) devices?
The operating system required for the U2300A Series Modular Multifunction Data Acquisition (DAQ) devices is….

FAQ 2008-09-25

USB DAQソフトウェアはLinuxオペレーティング・システムで動作しますか?
動作しません。

FAQ 2008-09-23

What are the differences between the BenchLink DataLogger software for 34970A and 34980A?

FAQ 2007-07-20

How do I configure channels in BenchLink Data Logger 3, run a scan in a remote location, and upload the data back into my computer?
Create a setup in BenchLink Data Logger 3 software as you normally would, then go to the "Configuration | Download Open Configuration to 34970A..." menu to download the setup to the 34970A...

FAQ 2006-01-18

Is there a way to show values on the axes of the strip chart in BenchLink Data Logger 3?
Yes! In the Quick Graph tab, choose Preferences and select "Show X-Axis Labels" then select "Apply" or "OK".

FAQ 2006-01-18

Are computed channels supported in the Keysight 34970A?
Computed channels are not supported on the 34970A, but are on the BenchLink Data Logger software.

FAQ 2006-01-18

Can I use BenchLink Data Logger 3 to turn on and off switches in the 34903A, 34904A, 34905A, or 34906A at certain intervals?
The BenchLink Data Logger 3 software was designed to be used for data acquisition rather than switching. Therefore the control of switching is limited through the BenchLink Data Logger software.

FAQ 2006-01-18

Is there a way to control the digital to analog converter output of the Keysight 34907A Multi-function module with the BenchLink Data Logger 3 softw...
Yes. The BenchLink Data Logger 3 Software can be used to set a discrete value DAC output of the 34970A. However, the output cannot be included in the scan list.

FAQ 2006-01-18

1 2 次へ