Aqui está a página que achamos que você queria. Veja o resultado da pesquisa ao invés de:

 

Contact an Expert

Suporte técnico

Medição Eletrônica

Support by Product Model Number:

1-25 de 30

Sort:
Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

How can previously created data in BenchLink II be exported?
Open a previously saved configuration file with data and then export the data as a Text (.txt) file or Comma Separated values (.csv) file.

FAQ 2012-11-05

Why won't Help (.hlp) files view properly with Windows Vista?
In order to view 32-bit Help (.hlp) files with Windows® Vista, you must download the WinHlp32.exe Help program from the Microsoft web site at http://go.microsoft.com/fwlink/?LinkID=82148.

FAQ 2010-10-12

Where can customers download instrument drivers? (LabVIEW, Visual-studio.net,…)
The instrument drivers are provided with each instrument on a CD...

FAQ 2010-10-06

What drivers will be provided with modular products?
IVI-COM, IVI-C and LabVIEW (G), are provided with all Keysight modular products...

FAQ 2010-10-06

How do I control instruments such as 82357A, E5810A, and 82350B using the GPIB interface?
There are several approaches to control instruments via the GPIB interface...

FAQ 2010-10-04

Why does the error message "Failed to retrieve available devices. Please make sure the connection to Keysight IO libraries is available" appear…
The message "Failed to retrieve available devices. Please make sure the connection to Keysight IO libraries is available" appear because….

FAQ 2010-08-09

How can I prevent a loading delay when using the Measurement Manager with Microsoft® .NET 2.0 on a computer that is connected to a LAN…
To prevent a loading delay when using the Measurement Manager (AMM) with Microsoft® .NET 2.0, follow the instructions below:….

FAQ 2010-08-09

Why is my acquired data for U2300A and U2500A shifted? eg. Column 2 data is in column 1, column 3 data is in column 2, and so on.
Install DAQ hardware driver version 1.05 and above.

FAQ 2010-08-09

When will Keysight USB modular instruments and USB Modular DAQs supports Windows 7?
For 32 bit Windows 7, the supportability of modular instruments and DAQs will happen...

FAQ 2010-07-18

Why do I not see all the data points on my graph tab?
When viewing your readings from the Graph Tab, some times not all of your data is displayed.

FAQ 2009-11-05

How do I avoid getting "The memory could not be "read"" error upon closing the software?
It’s most likely this issue is caused by a bad memory...

FAQ 2009-08-19

How to speed up my computer processing time while running the BenchLink DataLogger software continuously for a long period of time?
Do not leave the Quick Graph tab active in the BenchLink DataLogger...

FAQ 2009-08-19

How do I avoid getting “Out of memory” exception errors when using the BenchLink DataLogger software?
Do not leave the Quick Graph tab active in the BenchLink DataLogger...

FAQ 2009-08-19

Is U2300A and U2500A series DAQ supported in Linux environment?
No. U2300A and U2500A are not supportable in Linux environment.

FAQ 2009-08-06

Does the Measurement Manager (AMM) run on Window Vista operating system?
Yes. The Measurement Manager (AMM) rev. 1.8.3.0 and above will able to run on Windows Vista ...

FAQ 2009-06-10

Does the Keysight Measurement Manager (AMM) support regional language settings other than English (US)?
Yes, the Keysight Measurement Manager (AMM) supports regional language settings other than English (US)….

FAQ 2009-01-12

What is the required operating system for the U2300A Series Modular Multifunction Data Acquisition (DAQ) devices?
The operating system required for the U2300A Series Modular Multifunction Data Acquisition (DAQ) devices is….

FAQ 2008-09-25

Does the Measurement Manager (AMM) run on a Linux operating system?
No, the Measurement Manager (AMM) does not run on a Linux operating system.

FAQ 2008-09-25

What are the differences between the BenchLink DataLogger software for 34970A and 34980A?

FAQ 2007-07-20

Can Excel control a scan, and make and record measurements using the 34980A?
Use the 34980A IntuiLink add-in or the Excel Macro language.

FAQ 2007-01-22

Are computed channels supported in the Keysight 34970A?
Computed channels are not supported on the 34970A, but are on the BenchLink Data Logger software.

FAQ 2006-01-18

How do I configure channels in BenchLink Data Logger 3, run a scan in a remote location, and upload the data back into my computer?
Create a setup in BenchLink Data Logger 3 software as you normally would, then go to the "Configuration | Download Open Configuration to 34970A..." menu to download the setup to the 34970A...

FAQ 2006-01-18

Can I change the format of the data when I export from BenchLink Data Logger 3 software?
No, there is no way to change the default formats when exporting data from BenchLink Data Logger 3 software. However, you can easily change the data formats once you have the data in Microsoft(R) Excel.

FAQ 2006-01-18

Is there a way to show values on the axes of the strip chart in BenchLink Data Logger 3?
Yes! In the Quick Graph tab, choose Preferences and select "Show X-Axis Labels" then select "Apply" or "OK".

FAQ 2006-01-18

1 2 Avançar