Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

126-150 of 395

Sort:
How do I branch from one scan to another?
The Stop the scan and start the scan on action on the “Configure Events” tab, allows you to branch to another scan list on the occurrence of the corresponding event.

FAQ 2010-05-05

I don't have channels wired-up yet. How can I experiment with Data Logger Pro?
You can view getting started “simulations” by clicking Help > Start Simulation Mode and selecting a simulation from the list.

FAQ 2010-05-05

Can I have different channels in different scan lists?
You can have different enabled channels in different scan lists.

FAQ 2010-05-05

How is licensing implemented for Data Logger Pro?
To run the Data Logger Pro software after the evaluation period, you must have a license for each PC using the software.

FAQ 2010-05-05

What is an Action Script and what can I do with it?
An Action Script contains one or more action steps that perform actions on modules in 34970A/34980A instruments, and other instrumentation connected to the PC.

FAQ 2010-05-05

Can I start a scan and then close Data Logger Pro and continue scanning?
Yes. However, there are some limitations.

FAQ 2010-05-05

How can I open a configuration from a different data logger application?
See “Import Data Logger 3 Configuration”, or “Import Data Logger for 34980A Configuration”, or “Packages” in the Help menu for detail.

FAQ 2010-05-05

Can I reduce data while scanning?
No. All scanned data is saved in the datalog.

FAQ 2010-05-05

How are multiple scan lists graphed?
The starting point for each scan list is indicated by a vertical bar on the graph and the label Started.

FAQ 2010-05-05

Can I be scanning and run an Action Script at the same time (in parallel)?
No. Scan lists and Action Scripts are executed sequentially

FAQ 2010-05-05

Where can I export the data?
You can save data to files on any disk drive or storage media connected to your PC.

FAQ 2010-05-05

Can I upload instrument configurations and scanned data from an instrument?
Yes. To upload the instrument configuration and, if available, measured data, click Configuration > New by Upload...

FAQ 2010-05-05

How do I control instruments using SCPI commands?
You can use Action Scripts and SCPI commands to control any instrument connected to the PC.

FAQ 2010-05-05

I'm only interested in some of the scanned data. Can I automatically reduce the data during export?
Yes. You can also reduce data when graphing. See “Data Reduction” in the Help menu for details.

FAQ 2010-05-05

How can I Locate Exported Data on the Hard Disk?
You can control where files are stored using either the automatic or manual methods discussed above.

FAQ 2010-05-05

Can I mix 34980As and 34970As in the same configuration?
You can have a combination of one 34980A and one or two 34970As in a configuration.

FAQ 2010-05-05

How many instruments can I have in a configuration?
You can have up to two 34980As or four 34970As in a configuration

FAQ 2010-05-05

What are channel limits?
Limits can be set on multiplexer, totalizer and digital read channels (see the limit types question below).

FAQ 2010-05-05

Can I run two scan lists at the same time (in parallel)?
No. Scan lists can only be run sequentially

FAQ 2010-05-05

What is the Base scan list?
The default scan list is named Scan List A and is the Base scan list.

FAQ 2010-05-05

Can I filter the data shown on a graph?
Yes. On a graph tab, click the Channels... button to select which channels to graph and/or to show only certain measurement functions.

FAQ 2010-05-05

How can I update the 34980A to Firmware Revision 2.19?

FAQ 2010-05-05

Are there separate licenses for 34970A and 34980A instruments?
Yes. Each instrument uses a specific Data Logger Pro product number.

FAQ 2010-05-05

How can I tell if my PC is licensed?
In Data Logger Pro, click Tools > Licensing > License Status... The “License Status” dialog box displays your PC's license status.

FAQ 2010-05-05

Can I rename an instrument instead of using the default Instr1, Instr2... naming convention?
Yes. Click on InstrN in the Name column of the “Configure Instruments” tab and enter a new instrument name.

FAQ 2010-05-05

Previous 1 2 3 4 5 6 7 8 9 10 ... Next