Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

Уточнить список

убрать все фильтры

По теме

По типу содержания

По типу оборудования

51-75 из 397

Упорядочить:
Why won't Help (.hlp) files view properly with Windows Vista?
In order to view 32-bit Help (.hlp) files with Windows® Vista, you must download the WinHlp32.exe Help program from the Microsoft web site at http://go.microsoft.com/fwlink/?LinkID=82148.

FAQ 2010-10-12

34970A: How do I add a DMM to a 34970A that does not have one installed?
Order the customer installable retrofit kit 34970-80100.

FAQ 2010-10-12

What kind of backplane connectors do the PXI switches have?
The M9101A-M9160A PXI switches are PXI1 with a J1 only connector...

FAQ 2010-10-11

Are these switches programmed using SCPI?
No. Since the modules are essentially register-based, the software drivers handle all the direct module interaction and control...

FAQ 2010-10-11

Are there any calibration options?

FAQ 2010-10-11

Do these products appear in the Keysight connection expert?

FAQ 2010-10-11

Does this work in test stand? NI switch executive?

FAQ 2010-10-11

Can I put the Keysight Switch cards into a PXIe chassis?
Only a PXIe chassis that has hybrid slots...

FAQ 2010-10-11

Are there SCAN commands for the switches?
No. There is no scan-list / switch handshake personality built into the DMM + Switch...

FAQ 2010-10-11

How can I input 28V digital signal to U2651A/U2652A when it support digital input voltage < 24V?
You can connect a voltage divider in front of the digital input to reduce the voltage to <24V

FAQ 2010-10-07

What is the compatibility between PXIe chassis and Keysight new PXI/PXIe modules?
Keysight modules come in several varieties, so inspection is required to determine compatibility...

FAQ 2010-10-06

Can I use SCPI to communicate with my Keysight modules?
No. Connectivity is provided through Drivers.

FAQ 2010-10-06

Can I replace other vendors' module (for example a digitizer) with a Keysight one?
There are two aspects to consider...

FAQ 2010-10-06

Where can customers download instrument drivers? (LabVIEW, Visual-studio.net,…)
The instrument drivers are provided with each instrument on a CD...

FAQ 2010-10-06

Will ExpressVIs work with Keysight hardware?
No. Keysight has VIs available to use with LabView but not ExpressVIs.

FAQ 2010-10-06

How do I find a partner to help develop my modular solution?
Keysight has a number of solution partners that can help define and create your modular solution...

FAQ 2010-10-06

What drivers will be provided with modular products?
IVI-COM, IVI-C and LabVIEW (G), are provided with all Keysight modular products...

FAQ 2010-10-06

Are all PXIe system modules/controllers compatible with all chassis?
No, the PXIe standard requires the chassis support certain configurations but not all...

FAQ 2010-10-06

Can I use the PXIe products over LAN?
If the PXIe chassis has an embedded controller with a LAN port then the PXI system can connect to a LAN port...

FAQ 2010-10-06

Can I use PXI-1 existing cards in the Keysight Card cages and are there any that will no longer work?
Older PXI (PXI-1) modules (which have a J2 present) will not work in Keysight 18-slot PXIe chassis...

FAQ 2010-10-06

Can I run a program that is controlling my PXI instrument while using its soft front panel (SFP)?
Not at this time...

FAQ 2010-10-06

Where can customers find user manuals and example programs for AXIe & PXIe products?
Datasheets of modular products will be included on the CD shipped with every product and will be available on Keysight.com from the product page...

FAQ 2010-10-06

What is the data transfer rate of PXI, PXIe, and AXIe?
PXI-1 has two variants...

FAQ 2010-10-06

Does Keysight have mass interconnect solutions?
There are mass interconnect solutions from MAC panel....

FAQ 2010-10-06

What is the difference between PXIe and AXIe?
The AXIe standard provides the maximum scalability to address a range of platforms...

FAQ 2010-10-06

Назад 1 2 3 4 5 6 7 8 9 10 ... Следующие